<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: MQX TAD call stack in KDS 3</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423285#M14098</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ohad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using KDS you should be able to check &lt;STRONG&gt;MQX Task List&lt;/STRONG&gt;, this is an overview about all tasks created in the MQX RTOS application, for example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55713i954C32C1A3ECBCB0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Stack Usage&lt;/STRONG&gt;, this screen displays information about interrupt and task stacks. Typically, a stack overflow is the root cause for vast majority of problems in MQX RTOS user applications.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55736i43D3061C3DD3CC88/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Lightweight Memory Pools&lt;/STRONG&gt; displays address, size, and type information about each memory block allocated in the selected memory pool by the MQX RTOS system or applications.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55754i69C639CDF61C72D8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I/O Devices&lt;/STRONG&gt; displays name, type and address of I/O Devices used by MQX RTOS application.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55794iF975B6ECA154F2BB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you need to use the MQX Performance Tool like the below image? Unfortunately the MQX Performance Tool is available only in the CodeWarrior IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55822i7558CF6A977A8FCE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 09 Sep 2015 19:11:17 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2015-09-09T19:11:17Z</dc:date>
    <item>
      <title>MQX TAD call stack in KDS 3</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423282#M14095</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello all,&lt;/P&gt;&lt;P&gt;As I have mentioned in other threads here in the forum, we decided to port our application from K60 to K66.&lt;/P&gt;&lt;P&gt;With that, we were forced to stop using Code Warrior (Because the USB stack for K66 is only available for KDS).&lt;/P&gt;&lt;P&gt;The task of porting our code, Bootloader and MQX application, was a tedious one. I have finally been able to start debugging the MQX application.&lt;/P&gt;&lt;P&gt;I am unable to find a way to see the MQX task call stacks. I can only see the task that is currently running when I pause the application (It is always the Idle task...).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can I see all the tasks at once and jump to the needed task to see where it's at and debug?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 03 Sep 2015 07:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423282#M14095</guid>
      <dc:creator>ohadbenjamin</dc:creator>
      <dc:date>2015-09-03T07:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: MQX TAD call stack in KDS 3</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423283#M14096</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ohad, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please attach a screenshot?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 07 Sep 2015 21:56:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423283#M14096</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-09-07T21:56:51Z</dc:date>
    </item>
    <item>
      <title>Re: MQX TAD call stack in KDS 3</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423284#M14097</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here is a screenshot showing the task list but no stack trace.&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55000i51C7379183E39323/image-size/large?v=v2&amp;amp;px=999" title="Task_list.png" alt="Task_list.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Sep 2015 06:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423284#M14097</guid>
      <dc:creator>ohadbenjamin</dc:creator>
      <dc:date>2015-09-08T06:48:56Z</dc:date>
    </item>
    <item>
      <title>Re: MQX TAD call stack in KDS 3</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423285#M14098</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Ohad,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Using KDS you should be able to check &lt;STRONG&gt;MQX Task List&lt;/STRONG&gt;, this is an overview about all tasks created in the MQX RTOS application, for example:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55713i954C32C1A3ECBCB0/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_0.png" alt="pastedImage_0.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Stack Usage&lt;/STRONG&gt;, this screen displays information about interrupt and task stacks. Typically, a stack overflow is the root cause for vast majority of problems in MQX RTOS user applications.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55736i43D3061C3DD3CC88/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Lightweight Memory Pools&lt;/STRONG&gt; displays address, size, and type information about each memory block allocated in the selected memory pool by the MQX RTOS system or applications.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55754i69C639CDF61C72D8/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_5.png" alt="pastedImage_5.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;I/O Devices&lt;/STRONG&gt; displays name, type and address of I/O Devices used by MQX RTOS application.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55794iF975B6ECA154F2BB/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_6.png" alt="pastedImage_6.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you need to use the MQX Performance Tool like the below image? Unfortunately the MQX Performance Tool is available only in the CodeWarrior IDE.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/55822i7558CF6A977A8FCE/image-size/large?v=v2&amp;amp;px=999" title="pastedImage_8.png" alt="pastedImage_8.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 19:11:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423285#M14098</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-09-09T19:11:17Z</dc:date>
    </item>
    <item>
      <title>Re: MQX TAD call stack in KDS 3</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423286#M14099</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;So in other words the one feature I was asking about isn't available in KDS.&lt;/P&gt;&lt;P&gt;How do you expect the KDS users to debug a specific task?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Up until now we used CodeWarrior for our projects.&lt;/P&gt;&lt;P&gt;The only reason we want to use KDS is to get the USB_v2 working on the K66.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;KDS isn't in production level yet as this is a basic feature for debugging.&lt;/P&gt;&lt;P&gt;Can Freescale provide a working MQX USB_v2 project for CodeWarrior and spare the community the hassle of porting working projects into an IDE that is not yet suitable for real use?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 09 Sep 2015 19:19:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-TAD-call-stack-in-KDS-3/m-p/423286#M14099</guid>
      <dc:creator>ohadbenjamin</dc:creator>
      <dc:date>2015-09-09T19:19:54Z</dc:date>
    </item>
  </channel>
</rss>