<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックMQX 4.2 Cloning Wizard Name Size Limit?</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Cloning-Wizard-Name-Size-Limit/m-p/416518#M13877</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a size limit for the Name of a cloned BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I originally put a fairly long descriptive name for a new BSP - but when I tried to generate the project an error was shown.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example - if I use a Name of: abcdefghijklmnopqrstuvwxyz0123456789&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following error is shown:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:/Users/allwel/AppData/Local/Temp/ocr3A43.tmp/src/core/uproject/internal/_xml_utils.rb:21:in `initialize': No such file or directory @ rb_sysopen - ../../../mqx/examples/context_switch_callback/build/kds/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789 int flash release jlink.launch (Errno::ENOENT)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something shorter - abcdefghijklmnopqrstuvwxyz - will work ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there meant to be a size limit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Allen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 28 Sep 2015 14:20:06 GMT</pubDate>
    <dc:creator>gorakk</dc:creator>
    <dc:date>2015-09-28T14:20:06Z</dc:date>
    <item>
      <title>MQX 4.2 Cloning Wizard Name Size Limit?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Cloning-Wizard-Name-Size-Limit/m-p/416518#M13877</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Is there a size limit for the Name of a cloned BSP?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I originally put a fairly long descriptive name for a new BSP - but when I tried to generate the project an error was shown.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example - if I use a Name of: abcdefghijklmnopqrstuvwxyz0123456789&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The following error is shown:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;C:/Users/allwel/AppData/Local/Temp/ocr3A43.tmp/src/core/uproject/internal/_xml_utils.rb:21:in `initialize': No such file or directory @ rb_sysopen - ../../../mqx/examples/context_switch_callback/build/kds/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789/context_switch_callback_abcdefghijklmnopqrstuvwxyz0123456789 int flash release jlink.launch (Errno::ENOENT)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something shorter - abcdefghijklmnopqrstuvwxyz - will work ok.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there meant to be a size limit?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Allen&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 28 Sep 2015 14:20:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Cloning-Wizard-Name-Size-Limit/m-p/416518#M13877</guid>
      <dc:creator>gorakk</dc:creator>
      <dc:date>2015-09-28T14:20:06Z</dc:date>
    </item>
    <item>
      <title>Re: MQX 4.2 Cloning Wizard Name Size Limit?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Cloning-Wizard-Name-Size-Limit/m-p/416519#M13878</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Allen,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Only 32 characters can be used for the name.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 29 Sep 2015 19:52:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-2-Cloning-Wizard-Name-Size-Limit/m-p/416519#M13878</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-09-29T19:52:49Z</dc:date>
    </item>
  </channel>
</rss>