<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: MQX won't detect UART data present</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-won-t-detect-UART-data-present/m-p/416304#M13876</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry to reply to my own post but I have some new information and I thought it may help someone to help me.&amp;nbsp; I'm not sure this is an MQX issue anymore.&amp;nbsp; In the ISR it is checking for UART2_S1[RDRF] to be set.&amp;nbsp; This is not happening (based on register inspection).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what I gather, the FIFO on UART2 of the K11 is 1 byte in depth.&amp;nbsp; I read the datasheet regarding RWFIFO[RXWATER] setting and how it affects RDRF.&amp;nbsp; I have RXWATER set to 0x01 but the datasheet says this value must be set *less than* the FIFO size for the UART and greater than zero.&amp;nbsp; This would be impossible for a FIFO 1 byte deep.&amp;nbsp; In any case any help is appreciated, I must be mistaken about something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Roy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 18 Nov 2015 00:02:40 GMT</pubDate>
    <dc:creator>snapcount</dc:creator>
    <dc:date>2015-11-18T00:02:40Z</dc:date>
    <item>
      <title>MQX won't detect UART data present</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-won-t-detect-UART-data-present/m-p/416303#M13875</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using the _io_fstatus() function to wait for a byte to show up on ittyc: on a K11 part.&amp;nbsp; I checked the 'D' register and can see the byte is reaching the micro but for some reason the call to _io_fstatus() is never returning true.&amp;nbsp; I have tried this on other UARTs on the same part and it works great.&amp;nbsp; I was wondering if anyone has any ideas or a list of things to check in order for this method to work correctly.&amp;nbsp; This is MQX v4.01.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks in advance!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Roy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 16 Nov 2015 22:20:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-won-t-detect-UART-data-present/m-p/416303#M13875</guid>
      <dc:creator>snapcount</dc:creator>
      <dc:date>2015-11-16T22:20:34Z</dc:date>
    </item>
    <item>
      <title>Re: MQX won't detect UART data present</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-won-t-detect-UART-data-present/m-p/416304#M13876</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry to reply to my own post but I have some new information and I thought it may help someone to help me.&amp;nbsp; I'm not sure this is an MQX issue anymore.&amp;nbsp; In the ISR it is checking for UART2_S1[RDRF] to be set.&amp;nbsp; This is not happening (based on register inspection).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;From what I gather, the FIFO on UART2 of the K11 is 1 byte in depth.&amp;nbsp; I read the datasheet regarding RWFIFO[RXWATER] setting and how it affects RDRF.&amp;nbsp; I have RXWATER set to 0x01 but the datasheet says this value must be set *less than* the FIFO size for the UART and greater than zero.&amp;nbsp; This would be impossible for a FIFO 1 byte deep.&amp;nbsp; In any case any help is appreciated, I must be mistaken about something.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Roy&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 18 Nov 2015 00:02:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-won-t-detect-UART-data-present/m-p/416304#M13876</guid>
      <dc:creator>snapcount</dc:creator>
      <dc:date>2015-11-18T00:02:40Z</dc:date>
    </item>
  </channel>
</rss>