<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Ethernet TCP, delay on send() in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415619#M13852</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is hard to say what could be reason for this behavior.&lt;/P&gt;&lt;P&gt;From your description it seems that packet was dropped at some lower layer of RTCS stack and after that it tries sending it again.&lt;/P&gt;&lt;P&gt;Unfortunately TCP doesn’t have specified any delivery time. It is save protocol, but without any time guarantee.&lt;/P&gt;&lt;P&gt;Did you set OPT_SEND_TIMEOUT to 10ms? Or there missing some zeros?&lt;/P&gt;&lt;P&gt;Could you please place here full wireshark log and describe your network (it is just board-PC connection, or connected to some bigger LAN)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 20 Apr 2015 14:25:32 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2015-04-20T14:25:32Z</dc:date>
    <item>
      <title>Ethernet TCP, delay on send()</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415618#M13851</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello&lt;/P&gt;&lt;P&gt;I'm working on the tower K60n512 with MQX4.1.1.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I init the RTCS like following:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;PRE __default_attr="c++" __jive_macro_name="code" class="jive_text_macro _jivemacro_uid_1429188834338845 jive_macro_code" jivemacro_uid="_1429188834338845" modifiedtitle="true"&gt;
&lt;P&gt;RTCS_Create();&lt;/P&gt;
&lt;P&gt;ENET_initialize(..)&lt;/P&gt;
&lt;P&gt;RTCS_if_add(..)&lt;/P&gt;
&lt;P&gt;RTCS_if_bind(..)&lt;/P&gt;
&lt;P&gt;socket(PF_INET, SOCK_STREAM, 0)&lt;/P&gt;
&lt;P&gt;bind(..)&lt;/P&gt;
&lt;P&gt;listen(..)&lt;/P&gt;
&lt;P&gt;accept(..)&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;setsockopt(.. SOL_TCP, OPT_SEND_NOWAIT, true..) &lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;setsockopt(.. SOL_TCP, OPT_SEND_TIMEOUT, 10..)&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;
&lt;/SPAN&gt;&lt;/P&gt;
&lt;/PRE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Then in cyclic task (5s) I call&lt;BR /&gt;:&lt;/P&gt;&lt;P&gt;send(.., buffer, 5) with buffer is a counter incremented on each send call.&lt;/P&gt;&lt;P&gt;I make toggle a pin just before call send(). After check with oscilloscope, the call to "send()" is really done every exactly each 5s.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I link Ethernet to my laptop with wireshark.&lt;/P&gt;&lt;P&gt;The received frame is not cyclic of 5s. Sometime a delay of 2s can occurs!&lt;/P&gt;&lt;BLOCKQUOTE&gt;
&lt;P&gt;&lt;/P&gt;
&lt;P&gt; 32 14:48:58.708895000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.125 192.168.1.122&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 60 502?60226 [PSH, ACK] Seq=61 Ack=1 Win=4380 Len=5&lt;BR /&gt; 33 14:48:58.926112000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.122 192.168.1.125&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 54 60226?502 [ACK] Seq=1 Ack=66 Win=16428800 Len=0&lt;BR /&gt; &lt;BR /&gt; &lt;BR /&gt; 34 14:49:03.571633000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.125 192.168.1.122&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 60 502?60226 [PSH, ACK] Seq=66 Ack=1 Win=4380 Len=5&lt;BR /&gt; 35 14:49:03.574697000 Dell_02:63:cd IcannIan_a8:01:7d ARP 42 Who has 192.168.1.125? Tell 192.168.1.122&lt;BR /&gt; 36 14:49:03.777609000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.122 192.168.1.125&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 54 60226?502 [ACK] Seq=1 Ack=71 Win=16427520 Len=0&lt;BR /&gt; &lt;BR /&gt; 37 14:49:04.573087000 Dell_02:63:cd IcannIan_a8:01:7d ARP 42 Who has 192.168.1.125? Tell 192.168.1.122&lt;BR /&gt; 38 14:49:04.573365000 IcannIan_a8:01:7 d Dell_02:63:cd ARP 60 192.168.1.125 is at 00:00:5e:a8:01:7d&lt;BR /&gt; &lt;BR /&gt; &lt;BR /&gt; 39 14:49:10.081473000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.125 192.168.1.122&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 60 502?60226 [PSH, ACK] Seq=71 Ack=1 Win=4380 Len=5&lt;BR /&gt; 40 14:49:10.298146000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.122 192.168.1.125&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 54 60226?502 [ACK] Seq=1 Ack=76 Win=16426240 Len=0&lt;BR /&gt; 41 14:49:12.086411000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.125 192.168.1.122&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 60 [TCP Retransmission] 502?60226 [PSH, ACK] Seq=71 Ack=1 Win=4380 Len=5&lt;BR /&gt; 42 14:49:12.086479000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.122 192.168.1.125&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 54 [TCP Dup ACK 40#1] 60226?502 [ACK] Seq=1 Ack=76 Win=16426240 Len=0&lt;BR /&gt; &lt;BR /&gt; 43 14:49:13.571434000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.125 192.168.1.122&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 60 502?60226 [PSH, ACK] Seq=76 Ack=1 Win=4380 Len=5&lt;BR /&gt; 44 14:49:13.777004000&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 192.168.1.122 192.168.1.125&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; TCP 54 60226?502 [ACK] Seq=1 Ack=81 Win=16424960 Len=0&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;/BLOCKQUOTE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Twrk60 has ip = 192.168.1.125&lt;/P&gt;&lt;P&gt;Laptop has ip = 192.168.1.122&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I see a good frame #32 and #33 (Request from tower/ Ack from laptop)&lt;/P&gt;&lt;P&gt;Same for #34 and 36&lt;/P&gt;&lt;P&gt;But the #39 should arrive at time 14:49:08.xxxx ut arrive at 14:49:10.xxxx so there are in late! (very late! 1s...)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#43/#44 has the good time.&lt;/P&gt;&lt;P&gt;I don't understand why this frame is send with this late,&amp;nbsp; why Retransmission is done 2s later? (#41)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For my application, I would have to send frame with a very speed (every 10 or 100ms...) but with simple test (one frame every 5s) sometime some frame are very delayed!.&lt;/P&gt;&lt;P&gt;Have you an idea why?&lt;/P&gt;&lt;P&gt;Note: nothing else is done on K60. Only Ethernet load the µC..:smileyplain:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 16 Apr 2015 13:11:19 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415618#M13851</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2015-04-16T13:11:19Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet TCP, delay on send()</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415619#M13852</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It is hard to say what could be reason for this behavior.&lt;/P&gt;&lt;P&gt;From your description it seems that packet was dropped at some lower layer of RTCS stack and after that it tries sending it again.&lt;/P&gt;&lt;P&gt;Unfortunately TCP doesn’t have specified any delivery time. It is save protocol, but without any time guarantee.&lt;/P&gt;&lt;P&gt;Did you set OPT_SEND_TIMEOUT to 10ms? Or there missing some zeros?&lt;/P&gt;&lt;P&gt;Could you please place here full wireshark log and describe your network (it is just board-PC connection, or connected to some bigger LAN)?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 14:25:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415619#M13852</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-04-20T14:25:32Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet TCP, delay on send()</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415620#M13853</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;OPT_SEND_TIMEOUT was set with 10ms.&lt;/P&gt;&lt;P&gt;But problem occurs with or without this setting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I need to do some test with my computer software (Docklight)&lt;/P&gt;&lt;P&gt;May be some time this soft put in buffer data to send and received to really sent its or display received...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But With wireshark, I see many time a realy response with very big latence time.&lt;/P&gt;&lt;P&gt;I need to reproduce exactly and with a sure maner the problem.&lt;/P&gt;&lt;P&gt;I will back to you&lt;/P&gt;&lt;P&gt;:smileywink:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 20 Apr 2015 14:48:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415620#M13853</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2015-04-20T14:48:56Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet TCP, delay on send()</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415621#M13854</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;TO close this point, it was my PC tool which wait some data to send a bigger packet.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After test, the response time is ok!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Jan 2016 06:39:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-TCP-delay-on-send/m-p/415621#M13854</guid>
      <dc:creator>arnogir</dc:creator>
      <dc:date>2016-01-05T06:39:00Z</dc:date>
    </item>
  </channel>
</rss>