<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic twrk65f180m bsp - flash size in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/twrk65f180m-bsp-flash-size/m-p/409958#M13710</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;I am trying to port my system to use the K66 with 2048MB flash, and I am using TWRK65F180M as a reference (as I was told K65 is a super-set compatible with K66).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;Accroding to the documentation, the tower includes MK65FN2M0VMI18, which includes &lt;SPAN style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;2048MB flash as well.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 12px; font-family: arial, sans-serif;"&gt;However, when I look at the &lt;STRONG&gt;&lt;EM&gt;mqx\source\bsp\twrk65f180m\twrk65f180m.h&lt;/EM&gt;&lt;/STRONG&gt; files I see that the flash size is defined as:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BSP_INTERNAL_FLASH_BASE&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000000&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#define BSP_INTERNAL_FLASH_SIZE&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00100000&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;#define BSP_INTERNAL_FLASH_SECTOR_SIZE 0x1000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, if the chip has 2MB of flash - why the BSP defines only half of it (0x100000)? What am I missing here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Jul 2015 13:52:42 GMT</pubDate>
    <dc:creator>panpwr</dc:creator>
    <dc:date>2015-07-14T13:52:42Z</dc:date>
    <item>
      <title>twrk65f180m bsp - flash size</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/twrk65f180m-bsp-flash-size/m-p/409958#M13710</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;Hello,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;I am trying to port my system to use the K66 with 2048MB flash, and I am using TWRK65F180M as a reference (as I was told K65 is a super-set compatible with K66).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;Accroding to the documentation, the tower includes MK65FN2M0VMI18, which includes &lt;SPAN style="color: #51626f; font-family: arial, sans-serif; font-size: 12px;"&gt;2048MB flash as well.&lt;/SPAN&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #51626f; font-size: 12px; font-family: arial, sans-serif;"&gt;However, when I look at the &lt;STRONG&gt;&lt;EM&gt;mqx\source\bsp\twrk65f180m\twrk65f180m.h&lt;/EM&gt;&lt;/STRONG&gt; files I see that the flash size is defined as:&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;#define BSP_INTERNAL_FLASH_BASE&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00000000&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;#define BSP_INTERNAL_FLASH_SIZE&amp;nbsp;&amp;nbsp;&amp;nbsp; 0x00100000&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;#define BSP_INTERNAL_FLASH_SECTOR_SIZE 0x1000&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So, if the chip has 2MB of flash - why the BSP defines only half of it (0x100000)? What am I missing here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Lior.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Jul 2015 13:52:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/twrk65f180m-bsp-flash-size/m-p/409958#M13710</guid>
      <dc:creator>panpwr</dc:creator>
      <dc:date>2015-07-14T13:52:42Z</dc:date>
    </item>
    <item>
      <title>Re: twrk65f180m bsp - flash size</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/twrk65f180m-bsp-flash-size/m-p/409959#M13711</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Lior,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Yes, you are right. You can modify this value.&lt;/P&gt;&lt;P&gt;The linker file has the correct values, you can check it; the location of the linker file is at&lt;BR /&gt; &amp;lt;Freescale MQX 4.2&amp;gt;\mqx\source\bsp\&amp;lt;platform&amp;gt;\cw\*.ld&lt;/P&gt;&lt;P&gt;Thank you for your feedback.&lt;/P&gt;&lt;P&gt;Have a nice day !!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;/P&gt;&lt;P&gt;Sol &lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Jul 2015 15:49:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/twrk65f180m-bsp-flash-size/m-p/409959#M13711</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-07-15T15:49:46Z</dc:date>
    </item>
  </channel>
</rss>