<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: esdhc slow write speed with SD card</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/esdhc-slow-write-speed-with-SD-card/m-p/403524#M13520</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using a freescale board? &lt;/P&gt;&lt;P&gt;Did you test using a sample code? &lt;/P&gt;&lt;P&gt;Could you please try using the SDCARD example, it is located at the path: C:\Freescale\Freescale_MQX_4_2\mfs\examples\sdcard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 10 Aug 2015 17:52:20 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2015-08-10T17:52:20Z</dc:date>
    <item>
      <title>esdhc slow write speed with SD card</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/esdhc-slow-write-speed-with-SD-card/m-p/403522#M13518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello - &lt;/P&gt;&lt;P&gt;I have a design using a K60F120 part and an SD card with the esdhc driver.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The driver is configured for a 50 Mhz clock to the sd card, and 4 bit SPI mode. The OS was just updated to to MQX4.2, and MFS is used for the filesystem on the SD card.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; I am seeing very slow write speeds to the SD card. FTP writes are roughly 400KBytes/Sec. The MFS swt test utility, when benchmarked with a hardware based millisecond counter I have in the design takes about 32 milliseconds to write each of its 10K files, with performance best at the 512 Byte size.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Has anyone seen similar speeds, and is there a way to speed things up?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 01 Aug 2015 23:14:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/esdhc-slow-write-speed-with-SD-card/m-p/403522#M13518</guid>
      <dc:creator>jlevie</dc:creator>
      <dc:date>2015-08-01T23:14:15Z</dc:date>
    </item>
    <item>
      <title>Re: esdhc slow write speed with SD card</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/esdhc-slow-write-speed-with-SD-card/m-p/403523#M13519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Have you confirmed that the clock is running at 50MHz?&lt;/P&gt;&lt;P&gt;What type of card are you using?&lt;/P&gt;&lt;P&gt;Also, it could be task or interrupt priority issue.&amp;nbsp; See this post &lt;A href="https://community.nxp.com/message/444035"&gt;SDHC Interrupt&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 06 Aug 2015 17:21:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/esdhc-slow-write-speed-with-SD-card/m-p/403523#M13519</guid>
      <dc:creator>bonzo</dc:creator>
      <dc:date>2015-08-06T17:21:00Z</dc:date>
    </item>
    <item>
      <title>Re: esdhc slow write speed with SD card</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/esdhc-slow-write-speed-with-SD-card/m-p/403524#M13520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Jeff,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Are you using a freescale board? &lt;/P&gt;&lt;P&gt;Did you test using a sample code? &lt;/P&gt;&lt;P&gt;Could you please try using the SDCARD example, it is located at the path: C:\Freescale\Freescale_MQX_4_2\mfs\examples\sdcard&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Aug 2015 17:52:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/esdhc-slow-write-speed-with-SD-card/m-p/403524#M13520</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-08-10T17:52:20Z</dc:date>
    </item>
  </channel>
</rss>