<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: How to create a set MQX libs of  for a custom board in CW 10.6/MQX 4.1.1 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-create-a-set-MQX-libs-of-for-a-custom-board-in-CW-10-6/m-p/395421#M13277</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for all the help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I figured out to use the BSP Cloning Wizard after uninstalling my existing MQX 4.1 installation and reinstalling all of MQX 4.1.1. Then I copied the missing globals_full.yml file into the C:\Freescale\Freescale_MQX_4_1\tools\generator\records\mqx_records directory from the 4.0 installation I had backed up on another drive. Then I could follow the procedure in the MQX_BSP_Cloning_Wizard_Getting_Started document and create a new bsp clone as a starting point for my bsp. The build_libs.wsd file would not install the libs because workingsets.xsd file is nowhere to be found, but the old install existing project steps do work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll be sure and come back here for more help the next time I have an issue.&lt;/P&gt;&lt;P&gt;:smileylaugh:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 14 Apr 2015 17:29:32 GMT</pubDate>
    <dc:creator>jhmrd</dc:creator>
    <dc:date>2015-04-14T17:29:32Z</dc:date>
    <item>
      <title>How to create a set MQX libs of  for a custom board in CW 10.6/MQX 4.1.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-create-a-set-MQX-libs-of-for-a-custom-board-in-CW-10-6/m-p/395420#M13276</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am trying to update a completed project built with MQX 4.0 and CW 10.4 to the latest CW 10.6 and MQX 4.1.1. To start with, I imported the example twrk60n512 MQX library projects as I have always done with CW 10.4. But building them did not generate code. So I tried copy and paste of the .WSD file into the project window and it caused all the library projects to be imported and then they ran.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have always created MQX library projects for my custom hardware by manually editing the XML .project and .cproject files. But now there is a .WSD file, which is an XML file as well. But the .WSD files have no line separators, not linux or windows format. So editing those will be a real pain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How are we supposed to create new MQX lib projects in the wonderful new world of CW 10.6?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Apr 2015 22:32:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-create-a-set-MQX-libs-of-for-a-custom-board-in-CW-10-6/m-p/395420#M13276</guid>
      <dc:creator>jhmrd</dc:creator>
      <dc:date>2015-04-09T22:32:41Z</dc:date>
    </item>
    <item>
      <title>Re: How to create a set MQX libs of  for a custom board in CW 10.6/MQX 4.1.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-create-a-set-MQX-libs-of-for-a-custom-board-in-CW-10-6/m-p/395421#M13277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for all the help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I figured out to use the BSP Cloning Wizard after uninstalling my existing MQX 4.1 installation and reinstalling all of MQX 4.1.1. Then I copied the missing globals_full.yml file into the C:\Freescale\Freescale_MQX_4_1\tools\generator\records\mqx_records directory from the 4.0 installation I had backed up on another drive. Then I could follow the procedure in the MQX_BSP_Cloning_Wizard_Getting_Started document and create a new bsp clone as a starting point for my bsp. The build_libs.wsd file would not install the libs because workingsets.xsd file is nowhere to be found, but the old install existing project steps do work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'll be sure and come back here for more help the next time I have an issue.&lt;/P&gt;&lt;P&gt;:smileylaugh:&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 14 Apr 2015 17:29:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-create-a-set-MQX-libs-of-for-a-custom-board-in-CW-10-6/m-p/395421#M13277</guid>
      <dc:creator>jhmrd</dc:creator>
      <dc:date>2015-04-14T17:29:32Z</dc:date>
    </item>
    <item>
      <title>Re: How to create a set MQX libs of  for a custom board in CW 10.6/MQX 4.1.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-create-a-set-MQX-libs-of-for-a-custom-board-in-CW-10-6/m-p/395422#M13278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Yes, globals_full.yml was renamed to globals.yml. It is known bug and this bug has solution in &lt;A href="https://freescale.flexnetoperations.com/control/frse/download?agree=Accept&amp;amp;element=5905481"&gt;Cloning wizard patch for MQX 4.1.1&lt;/A&gt; installation. This solves also few additional issues in this tool.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;About editing wsd files)&lt;/P&gt;&lt;P&gt;I would like to recommend download and install &lt;A href="http://notepad-plus-plus.org/"&gt;Notepad++ editor&lt;/A&gt; (free tool).&lt;/P&gt;&lt;P&gt;After that go to menu-Plugins-Plugin Manager-Show Plugin manager-and select XML tools.&lt;/P&gt;&lt;P&gt;After that go to menu-Plugins-XML tools-Pretty prints (XML only-with line breaks).&lt;/P&gt;&lt;P&gt;Now you can simply edit this file.&lt;/P&gt;&lt;P&gt;When you finish your modifications, you can Linearize XML file back and save in short format.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 15 Apr 2015 11:40:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/How-to-create-a-set-MQX-libs-of-for-a-custom-board-in-CW-10-6/m-p/395422#M13278</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-04-15T11:40:27Z</dc:date>
    </item>
  </channel>
</rss>