<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: USB_v2 Error K64</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393692#M13203</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;up&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 27 Oct 2015 07:54:42 GMT</pubDate>
    <dc:creator>Microfelix</dc:creator>
    <dc:date>2015-10-27T07:54:42Z</dc:date>
    <item>
      <title>USB_v2 Error K64</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393689#M13200</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;I compiled the project "host_msd_fatfs_twrk64f120m"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX 4.2&lt;/P&gt;&lt;P&gt;KDS 3.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;After compiling libraries and related project, I get an error on the shell closing Filesystem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Library:&lt;/P&gt;&lt;P&gt;bsp.a&lt;/P&gt;&lt;P&gt;psp.a&lt;/P&gt;&lt;P&gt;shell.a&lt;/P&gt;&lt;P&gt;msf.a&lt;/P&gt;&lt;P&gt;libusbh_mqx.a&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;can you help me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/57423i00044F850962BF3C/image-size/large?v=v2&amp;amp;px=999" title="error_usb_v2.png" alt="error_usb_v2.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 15:02:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393689#M13200</guid>
      <dc:creator>Microfelix</dc:creator>
      <dc:date>2015-09-18T15:02:29Z</dc:date>
    </item>
    <item>
      <title>Re: USB_v2 Error K64</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393690#M13201</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Maurizio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Unfortunately I cannot to reproduce your issue. If you are using the Twr-k64f12m board please check the jumper configurations.&lt;/P&gt;&lt;P&gt;• For USB Host mode, use onboard J17 Micro USB connector and jumpers set to default settings. Connect the J2 (K20&lt;/P&gt;&lt;P&gt;DEBUG) Mini USB to the PC to enable power for the USB Host.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition please confirm that the ID pin is grounded.&lt;/P&gt;&lt;P&gt;The ID pin is for detecting if the USB port is Host or Device. When a port is Host, the ID pin should be grounded. If the port is Device, the ID pin should remain floating.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt;Sol &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 18 Sep 2015 21:37:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393690#M13201</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-09-18T21:37:40Z</dc:date>
    </item>
    <item>
      <title>Re: USB_v2 Error K64</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393691#M13202</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am not using the TWR.&lt;/P&gt;&lt;P&gt;I'm using "MK64FN1M0VLL12" smaller&amp;nbsp; (only 100 pins)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;For example, the pin PTE12, pin ID, does not exist.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This problem I had not before using MQX 4.1 and CodeWarrior.&lt;/P&gt;&lt;P&gt;But now using KDS, with USB_v2, I have this problem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;There are settings to change the library USBH?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 21 Sep 2015 07:09:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393691#M13202</guid>
      <dc:creator>Microfelix</dc:creator>
      <dc:date>2015-09-21T07:09:20Z</dc:date>
    </item>
    <item>
      <title>Re: USB_v2 Error K64</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393692#M13203</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;up&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 27 Oct 2015 07:54:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-v2-Error-K64/m-p/393692#M13203</guid>
      <dc:creator>Microfelix</dc:creator>
      <dc:date>2015-10-27T07:54:42Z</dc:date>
    </item>
  </channel>
</rss>