<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Forcing 10 Mbps Ethernet Connection</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Forcing-10-Mbps-Ethernet-Connection/m-p/161620#M1286</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a parameter where I can force RTCS to establish a 10 Mbps (10Base-T) even if the network supports 100 Mbps connections (100Base-TX)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, if I do so, are there 100Base-TX only networks? I suppose a 10Base-T should work in any network, correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need this in order to save power in my end-device&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Nov 2010 01:43:18 GMT</pubDate>
    <dc:creator>rdazcal</dc:creator>
    <dc:date>2010-11-10T01:43:18Z</dc:date>
    <item>
      <title>Forcing 10 Mbps Ethernet Connection</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Forcing-10-Mbps-Ethernet-Connection/m-p/161620#M1286</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Greetings,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Is there a parameter where I can force RTCS to establish a 10 Mbps (10Base-T) even if the network supports 100 Mbps connections (100Base-TX)?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Also, if I do so, are there 100Base-TX only networks? I suppose a 10Base-T should work in any network, correct?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I need this in order to save power in my end-device&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Nov 2010 01:43:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Forcing-10-Mbps-Ethernet-Connection/m-p/161620#M1286</guid>
      <dc:creator>rdazcal</dc:creator>
      <dc:date>2010-11-10T01:43:18Z</dc:date>
    </item>
    <item>
      <title>Re: Forcing 10 Mbps Ethernet Connection</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Forcing-10-Mbps-Ethernet-Connection/m-p/161621#M1287</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;If anyone is interested, here is a link for the solution in another thread:&amp;nbsp;&lt;A __default_attr="72070" class="jive_macro jive_macro_thread default_title" href="https://community.freescale.com/thread/72070" jivemacro="thread" title="https://community.freescale.com/thread/72070"&gt;https://community.freescale.com/thread/72070&lt;/A&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 22 Nov 2010 20:57:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Forcing-10-Mbps-Ethernet-Connection/m-p/161621#M1287</guid>
      <dc:creator>rdazcal</dc:creator>
      <dc:date>2010-11-22T20:57:25Z</dc:date>
    </item>
  </channel>
</rss>