<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: SPI baud rate</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-baud-rate/m-p/385127#M12833</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you sure, that bus clock at your board has right value?&lt;/P&gt;&lt;P&gt;I suppose that you used twrvf65gs10 BSP as base for your own BSP. Correct?&lt;/P&gt;&lt;P&gt;Unfortunately I was not able found value of external crystal/resonator at pcm052 board.&lt;/P&gt;&lt;P&gt;Main oscillator at twrvf65gs10 has clock 24MHz. Ratio between set and generated baudrate is approximately 2.5~2.6. This leads to 62MHz crystal at your board or some different clock settings. Is it possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 17 Mar 2015 14:32:59 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2015-03-17T14:32:59Z</dc:date>
    <item>
      <title>SPI baud rate</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-baud-rate/m-p/385126#M12832</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I tested the MQX SPI example in folder MQX/examples/spi. I used the Vybrid pcm052 board / M4 processor. I changed the baud rate to 1000. I read back the baud rate, it returned 1017 ... no problem here.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On the scope, I measure a clock rate of 2600 Hz which gives 333 byte/s (1/2600 * 8bit). I'm a little bit confused.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anybody explain me why ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 13 Mar 2015 18:19:32 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-baud-rate/m-p/385126#M12832</guid>
      <dc:creator>hardwaredevelop</dc:creator>
      <dc:date>2015-03-13T18:19:32Z</dc:date>
    </item>
    <item>
      <title>Re: SPI baud rate</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-baud-rate/m-p/385127#M12833</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Are you sure, that bus clock at your board has right value?&lt;/P&gt;&lt;P&gt;I suppose that you used twrvf65gs10 BSP as base for your own BSP. Correct?&lt;/P&gt;&lt;P&gt;Unfortunately I was not able found value of external crystal/resonator at pcm052 board.&lt;/P&gt;&lt;P&gt;Main oscillator at twrvf65gs10 has clock 24MHz. Ratio between set and generated baudrate is approximately 2.5~2.6. This leads to 62MHz crystal at your board or some different clock settings. Is it possible?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 17 Mar 2015 14:32:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/SPI-baud-rate/m-p/385127#M12833</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-03-17T14:32:59Z</dc:date>
    </item>
  </channel>
</rss>