<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: I2S/SAI defines missing</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383240#M12763</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the feedback!&lt;/P&gt;&lt;P&gt;I'm using CW10.3, MQX4.0 and started from a bsp twr60F120. The device is a MK60FN1M0VLQ12.&lt;/P&gt;&lt;P&gt;I see that the file sai.h is included which is located in "C:\Freescale\Freescale_MQX_4_0\mqx\source\io\sai"&lt;/P&gt;&lt;P&gt;This file contains the structure below which lacks SIZE, IN_BUFFER, and OUT_BUFFER. I see that it is present in the sai.h of MQX 4.1.&lt;/P&gt;&lt;P&gt;Does it mean that I have to switch to 4.1 (which might be a small risk for the existing project) or can I just copy the 4.1 file to the 4.0 directory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;typedef struct i2s_statistics_struct&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of SAI interrupts so far */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 INTERRUPTS;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* FIFO error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 FIFO_ERROR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* FIFO sync error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 BUFFER_ERROR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of valid bytes received (not dummy receives) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 RX_PACKETS;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of valid bytes transmitted (not dummy transmits) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 TX_PACKETS;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of bytes currently read or wrote */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 PACKETS_PROCESSED;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of bytes currently buffered */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 PACKETS_QUEUED;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of bytes requested for reading or writing */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 PACKETS_REQUESTED;&lt;/P&gt;&lt;P&gt;} I2S_STATISTICS_STRUCT, _PTR_ I2S_STATISTICS_STRUCT_PTR;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Dec 2014 09:22:04 GMT</pubDate>
    <dc:creator>degry</dc:creator>
    <dc:date>2014-12-03T09:22:04Z</dc:date>
    <item>
      <title>I2S/SAI defines missing</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383237#M12760</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm trying to add I2S/SAI functionality to an existing project. I started from the sai_dma_demo from MQX 4.1 but I get these errors:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;'SIZE' is not a member of class 'struct i2s_statistics_struct'&lt;/P&gt;&lt;/TD&gt;&lt;TD&gt;K60_Run&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;C/C++ Problem&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;'IN_BUFFER' is not a member of class 'struct i2s_statistics_struct'&lt;/TD&gt;&lt;TD&gt;sh_audio.c&lt;/TD&gt;&lt;TD&gt;C/C++ Problem&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;'OUT_BUFFER' is not a member of class 'struct i2s_statistics_struct'&lt;/TD&gt;&lt;TD&gt;sh_audio.c&lt;/TD&gt;&lt;TD&gt;C/C++ Problem&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;undefined identifier 'IO_IOCTL_I2S_START_RX'&lt;/TD&gt;&lt;TD&gt;sh_audio.c&lt;/TD&gt;&lt;TD&gt;/K60_Run/Sources/SourceFiles&lt;/TD&gt;&lt;TD&gt;line 445&lt;/TD&gt;&lt;TD&gt;C/C++ Problem&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;undefined identifier 'IO_IOCTL_I2S_UPDATE_RX_STATUS'&lt;/TD&gt;&lt;TD&gt;sh_audio.c&lt;/TD&gt;&lt;TD&gt;/K60_Run/Sources/SourceFiles&lt;/TD&gt;&lt;TD&gt;line 471&lt;/TD&gt;&lt;TD&gt;C/C++ Problem&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;undefined identifier 'IO_IOCTL_I2S_WAIT_RX_EVENT'&lt;/TD&gt;&lt;TD&gt;sh_audio.c&lt;/TD&gt;&lt;TD&gt;/K60_Run/Sources/SourceFiles&lt;/TD&gt;&lt;TD&gt;line 454&lt;/TD&gt;&lt;TD&gt;C/C++ Problem&lt;/TD&gt;&lt;/TR&gt;&lt;TR&gt;&lt;TD&gt;undefined identifier 'IO_IOCTL_I2S_START_TX'&lt;/TD&gt;&lt;TD&gt;&lt;/TD&gt;&lt;TD&gt;sh_audio.c&lt;/TD&gt;&lt;TD&gt;/K60_Run/Sources/SourceFiles&lt;/TD&gt;&lt;TD&gt;line 445&lt;/TD&gt;&lt;TD&gt;C/C++ Problem&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;undefined identifier 'IO_IOCTL&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;undefined identifier 'IO_IOCTL_I2S_WAIT_TX_EVENT'&lt;/TD&gt;&lt;TD&gt;sh_audio.c&lt;/TD&gt;&lt;TD&gt;/K60_Run/Sources/SourceFiles&lt;/TD&gt;&lt;TD&gt;line 454&lt;/TD&gt;&lt;TD&gt;C/C++ Problem&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using an existing BSP where I enabled I2S.&lt;/P&gt;&lt;P&gt;Any idea what I'm missing? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 16:22:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383237#M12760</guid>
      <dc:creator>degry</dc:creator>
      <dc:date>2014-12-01T16:22:14Z</dc:date>
    </item>
    <item>
      <title>Re: I2S/SAI defines missing</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383238#M12761</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;struct i2s_statistics_struct is defined in sai.h.&amp;nbsp; When I look at my copy it contains SIZE, IN_BUFFER, and OUT_BUFFER.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;You mentioned that you have an existing BSP where you enabled I2S.&amp;nbsp; I think the example makes use of the SAI driver.&amp;nbsp; Did you set BSPCFG_ENABLE_SAI to true in user_config.h?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 01 Dec 2014 22:07:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383238#M12761</guid>
      <dc:creator>pbanta</dc:creator>
      <dc:date>2014-12-01T22:07:51Z</dc:date>
    </item>
    <item>
      <title>Re: I2S/SAI defines missing</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383239#M12762</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi patrick degry,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please double check that you enable in the user_config.h the below line&lt;/P&gt;&lt;TABLE&gt;&lt;TBODY&gt;&lt;TR&gt;&lt;TD&gt;#define BSPCFG_ENABLE_SAI&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/TD&gt;&lt;TD&gt;1&lt;/TD&gt;&lt;/TR&gt;&lt;/TBODY&gt;&lt;/TABLE&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In addition please build the BSP, PSP and MFS libraries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please let me know if this helps. &lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol &lt;BR /&gt; &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2014 00:31:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383239#M12762</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-12-02T00:31:40Z</dc:date>
    </item>
    <item>
      <title>Re: I2S/SAI defines missing</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383240#M12763</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the feedback!&lt;/P&gt;&lt;P&gt;I'm using CW10.3, MQX4.0 and started from a bsp twr60F120. The device is a MK60FN1M0VLQ12.&lt;/P&gt;&lt;P&gt;I see that the file sai.h is included which is located in "C:\Freescale\Freescale_MQX_4_0\mqx\source\io\sai"&lt;/P&gt;&lt;P&gt;This file contains the structure below which lacks SIZE, IN_BUFFER, and OUT_BUFFER. I see that it is present in the sai.h of MQX 4.1.&lt;/P&gt;&lt;P&gt;Does it mean that I have to switch to 4.1 (which might be a small risk for the existing project) or can I just copy the 4.1 file to the 4.0 directory?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;typedef struct i2s_statistics_struct&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of SAI interrupts so far */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 INTERRUPTS;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* FIFO error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 FIFO_ERROR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* FIFO sync error */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 BUFFER_ERROR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of valid bytes received (not dummy receives) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 RX_PACKETS;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of valid bytes transmitted (not dummy transmits) */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 TX_PACKETS;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of bytes currently read or wrote */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 PACKETS_PROCESSED;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of bytes currently buffered */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 PACKETS_QUEUED;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Number of bytes requested for reading or writing */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint_32 PACKETS_REQUESTED;&lt;/P&gt;&lt;P&gt;} I2S_STATISTICS_STRUCT, _PTR_ I2S_STATISTICS_STRUCT_PTR;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Dec 2014 09:22:04 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/I2S-SAI-defines-missing/m-p/383240#M12763</guid>
      <dc:creator>degry</dc:creator>
      <dc:date>2014-12-03T09:22:04Z</dc:date>
    </item>
  </channel>
</rss>