<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic In the CDC Ethernet over USB code there appears to be an IP address in the code, why? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/In-the-CDC-Ethernet-over-USB-code-there-appears-to-be-an-IP/m-p/380487#M12695</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm thinking along the lines that the CDC Ethernet over USB (cdc_vnic_twrk70f120m) code should only pass traffic from USB to Ethernet and back and have no need for an IP address.&amp;nbsp; But in the file "virtuial_nic_enet.h" there appears to be an IP address:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Line 65 (or there abouts): &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define ENET_IPADDR&amp;nbsp; IPADDR(169,254,3,3)/* Default IP Address */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this serve a purpose?&amp;nbsp; Perhaps if I understand this I could better understand how the Freescale example works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 28 Nov 2014 15:58:41 GMT</pubDate>
    <dc:creator>rickstuart</dc:creator>
    <dc:date>2014-11-28T15:58:41Z</dc:date>
    <item>
      <title>In the CDC Ethernet over USB code there appears to be an IP address in the code, why?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/In-the-CDC-Ethernet-over-USB-code-there-appears-to-be-an-IP/m-p/380487#M12695</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm thinking along the lines that the CDC Ethernet over USB (cdc_vnic_twrk70f120m) code should only pass traffic from USB to Ethernet and back and have no need for an IP address.&amp;nbsp; But in the file "virtuial_nic_enet.h" there appears to be an IP address:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;On Line 65 (or there abouts): &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define ENET_IPADDR&amp;nbsp; IPADDR(169,254,3,3)/* Default IP Address */&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does this serve a purpose?&amp;nbsp; Perhaps if I understand this I could better understand how the Freescale example works.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 28 Nov 2014 15:58:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/In-the-CDC-Ethernet-over-USB-code-there-appears-to-be-an-IP/m-p/380487#M12695</guid>
      <dc:creator>rickstuart</dc:creator>
      <dc:date>2014-11-28T15:58:41Z</dc:date>
    </item>
  </channel>
</rss>