<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: Ethernet Communication using TFTP protocol</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-Communication-using-TFTP-protocol/m-p/375807#M12506</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Utsavi Kalpesh Bharuchwala,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you consider using FTP protocol (FTP server) ? There exists already example for this in MQX 4.0:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;c:\Freescale\Freescale_MQX_4_0\rtcs\examples\shell\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the demo uses ramdisk at a: as the root directory. You can open an MFS device on SD card driver according to mfs sdcard demo. "ftpd start" command on shell starts the FTP server in the demo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 09 Oct 2014 14:34:01 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2014-10-09T14:34:01Z</dc:date>
    <item>
      <title>Ethernet Communication using TFTP protocol</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-Communication-using-TFTP-protocol/m-p/375806#M12505</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working on CodeWarrior v10.2 and MQX v4.0&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In my project I need to send the file say Data.txt from Pc to module(TWR-K60D100M) using TFTP protocol via Ethernet Communication.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also module will send this file to Pc whenever Pc need it.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have tried Ethernet Communication using HTTP protocol,but not send the whole file yet using TFTP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anybody tell me How can I do Ethernet Communication to send/receive file using TFTP???&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 08 Oct 2014 09:21:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-Communication-using-TFTP-protocol/m-p/375806#M12505</guid>
      <dc:creator>utsavikalpesh</dc:creator>
      <dc:date>2014-10-08T09:21:56Z</dc:date>
    </item>
    <item>
      <title>Re: Ethernet Communication using TFTP protocol</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-Communication-using-TFTP-protocol/m-p/375807#M12506</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Utsavi Kalpesh Bharuchwala,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Did you consider using FTP protocol (FTP server) ? There exists already example for this in MQX 4.0:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;c:\Freescale\Freescale_MQX_4_0\rtcs\examples\shell\&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;the demo uses ramdisk at a: as the root directory. You can open an MFS device on SD card driver according to mfs sdcard demo. "ftpd start" command on shell starts the FTP server in the demo.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 09 Oct 2014 14:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Ethernet-Communication-using-TFTP-protocol/m-p/375807#M12506</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-10-09T14:34:01Z</dc:date>
    </item>
  </channel>
</rss>