<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic building RTCS Lib without ethernet support for MK22 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/building-RTCS-Lib-without-ethernet-support-for-MK22/m-p/372077#M12280</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a MK22f120 trying to build RTCS . I don't need the Ethernet port because I will be setting up a PPP connection over a cellular module but need the support of the TCP/IP stack. is there a define that I can enable/disable so that I can build because the MK22 does not support Ethernet&lt;/P&gt;&lt;P&gt;so far I have not found one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 23 Dec 2014 18:38:28 GMT</pubDate>
    <dc:creator>Donsnook</dc:creator>
    <dc:date>2014-12-23T18:38:28Z</dc:date>
    <item>
      <title>building RTCS Lib without ethernet support for MK22</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/building-RTCS-Lib-without-ethernet-support-for-MK22/m-p/372077#M12280</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm using a MK22f120 trying to build RTCS . I don't need the Ethernet port because I will be setting up a PPP connection over a cellular module but need the support of the TCP/IP stack. is there a define that I can enable/disable so that I can build because the MK22 does not support Ethernet&lt;/P&gt;&lt;P&gt;so far I have not found one.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 23 Dec 2014 18:38:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/building-RTCS-Lib-without-ethernet-support-for-MK22/m-p/372077#M12280</guid>
      <dc:creator>Donsnook</dc:creator>
      <dc:date>2014-12-23T18:38:28Z</dc:date>
    </item>
    <item>
      <title>Re: building RTCS Lib without ethernet support for MK22</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/building-RTCS-Lib-without-ethernet-support-for-MK22/m-p/372078#M12281</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I was able to build with a couple of #ifndef in RTC.h and RTC_IF.h so that don't include any enet*.h &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Dec 2014 15:41:42 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/building-RTCS-Lib-without-ethernet-support-for-MK22/m-p/372078#M12281</guid>
      <dc:creator>Donsnook</dc:creator>
      <dc:date>2014-12-24T15:41:42Z</dc:date>
    </item>
    <item>
      <title>Re: building RTCS Lib without ethernet support for MK22</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/building-RTCS-Lib-without-ethernet-support-for-MK22/m-p/372079#M12282</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think the enet driver was excluded in source code if you are using BSP for TWR-K22F120M.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 14 Jan 2015 07:39:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/building-RTCS-Lib-without-ethernet-support-for-MK22/m-p/372079#M12282</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2015-01-14T07:39:16Z</dc:date>
    </item>
  </channel>
</rss>