<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: Flash update sometimes not working</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-update-sometimes-not-working/m-p/372043#M12278</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;More information.&lt;/P&gt;&lt;P&gt;The only relevant hardware difference between the working and non-working boards is a sensor device on I2C0 at address 0x30.&lt;/P&gt;&lt;P&gt;This device comes in 8 flavors based on I2C address, so I have a static const []... table (written in Flash) which is looked up when the I2C scan routine comes across any address that does not give a NACK.&amp;nbsp; So I have 8 entries in my table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems the Flash erase fails only when &lt;SPAN style="font-size: 13.6000003814697px;"&gt;I have 3 or more entries in the table (not commented out) *and* I scan address 0x30&lt;/SPAN&gt;.&amp;nbsp; The I2C scan and the Flash routines have *nothing* in common.&amp;nbsp; The I2C scan happen during initialization, and the flash routine happens eons later during normal operation.&amp;nbsp; If I skip address 0x30, or if I have 2 or fewer entries in the table (whether they match address 0x30 or not) then the Flash erase and subsequent rewrite works correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It also turns out my "working" board fails under seemingly opposite conditions of the failing board: the "working" board (which doesn't even have the sensor device at 0x30) fails if I skip scanning address 0x30 or if I comment out several of the entries in the table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also noticed under these funny conditions that Jlink-Commander is also unable to erase the device.&amp;nbsp; I have to do "kinetis unlock" for the Jlink-Commander to erase the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it seems that somehow the Flash is getting locked, and it seems somehow related to the I2C scanning, which doesn't make any sense at all.&lt;/P&gt;&lt;P&gt;It perhaps has something to do instead with how the table is written in the Flash by the linker, but that also doesn't make any sense, nor does it make any sense that two boards, which only differ in there being a device hanging on I2C0 address 0x30, would have different behaviors when it comes to dealing with Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my workaround for now, since I need access to that device at 0x30, is to remove some entries in the table.&amp;nbsp; That seems to re-enable the function of Flash, but now I'm worried this isn't really a fix since it absolutely makes no sensor whatsoever.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...argh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 03 Nov 2014 22:23:48 GMT</pubDate>
    <dc:creator>michaelschwager</dc:creator>
    <dc:date>2014-11-03T22:23:48Z</dc:date>
    <item>
      <title>Flash update sometimes not working</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-update-sometimes-not-working/m-p/372042#M12277</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I have 2 custom boards, both with MK60DN512VLQ10 in 144-pin package, running MQX 4.1, and running everything through IAR on Windows 7.&amp;nbsp; Both boards are running the exact same binary.&lt;/P&gt;&lt;P&gt;I can run the flash swap example correctly on both of them.&lt;/P&gt;&lt;P&gt;However one of the two boards is having trouble.&amp;nbsp; I've tried this on 6 different boards (3 working variety and 3 non-working variety) and the results are the same.&lt;/P&gt;&lt;P&gt;The problem almost smells like a hardware problem if seen on its own, but not when you see the full picture.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Setup as follows:&lt;/P&gt;&lt;P&gt;A non-main task runs a loop which uses the Processor Expert SPI slave driver, and blocks (_lwsem_wait_ticks(...) )on a semaphore which is posted by the SPI slave driver.&amp;nbsp; When this driver receives a SPI message from the host, it calls the callback which posts the semaphore and the loop continues.&amp;nbsp; Some time later within the loop and based on the contents of the SPI message, an attempt is made to write to the Flash.&amp;nbsp; For debugging I have sprinkled calls to clone_application(...) in several places.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board 1 (working board):&lt;/P&gt;&lt;P&gt;clone_application() from main_task runs fine&lt;/P&gt;&lt;P&gt;clone_application() from aforementioned non-main task runs fine&lt;/P&gt;&lt;P&gt;my own flash writing code using normal fseek, write, etc., based exactly on the example runs fine.&lt;/P&gt;&lt;P&gt;There is a noticeable and seemingly appropriate delay when erasing the flash via FLASH_IOCTL_ERASE_FILE&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Board (non-working board):&lt;/P&gt;&lt;P&gt;clone_application() from main_task runs fine.&lt;/P&gt;&lt;P&gt;clone_application() from aforementioned non-main task runs fine before it calls _lwsem_wait_ticks(...), runs fine even from within the SPI callback (which is in the interrupt frame) before and after posting the semaphore, but fails after _lwsem_wait_ticks(...) returns.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;IAR stack usage shows i'm not blowing the stack and there appear to be no other errors.&amp;nbsp; The clone_application() runs one or two times through its main loop and then fails with the write(...) call returning -1, ie the write command does not write all 64 bytes.&amp;nbsp; Sometimes it writes more bytes than other times.&amp;nbsp; I've noticed in this failing case that FLASH_IOCTL_ERASE_FILE actually only erases 2048 bytes (from 0x0040_0000 to 0x0040_08000) and the ioctl(...) call does not have the same delay.&amp;nbsp; There is a 100% correlation between erase failing and write failing, but the bytes don't really match.&amp;nbsp; That is, erase only erases 2048 bytes, but write only goes on the order of 8-80 bytes or so before failing, that is, sometimes it'll write one full 64-byte buffer okay, then write something less than 64 bytes and then the write(...) returns -1.&amp;nbsp; So something is screwing with both the erase and the write at different points.&amp;nbsp; I have disabled any other interrupts sources, ie external sensors... anyway, the hardware is virtually identical between working and non-working.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The main hardware difference is the non-working board has far fewer GPIO pin connected, ie doesn't have ethernet and a bunch of debug GPIOs connected.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt; So what could possibly be causing Flash erase to fail and subsequently write to fail?&lt;/P&gt;&lt;P&gt;Why does write(...) return -1 rather than the actual number of bytes written?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Nov 2014 01:34:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-update-sometimes-not-working/m-p/372042#M12277</guid>
      <dc:creator>michaelschwager</dc:creator>
      <dc:date>2014-11-03T01:34:28Z</dc:date>
    </item>
    <item>
      <title>Re: Flash update sometimes not working</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-update-sometimes-not-working/m-p/372043#M12278</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;More information.&lt;/P&gt;&lt;P&gt;The only relevant hardware difference between the working and non-working boards is a sensor device on I2C0 at address 0x30.&lt;/P&gt;&lt;P&gt;This device comes in 8 flavors based on I2C address, so I have a static const []... table (written in Flash) which is looked up when the I2C scan routine comes across any address that does not give a NACK.&amp;nbsp; So I have 8 entries in my table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems the Flash erase fails only when &lt;SPAN style="font-size: 13.6000003814697px;"&gt;I have 3 or more entries in the table (not commented out) *and* I scan address 0x30&lt;/SPAN&gt;.&amp;nbsp; The I2C scan and the Flash routines have *nothing* in common.&amp;nbsp; The I2C scan happen during initialization, and the flash routine happens eons later during normal operation.&amp;nbsp; If I skip address 0x30, or if I have 2 or fewer entries in the table (whether they match address 0x30 or not) then the Flash erase and subsequent rewrite works correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It also turns out my "working" board fails under seemingly opposite conditions of the failing board: the "working" board (which doesn't even have the sensor device at 0x30) fails if I skip scanning address 0x30 or if I comment out several of the entries in the table.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've also noticed under these funny conditions that Jlink-Commander is also unable to erase the device.&amp;nbsp; I have to do "kinetis unlock" for the Jlink-Commander to erase the device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So it seems that somehow the Flash is getting locked, and it seems somehow related to the I2C scanning, which doesn't make any sense at all.&lt;/P&gt;&lt;P&gt;It perhaps has something to do instead with how the table is written in the Flash by the linker, but that also doesn't make any sense, nor does it make any sense that two boards, which only differ in there being a device hanging on I2C0 address 0x30, would have different behaviors when it comes to dealing with Flash.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;So my workaround for now, since I need access to that device at 0x30, is to remove some entries in the table.&amp;nbsp; That seems to re-enable the function of Flash, but now I'm worried this isn't really a fix since it absolutely makes no sensor whatsoever.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;...argh.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Nov 2014 22:23:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-update-sometimes-not-working/m-p/372043#M12278</guid>
      <dc:creator>michaelschwager</dc:creator>
      <dc:date>2014-11-03T22:23:48Z</dc:date>
    </item>
    <item>
      <title>Re: Flash update sometimes not working</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-update-sometimes-not-working/m-p/372044#M12279</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;More info...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found a memory leak during I2C scan.&amp;nbsp; I was allocating 3800 bytes of data per loop for some reason, but not releasing it.&amp;nbsp; Once I fixed this, then Flash erase seems to work.&amp;nbsp; This may have been triggered by the different hardware because it was doing one more memory allocation due to the extra device found on the bus.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 03 Nov 2014 22:57:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Flash-update-sometimes-not-working/m-p/372044#M12279</guid>
      <dc:creator>michaelschwager</dc:creator>
      <dc:date>2014-11-03T22:57:56Z</dc:date>
    </item>
  </channel>
</rss>