<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KDS V2.0.0 and KSDK_1.1.0 with MQX in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369632#M12193</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm also seeing the exact same issue, glad I'm not the only one actually since it doesn't come up on the forum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Essentially I followed this guide to building a framework MQX project: &lt;A href="https://community.nxp.com/docs/DOC-103405"&gt;How To: Create a New MQX RTOS for KSDK Project in KDS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something must be configured incorrectly in the linker or startup code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I load the same code from the pre-built example project (rtos hello world), it works fine.&amp;nbsp; If I try to build my own project from scratch by following these instructions (which I will need to do with a custom board) I run into this issue that appears to be the WDOG_EWM_IRQHandler being called and causing a DefaultISR interrup , even though if you look at the board files the DISABLE_WDOG code appears to be set correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the stack trace which happens just a few ms after startup:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45665i0DD62C6ACE8882ED/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried creating an explicit handler for this (which doesn't fire), I don't know what else to do.&amp;nbsp; I'm new to the quirks of MQX but I don't know how to make a project that is any simpler and it's already showing issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Appreciate any help you can give here, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Mar 2015 22:44:56 GMT</pubDate>
    <dc:creator>auralcircuitry</dc:creator>
    <dc:date>2015-03-30T22:44:56Z</dc:date>
    <item>
      <title>KDS V2.0.0 and KSDK_1.1.0 with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369629#M12190</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, &lt;/P&gt;&lt;P&gt;Can someone help me&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a problem with the FRDMK64F and my application.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The board&amp;nbsp; works properly with other applications.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 13.3333330154419px;"&gt;The proble is that a&lt;/SPAN&gt;fter a short time the application is interrupted&lt;/P&gt;&lt;P&gt;In the debug window, the following is displayed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;WDOG_EWM_IRQHandler () at startup_MK64F12.S: 362 0x568&lt;/P&gt;&lt;P&gt;&amp;lt;signal handler called&amp;gt; () at 0xfffffffd&lt;/P&gt;&lt;P&gt;_sched_start_internal () at dispatch.S: 94 0x56e&lt;/P&gt;&lt;P&gt;_mqx () at mqx.c: 812 0x736a&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i &lt;SPAN style="font-size: 13.3333330154419px;"&gt;disablen &lt;/SPAN&gt;WDOG_EWM_IRQ ?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 09 Mar 2015 13:29:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369629#M12190</guid>
      <dc:creator>onurb</dc:creator>
      <dc:date>2015-03-09T13:29:17Z</dc:date>
    </item>
    <item>
      <title>Re: KDS V2.0.0 and KSDK_1.1.0 with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369630#M12191</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello vedana bruno, &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please share your application in order to reproduce your issue???&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Soledad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2015 21:02:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369630#M12191</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-03-11T21:02:14Z</dc:date>
    </item>
    <item>
      <title>Re: Re: KDS V2.0.0 and KSDK_1.1.0 with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369631#M12192</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Soledad&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Since the project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bruno&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 12 Mar 2015 14:13:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369631#M12192</guid>
      <dc:creator>onurb</dc:creator>
      <dc:date>2015-03-12T14:13:03Z</dc:date>
    </item>
    <item>
      <title>Re: KDS V2.0.0 and KSDK_1.1.0 with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369632#M12193</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I'm also seeing the exact same issue, glad I'm not the only one actually since it doesn't come up on the forum.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Essentially I followed this guide to building a framework MQX project: &lt;A href="https://community.nxp.com/docs/DOC-103405"&gt;How To: Create a New MQX RTOS for KSDK Project in KDS&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Something must be configured incorrectly in the linker or startup code.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If I load the same code from the pre-built example project (rtos hello world), it works fine.&amp;nbsp; If I try to build my own project from scratch by following these instructions (which I will need to do with a custom board) I run into this issue that appears to be the WDOG_EWM_IRQHandler being called and causing a DefaultISR interrup , even though if you look at the board files the DISABLE_WDOG code appears to be set correctly.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is the stack trace which happens just a few ms after startup:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="pastedImage_1.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45665i0DD62C6ACE8882ED/image-size/large?v=v2&amp;amp;px=999" role="button" title="pastedImage_1.png" alt="pastedImage_1.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried creating an explicit handler for this (which doesn't fire), I don't know what else to do.&amp;nbsp; I'm new to the quirks of MQX but I don't know how to make a project that is any simpler and it's already showing issues.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Appreciate any help you can give here, thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 22:44:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369632#M12193</guid>
      <dc:creator>auralcircuitry</dc:creator>
      <dc:date>2015-03-30T22:44:56Z</dc:date>
    </item>
    <item>
      <title>Re: KDS V2.0.0 and KSDK_1.1.0 with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369633#M12194</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi &lt;A class="jx-jive-macro-user" href="https://community.nxp.com/people/onurb"&gt;onurb&lt;/A&gt;​, did you get this issue resolved?&amp;nbsp; I just experienced the same thing.&amp;nbsp; I'm looking around to see what possible solutions are out there for me to try on my application.&amp;nbsp; Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Feb 2016 21:55:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369633#M12194</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2016-02-10T21:55:21Z</dc:date>
    </item>
    <item>
      <title>Re: KDS V2.0.0 and KSDK_1.1.0 with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369634#M12195</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi All,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have same problem on K40. Did anybody resolved this issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Michal&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Apr 2016 08:17:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369634#M12195</guid>
      <dc:creator>mike_susen</dc:creator>
      <dc:date>2016-04-13T08:17:15Z</dc:date>
    </item>
    <item>
      <title>Re: KDS V2.0.0 and KSDK_1.1.0 with MQX</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369635#M12196</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Please check the below thread:&lt;/P&gt;&lt;P&gt;&lt;A _jive_internal="true" href="https://community.nxp.com/thread/353118#511192" title="https://community.freescale.com/thread/353118#511192"&gt;https://community.freescale.com/thread/353118#511192&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 13 Apr 2016 19:53:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KDS-V2-0-0-and-KSDK-1-1-0-with-MQX/m-p/369635#M12196</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2016-04-13T19:53:39Z</dc:date>
    </item>
  </channel>
</rss>