<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: GDB MQX K70 Segger</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/GDB-MQX-K70-Segger/m-p/366110#M12086</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply. &lt;/P&gt;&lt;P&gt;I am already familiar with those. &lt;/P&gt;&lt;P&gt;I think/hoped I have worked out many of my debugging issues. &lt;/P&gt;&lt;P&gt;They appear to have been related to a combination of debug/release code and the wrong debug/optimization options in the Freescale scripts. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale should look further at their scripts. &lt;/P&gt;&lt;P&gt;With some minor change I am able to build/debug with the g++-multiarch arm toolchain that is now pretty standard for debian based Linux distro's such as Ubuntu. &lt;/P&gt;&lt;P&gt;I can send you the script changes if you wish ?&lt;/P&gt;&lt;P&gt;For the moment I am using the Freescale recomended toolchain - I do nto think it makes any difference to my problems. but it is one less variable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 03 Dec 2014 14:48:07 GMT</pubDate>
    <dc:creator>asmith</dc:creator>
    <dc:date>2014-12-03T14:48:07Z</dc:date>
    <item>
      <title>GDB MQX K70 Segger</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/GDB-MQX-K70-Segger/m-p/366108#M12084</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with a K70 Target using MQX 4.1.1 and a Segger Jlink &lt;/P&gt;&lt;P&gt;Building using arm-none-eabi-gcc under Ubuntu 14.04&lt;/P&gt;&lt;P&gt;I am able to build MQX build the application, Link and debug using arm-none-eabi-gdb --tui application.elf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But I am frequently unable to step into (s) or execture through (n) functions - I can usually step into them using (si) - step by machine instruction. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But in many instances trying to (s) into or (n) over a function cause the processor to execute either until the next break point or until the program crashes&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any ideas would be appreciated&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Mmostly I am debugging quite well but the need to set large numbers of break points where (s) or (n) would make life easier slows things down&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 24 Nov 2014 18:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/GDB-MQX-K70-Segger/m-p/366108#M12084</guid>
      <dc:creator>asmith</dc:creator>
      <dc:date>2014-11-24T18:40:07Z</dc:date>
    </item>
    <item>
      <title>Re: GDB MQX K70 Segger</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/GDB-MQX-K70-Segger/m-p/366109#M12085</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below threads.&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/317201"&gt;gcc compiling + gdb debugging on Kinetis on a Linux host - Kinetis L Examples available&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/thread/329459"&gt;Problem with build_gcc_arm.sh script (echo)&lt;/A&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol &lt;BR /&gt; &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 02 Dec 2014 23:01:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/GDB-MQX-K70-Segger/m-p/366109#M12085</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-12-02T23:01:15Z</dc:date>
    </item>
    <item>
      <title>Re: GDB MQX K70 Segger</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/GDB-MQX-K70-Segger/m-p/366110#M12086</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for the reply. &lt;/P&gt;&lt;P&gt;I am already familiar with those. &lt;/P&gt;&lt;P&gt;I think/hoped I have worked out many of my debugging issues. &lt;/P&gt;&lt;P&gt;They appear to have been related to a combination of debug/release code and the wrong debug/optimization options in the Freescale scripts. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Freescale should look further at their scripts. &lt;/P&gt;&lt;P&gt;With some minor change I am able to build/debug with the g++-multiarch arm toolchain that is now pretty standard for debian based Linux distro's such as Ubuntu. &lt;/P&gt;&lt;P&gt;I can send you the script changes if you wish ?&lt;/P&gt;&lt;P&gt;For the moment I am using the Freescale recomended toolchain - I do nto think it makes any difference to my problems. but it is one less variable.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 03 Dec 2014 14:48:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/GDB-MQX-K70-Segger/m-p/366110#M12086</guid>
      <dc:creator>asmith</dc:creator>
      <dc:date>2014-12-03T14:48:07Z</dc:date>
    </item>
  </channel>
</rss>