<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: MQX for KSDK USB host fat system</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364483#M12027</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this manual shows only how to set up the MQX (lite) with PE, but for this it is very good. I´ve done this before, this was not the problem. In the example above, the FRDM board is used as an USB Host, I think this could be managed with the PE fsl_usb_framework of KSDK. At the moment i try to set up the parameters in PE to do the same as in the example. Init works fine. When i add a Device at the USB Port the ISR Callback is called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In next step i will have to add the FAT fs to save data, is there an additional PE Component to manage these functions. When i try to understand the example, and copy it line by line there are many #includes i have to do, could be easier with PE funcitons ready to work...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and have a great day&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Menko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Fri, 23 Jan 2015 08:04:36 GMT</pubDate>
    <dc:creator>menkooldewurtel</dc:creator>
    <dc:date>2015-01-23T08:04:36Z</dc:date>
    <item>
      <title>MQX for KSDK USB host fat system</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364481#M12025</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;BR /&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;with KDS2.0 and KSDK1.1.0 on FRDM-K64F Board: I want to write data&amp;nbsp; on a USB MSD with an FAT Filesystem.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I found this example: C:\Freescale\KSDK_1.1.0\usb\example\host\msd\msd_fatfs\sdk\kds\host_msd_fatfs_frdmk64f_mqx&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Now want to copy the example and modify for my application. In the user Guide it is only described for iar, but i want to develop it in KDS2.0. So what i have to do to copy the example? I´ve found this Tool: &lt;A href="https://community.nxp.com/docs/DOC-102547"&gt;Create new KSDK Projects&lt;/A&gt; but don´t know how to change the args when starting it for the fat-project. Can anyone help?`&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Next problem will come up: Is it possible to add Components with PE to the project? Could be easier then to use the BM example?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Menko &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 21 Jan 2015 15:39:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364481#M12025</guid>
      <dc:creator>menkooldewurtel</dc:creator>
      <dc:date>2015-01-21T15:39:03Z</dc:date>
    </item>
    <item>
      <title>Re: MQX for KSDK USB host fat system</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364482#M12026</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the below link and let me know if this helps!!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-103429"&gt;How To: Create an MQX RTOS project with Processor Expert in Kinetis Design Studio IDE&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol &lt;BR /&gt; &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 22 Jan 2015 18:42:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364482#M12026</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-01-22T18:42:55Z</dc:date>
    </item>
    <item>
      <title>Re: MQX for KSDK USB host fat system</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364483#M12027</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this manual shows only how to set up the MQX (lite) with PE, but for this it is very good. I´ve done this before, this was not the problem. In the example above, the FRDM board is used as an USB Host, I think this could be managed with the PE fsl_usb_framework of KSDK. At the moment i try to set up the parameters in PE to do the same as in the example. Init works fine. When i add a Device at the USB Port the ISR Callback is called.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In next step i will have to add the FAT fs to save data, is there an additional PE Component to manage these functions. When i try to understand the example, and copy it line by line there are many #includes i have to do, could be easier with PE funcitons ready to work...&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you and have a great day&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Menko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 08:04:36 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364483#M12027</guid>
      <dc:creator>menkooldewurtel</dc:creator>
      <dc:date>2015-01-23T08:04:36Z</dc:date>
    </item>
    <item>
      <title>Re: Re: MQX for KSDK USB host fat system</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364484#M12028</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi again,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;i have migrated the example to PE and everything works. But there is one problem:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When i use the fsl_usb_framework of PE its generates a usb_host_config.h file in Generated_Code/SDK/usb/usb_core/host/include/usb_host_config.h&lt;/P&gt;&lt;P&gt;Another file is stored in SDK/usb/usb_core/host/sources/classes/common/usb_classes.c&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In the second file (usb_classes.c)&amp;nbsp; is &lt;SPAN style="font-size: 10pt;"&gt; class_interface_map[]. With the defines in the headerfile (usb_config_host.h) i can enable components of the class interface map.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt;"&gt;In the example (look at the first question), is there #define &lt;/SPAN&gt;USBCFG_HOST_MSC (1). In the PE file not. If I add this by myself everything works. Where can i configure PE to do this for me?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have added my PE-file, hope you can help?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Menko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 23 Jan 2015 12:40:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-for-KSDK-USB-host-fat-system/m-p/364484#M12028</guid>
      <dc:creator>menkooldewurtel</dc:creator>
      <dc:date>2015-01-23T12:40:33Z</dc:date>
    </item>
  </channel>
</rss>