<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic USB CDC Virtaul COM between host and device failed in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363935#M12007</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a USB host of k20d76m running MQX3.8 and a USB CDC device of k20d50m running MQX4.1. The USB CDC device has no problem talking to a host PC via hyper terminal but there is no communication happens when connecting to the host. That means, when host sends bytes to device, it reads nothing back from the&amp;nbsp; device. The enumeration is done successfully in this case. But data communication failed, anyone has insights or comments on it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I traced into USB host source, noticed that when usb_class_cdc_in_data_callback() of usb_host_cdc.c is called, the status is 0x97 which means USBERR_TR_FAILED.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 02 Oct 2014 17:44:38 GMT</pubDate>
    <dc:creator>huishao2</dc:creator>
    <dc:date>2014-10-02T17:44:38Z</dc:date>
    <item>
      <title>USB CDC Virtaul COM between host and device failed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363935#M12007</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have a USB host of k20d76m running MQX3.8 and a USB CDC device of k20d50m running MQX4.1. The USB CDC device has no problem talking to a host PC via hyper terminal but there is no communication happens when connecting to the host. That means, when host sends bytes to device, it reads nothing back from the&amp;nbsp; device. The enumeration is done successfully in this case. But data communication failed, anyone has insights or comments on it?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I traced into USB host source, noticed that when usb_class_cdc_in_data_callback() of usb_host_cdc.c is called, the status is 0x97 which means USBERR_TR_FAILED.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 02 Oct 2014 17:44:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363935#M12007</guid>
      <dc:creator>huishao2</dc:creator>
      <dc:date>2014-10-02T17:44:38Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC Virtaul COM between host and device failed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363936#M12008</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please check the below link???&lt;/P&gt;&lt;P&gt;&lt;A href="https://community.nxp.com/docs/DOC-101404"&gt;USB CDC Virtual Com Example&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 21:26:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363936#M12008</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-10-22T21:26:46Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC Virtaul COM between host and device failed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363937#M12009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your help. I think I have worked around the issue that was caused by fact that my CDC device bootup time was longer than my CDC host. The workaround was to delay the Reset Bus Condition to cater for slower CDC device.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 22 Oct 2014 22:15:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363937#M12009</guid>
      <dc:creator>huishao2</dc:creator>
      <dc:date>2014-10-22T22:15:55Z</dc:date>
    </item>
    <item>
      <title>Re: USB CDC Virtaul COM between host and device failed</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363938#M12010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for sharing your solution,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Sol &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 23 Oct 2014 13:17:50 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-CDC-Virtaul-COM-between-host-and-device-failed/m-p/363938#M12010</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-10-23T13:17:50Z</dc:date>
    </item>
  </channel>
</rss>