<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Re: Webserver in MQX4.1.0.1 is not linked - MCF52255 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362977#M11936</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Carlos Alberto,&lt;/P&gt;&lt;P&gt;I tried your software with the TWRK70 and it is working.&lt;/P&gt;&lt;P&gt;I tried the demo software web_hvac founded in MQX4.1 demo directory with TWRK70 and it is working, too.&lt;/P&gt;&lt;P&gt;I started from the demo software web_hvac and I implemented my application for my board where I use the MCF52255 micro.&lt;/P&gt;&lt;P&gt;The initializialization as the way of RTCS MQX4.1.&lt;/P&gt;&lt;P&gt;My application is running without any error, there are all the tasks but the webserver doesn't answer and the "ping" command fails.&lt;/P&gt;&lt;P&gt;Attached some configuration files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made another test.&lt;/P&gt;&lt;P&gt;I tried to compile for MCF52255 the example "httpsrvr" found in MQX4.1\rtcs\examples directory but, when I start the debugger, always the debugger will stop everytime and it will display the error showed in Debugger_error_httpsrv.jpg. Why?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mirko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 19 Aug 2014 15:55:54 GMT</pubDate>
    <dc:creator>kappa74</dc:creator>
    <dc:date>2014-08-19T15:55:54Z</dc:date>
    <item>
      <title>Webserver in MQX4.1.0.1 is not linked - MCF52255</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362975#M11934</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I use MQX4.1 and CW10.4, the microcontroller is MCF52255. I want to port my project from library MQX3.8.1 to library MQX4.1 (patched 1) because the webserver didn't work properly and the technical support suggested to me to do this migration.&lt;/P&gt;&lt;P&gt;I don't use external RAM, it is not present in my project.&lt;/P&gt;&lt;P&gt;I started from the example "web_hvac" where I added my source files and an home page which displayed only "Hello world!!!".&lt;/P&gt;&lt;P&gt;After compiling in debug version, and programmed the microcontroller I connected my board directly to the PC and then I connected my board and the PC through a router: the results are the same.&lt;/P&gt;&lt;P&gt;The setting of the board is:IP=192.168.1.236 - mask=255.255.0.0 - gateway=192.168.1.252.&lt;/P&gt;&lt;P&gt;The setting of the PC is: IP=192.168.1.100 - mask=255.255.0.0 - gateway=192.168.1.252.&lt;/P&gt;&lt;P&gt;I disabled the DHCP.&lt;/P&gt;&lt;P&gt;I tried to communicate by Ethernet but:&lt;/P&gt;&lt;P&gt;- the "ping" command from DOS shell of the PC failed&lt;/P&gt;&lt;P&gt;- the webserver of MCF52255 didn't work, I tried with Mozilla Firefox and with Google Chrome but I didn't get any connection&lt;/P&gt;&lt;P&gt;- the connection by Ethernet didn't work, I have a supervision software which works by Ethernet connection&lt;/P&gt;&lt;P&gt;The initialization of RTCS task is OK, I hadn't any error in the task (viewed by "Task summery" and also by the debugger step by step).&lt;/P&gt;&lt;P&gt;In conclusion the webserver is not working!!!Running the tasks but I can't get any connection. There is no connection by Ethernet.&lt;/P&gt;&lt;P&gt;With the old version, and in the same condition, I got web connection.&lt;/P&gt;&lt;P&gt;You can find attached the source files, configuration files.&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Can you say me, which is the error?&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Mirko Fortunato&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338886"&gt;RTCS.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338886"&gt;user_config.h.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338886"&gt;vectors.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338886"&gt;small_ram_config.h.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338886"&gt;eth.h.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338886"&gt;HVAC_Task.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338886"&gt;Tasks.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 17 Aug 2014 09:13:56 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362975#M11934</guid>
      <dc:creator>kappa74</dc:creator>
      <dc:date>2014-08-17T09:13:56Z</dc:date>
    </item>
    <item>
      <title>Re: Webserver in MQX4.1.0.1 is not linked - MCF52255</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362976#M11935</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mirko,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;RTCS in MQX4.1 has many differences compared to MQX3.8 which are oriented to improve performance, therefore RTCS initialization does not work the same way in both versions.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please find attached a simple example of a webserver. I used K70, but you can copy the source files to a MCF5225x project as MQX is cross platform.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps!&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 18 Aug 2014 21:50:23 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362976#M11935</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2014-08-18T21:50:23Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Webserver in MQX4.1.0.1 is not linked - MCF52255</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362977#M11936</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Carlos Alberto,&lt;/P&gt;&lt;P&gt;I tried your software with the TWRK70 and it is working.&lt;/P&gt;&lt;P&gt;I tried the demo software web_hvac founded in MQX4.1 demo directory with TWRK70 and it is working, too.&lt;/P&gt;&lt;P&gt;I started from the demo software web_hvac and I implemented my application for my board where I use the MCF52255 micro.&lt;/P&gt;&lt;P&gt;The initializialization as the way of RTCS MQX4.1.&lt;/P&gt;&lt;P&gt;My application is running without any error, there are all the tasks but the webserver doesn't answer and the "ping" command fails.&lt;/P&gt;&lt;P&gt;Attached some configuration files.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I made another test.&lt;/P&gt;&lt;P&gt;I tried to compile for MCF52255 the example "httpsrvr" found in MQX4.1\rtcs\examples directory but, when I start the debugger, always the debugger will stop everytime and it will display the error showed in Debugger_error_httpsrv.jpg. Why?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mirko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 19 Aug 2014 15:55:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362977#M11936</guid>
      <dc:creator>kappa74</dc:creator>
      <dc:date>2014-08-19T15:55:54Z</dc:date>
    </item>
    <item>
      <title>Re: Webserver in MQX4.1.0.1 is not linked - MCF52255</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362978#M11937</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos Alberto,&lt;/P&gt;&lt;P&gt;I noted that in MQX4.1 there is the initialization for the physical Ethernet device ksz8041.&lt;/P&gt;&lt;P&gt;In my board I mounted the device ksz8721BL. With this initialization the Ethernet device doesn't work.&lt;/P&gt;&lt;P&gt;If I change the initialization using the file dp83xxx.c, the Ethenet device will start to work.&lt;/P&gt;&lt;P&gt;Do you think that I can use this initialization or can I have some problem?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MQX4.1 the initialization for ksz8721BL is missing.&lt;/P&gt;&lt;P&gt;Have you developped any initialization file for this device?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Mirko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 20 Aug 2014 12:54:59 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362978#M11937</guid>
      <dc:creator>kappa74</dc:creator>
      <dc:date>2014-08-20T12:54:59Z</dc:date>
    </item>
    <item>
      <title>Re: Webserver in MQX4.1.0.1 is not linked - MCF52255</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362979#M11938</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Mirko,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I recommend to create your own initialization for the PHY, I have not used othe PHYs than the ones that are in our boards.&lt;/P&gt;&lt;P&gt;If you need help with this I would suggest MQX level 2 support as this is a specific change in BSP.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please visit&lt;/P&gt;&lt;P&gt;&lt;A href="http://www.freescale.com/webapp/sps/site/prod_summary.jsp?code=MQX_SUPPORT"&gt;www.freescale.com/mqx/support&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Should you need to contact us with regard to this message, please see the notes below.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 21 Aug 2014 05:35:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Webserver-in-MQX4-1-0-1-is-not-linked-MCF52255/m-p/362979#M11938</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2014-08-21T05:35:49Z</dc:date>
    </item>
  </channel>
</rss>