<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic K60 TCP/IP debugger Multilink Universal not working in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/K60-TCP-IP-debugger-Multilink-Universal-not-working/m-p/354024#M11526</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I use K60 with MQX4.0.2 and CW14. I compiled my software in debug mode and try to debug it.&lt;/P&gt;&lt;P&gt;I implemented a webserver. My debugger is the PE Multilink Universal.&lt;/P&gt;&lt;P&gt;If I run the software without debugger, the webserver will work normally.&lt;/P&gt;&lt;P&gt;If I run the software using the debugger, the webserver and also the ping command will not working.&lt;/P&gt;&lt;P&gt;By Task summery window I see on TCP/IP task, the message: Rx Msg Blocked, Timeouted!&lt;/P&gt;&lt;P&gt;Why?&lt;/P&gt;&lt;P&gt;Does the debugger work with TCP/IP connection?&lt;/P&gt;&lt;P&gt;I use the initialization of the webserver example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Mirko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 10 Sep 2014 10:04:28 GMT</pubDate>
    <dc:creator>kappa74</dc:creator>
    <dc:date>2014-09-10T10:04:28Z</dc:date>
    <item>
      <title>K60 TCP/IP debugger Multilink Universal not working</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/K60-TCP-IP-debugger-Multilink-Universal-not-working/m-p/354024#M11526</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Good morning,&lt;/P&gt;&lt;P&gt;I use K60 with MQX4.0.2 and CW14. I compiled my software in debug mode and try to debug it.&lt;/P&gt;&lt;P&gt;I implemented a webserver. My debugger is the PE Multilink Universal.&lt;/P&gt;&lt;P&gt;If I run the software without debugger, the webserver will work normally.&lt;/P&gt;&lt;P&gt;If I run the software using the debugger, the webserver and also the ping command will not working.&lt;/P&gt;&lt;P&gt;By Task summery window I see on TCP/IP task, the message: Rx Msg Blocked, Timeouted!&lt;/P&gt;&lt;P&gt;Why?&lt;/P&gt;&lt;P&gt;Does the debugger work with TCP/IP connection?&lt;/P&gt;&lt;P&gt;I use the initialization of the webserver example.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Mirko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 10 Sep 2014 10:04:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/K60-TCP-IP-debugger-Multilink-Universal-not-working/m-p/354024#M11526</guid>
      <dc:creator>kappa74</dc:creator>
      <dc:date>2014-09-10T10:04:28Z</dc:date>
    </item>
    <item>
      <title>Re: K60 TCP/IP debugger Multilink Universal not working</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/K60-TCP-IP-debugger-Multilink-Universal-not-working/m-p/354025#M11527</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The debugger can work with TCPIP connection.&lt;/P&gt;&lt;P&gt;The web server demo can work well with debugger in TWR-K60 board.&lt;/P&gt;&lt;P&gt;Maybe you need to check whether it is a hardware issue or not.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;Daniel&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 11 Sep 2014 02:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/K60-TCP-IP-debugger-Multilink-Universal-not-working/m-p/354025#M11527</guid>
      <dc:creator>danielchen</dc:creator>
      <dc:date>2014-09-11T02:55:34Z</dc:date>
    </item>
  </channel>
</rss>