<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックK64 UART buffer extend to 1KBytes</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/K64-UART-buffer-extend-to-1KBytes/m-p/353777#M11517</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We want to extend UART buffer up to 1KBytes.&lt;/P&gt;&lt;P&gt;We understand that we can extend UART buffer size by add the following code into the user_config.h.&lt;/P&gt;&lt;P&gt;#define BSPCFG_SCI1_QUEUE_SIZE&amp;nbsp; 1024&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But we find out the following comment in the twrk64f120m.h.&lt;/P&gt;&lt;P&gt;/*&lt;/P&gt;&lt;P&gt;** TTYB and ITTYB buffer size&lt;/P&gt;&lt;P&gt;** MGCT: &amp;lt;option type="number" min="0" max="256"/&amp;gt;&lt;/P&gt;&lt;P&gt;*/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We checked source code, but we cannot find out a reason that why maximum size of UART buffer is 256 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my questions.&lt;/P&gt;&lt;P&gt;1. Can we extend UART buffer to 1,24 bytes?&lt;/P&gt;&lt;P&gt;2. If no, please explain that why we cannot extend UART buffer to 1,024 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please reply as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Takakshima&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 16 Dec 2014 08:37:20 GMT</pubDate>
    <dc:creator>isaotakashima</dc:creator>
    <dc:date>2014-12-16T08:37:20Z</dc:date>
    <item>
      <title>K64 UART buffer extend to 1KBytes</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/K64-UART-buffer-extend-to-1KBytes/m-p/353777#M11517</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We want to extend UART buffer up to 1KBytes.&lt;/P&gt;&lt;P&gt;We understand that we can extend UART buffer size by add the following code into the user_config.h.&lt;/P&gt;&lt;P&gt;#define BSPCFG_SCI1_QUEUE_SIZE&amp;nbsp; 1024&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;But we find out the following comment in the twrk64f120m.h.&lt;/P&gt;&lt;P&gt;/*&lt;/P&gt;&lt;P&gt;** TTYB and ITTYB buffer size&lt;/P&gt;&lt;P&gt;** MGCT: &amp;lt;option type="number" min="0" max="256"/&amp;gt;&lt;/P&gt;&lt;P&gt;*/&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We checked source code, but we cannot find out a reason that why maximum size of UART buffer is 256 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here is my questions.&lt;/P&gt;&lt;P&gt;1. Can we extend UART buffer to 1,24 bytes?&lt;/P&gt;&lt;P&gt;2. If no, please explain that why we cannot extend UART buffer to 1,024 bytes.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please reply as soon as possible.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;Takakshima&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 08:37:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/K64-UART-buffer-extend-to-1KBytes/m-p/353777#M11517</guid>
      <dc:creator>isaotakashima</dc:creator>
      <dc:date>2014-12-16T08:37:20Z</dc:date>
    </item>
    <item>
      <title>Re: K64 UART buffer extend to 1KBytes</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/K64-UART-buffer-extend-to-1KBytes/m-p/353778#M11518</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Takashima,&lt;/P&gt;&lt;P&gt;There really is no limit other than available SRAM.&lt;/P&gt;&lt;P&gt;I tested with the TWR-K64F120M using a 1024 buffer modified in the twrk64f120m.h as follows:&lt;/P&gt;&lt;P&gt;#ifndef BSPCFG_SCI5_QUEUE_SIZE&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; #define BSPCFG_SCI5_QUEUE_SIZE&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1024 //DES was 64&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I also setup to use interrupt mode for my UART5 (ittyf).&lt;/P&gt;&lt;P&gt;My simple test was (NOTE I did modify the BSP serl_int.c code) as follows to return number of characters in the queue:&lt;/P&gt;&lt;P&gt;_mqx_int _io_serial_int_ioctl&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; (&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* [IN] the handle returned from _fopen */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; FILE_DEVICE_STRUCT_PTR fd_ptr,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* [IN] the ioctl command */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _mqx_uint&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; cmd,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* [IN] the ioctl parameters */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; void&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *param_ptr&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; )&lt;/P&gt;&lt;P&gt;{ /* Body */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; IO_DEVICE_STRUCT_PTR&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; io_dev_ptr;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; IO_SERIAL_INT_DEVICE_STRUCT_PTR int_io_dev_ptr;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; _mqx_uint&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; result = MQX_OK;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; _mqx_uint_ptr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uparam_ptr = (_mqx_uint_ptr)param_ptr;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; io_dev_ptr&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; = fd_ptr-&amp;gt;DEV_PTR;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; int_io_dev_ptr = (void *)io_dev_ptr-&amp;gt;DRIVER_INIT_PTR;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; switch (cmd) {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; case IO_IOCTL_CHAR_AVAIL:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if ( _CHARQ_SIZE(int_io_dev_ptr-&amp;gt;IN_QUEUE) ) {&lt;/P&gt;&lt;P&gt;//&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *((bool *)param_ptr) = TRUE; //DES??? why not return _CHARQ_SIZE ???&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *((_mqx_int *)param_ptr) = _CHARQ_SIZE(int_io_dev_ptr-&amp;gt;IN_QUEUE); //DES??? why not return _CHARQ_SIZE ???&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; } else {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; *((bool *)param_ptr) = FALSE;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; } /* Endif */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Used the MQX hello example and modified hello.c as follows:&lt;/P&gt;&lt;P&gt;void hello_task&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; (&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; uint32_t initial_data&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; )&lt;/P&gt;&lt;P&gt;{&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; (void)initial_data; /* disable 'unused variable' warning */&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int io_param; //DES added&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int inchar; //DES added&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; int rc; //DES added&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; printf("Hello World\n");&lt;/P&gt;&lt;P&gt;#if 1 //DES 1=test, 0=default code&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; for (;;)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; rc = _io_ioctl(stdin,IO_IOCTL_CHAR_AVAIL,&amp;amp;io_param);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; while(io_param) //DES was&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; if(io_param)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; {&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; inchar = fgetc(stdin);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; fputc(inchar, stdout);&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; io_param--;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; _time_delay(5000); //DES block for 5 seconds (5000msec)...give time to fill UART Rx queue&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; }&lt;/P&gt;&lt;P&gt;#endif&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; _task_block();&lt;/P&gt;&lt;P&gt;}&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 16 Dec 2014 16:56:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/K64-UART-buffer-extend-to-1KBytes/m-p/353778#M11518</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2014-12-16T16:56:00Z</dc:date>
    </item>
    <item>
      <title>Re: K64 UART buffer extend to 1KBytes</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/K64-UART-buffer-extend-to-1KBytes/m-p/353779#M11519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Is this still the case that the max buffer size can be increased over the stated maximum (mqx 4.1.1 with K60)?&lt;/P&gt;&lt;P&gt;I have one set to 512 in user config and its red with "Given value is larger than define maximum for this parameter (256).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Also is there a way for me to tell if the buffers are being filled?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Jon&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 14 Aug 2015 10:17:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/K64-UART-buffer-extend-to-1KBytes/m-p/353779#M11519</guid>
      <dc:creator>jonny</dc:creator>
      <dc:date>2015-08-14T10:17:33Z</dc:date>
    </item>
  </channel>
</rss>