<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: MQX with KSDK and Processor Expert</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351660#M11439</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Jason,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Processor Expert (PEx) does not provide the ability with MQX to add the other libraries for you, like the shell, MFS file system, RTCS TCP/IP or USB stacks.&amp;nbsp; But you can manually add these libraries to the MQX project generated by PEx.&amp;nbsp; That means changing the linker settings to add the library and change the compiler include paths for the library header files.&amp;nbsp; You can refer to our MQX examples that use the shell or these libraries as an example for these settings, and as a reference for the source code in your application to use the library.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Below is an example of these project settings.&amp;nbsp; I no longer have this older version of MQX for KSDK installed, which was the version used at the beginning of this post.&amp;nbsp; But I'll use the latest MQX for KSDK v1.3 as an example.&amp;nbsp; This is using the RTCS shell example installed at \KSDK_1.3.0\middleware\tcpip\rtcs\examples\shell\build\kds\shell_frdmk64f, and uses the Kinetis Design Studio (KDS) toolchain.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Here are the linker settings including the nshell library, and the path to that library:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="shell_linker.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1309iFE04D090A947C4CD/image-size/large?v=v2&amp;amp;px=999" role="button" title="shell_linker.jpg" alt="shell_linker.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;And the compiler settings for the include path&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="shell_compiler.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/1355iDA5A1903CA86A671/image-size/large?v=v2&amp;amp;px=999" role="button" title="shell_compiler.jpg" alt="shell_compiler.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 02 Aug 2016 23:30:35 GMT</pubDate>
    <dc:creator>dereksnell</dc:creator>
    <dc:date>2016-08-02T23:30:35Z</dc:date>
    <item>
      <title>MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351628#M11407</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;The Freescale MQX RTOS is transitioning to use the Kinetis Software Development Kit (KSDK), and there is a Beta release of MQX for KSDK available now.&amp;nbsp; See &lt;A _jive_internal="true" data-containerid="2023" data-containertype="14" data-objectid="328720" data-objecttype="1" href="https://community.nxp.com/thread/328720"&gt;Beta version of MQX RTOS for Kinetis SDK - Now Available&lt;/A&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;.&amp;nbsp; Processor Expert (PEx) is a code generation and configuration tool that is already integrated with KSDK.&amp;nbsp; This post shows how PEx can be used with MQX for KSDK.&amp;nbsp; This method is good for simple MQX projects just needing the kernel.&amp;nbsp; PEx simplifies the project by adding the KSDK and MQX kernel files directly to the project.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;These steps are written using MQX for KSDK v1.0.0 Beta.&amp;nbsp; The Kinetis Design Studio (KDS) v1.1.1 toolchain is used, with example project attached.&amp;nbsp; KDS has PEx integrated in the IDE and is used for this example, although the stand-alone tool &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=http%3A%2F%2Fwww.freescale.com%2Fwebapp%2Fsps%2Fsite%2Fprod_summary.jsp%3Fcode%3DPE_DRIVER_SUITE%26tid%3DPEH" rel="nofollow" target="_blank"&gt;Processor Expert Driver Suite&lt;/A&gt; v10.4 can be used with other toolchains.&amp;nbsp; For help getting started with PEx, check out the videos at &lt;A _jive_internal="true" data-containerid="2022" data-containertype="14" data-objectid="93433" data-objecttype="102" href="https://community.nxp.com/docs/DOC-93433"&gt;Processor Expert Tools in CodeWarrior 10.3 - Training Videos&lt;/A&gt;&lt;/SPAN&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;MQX for KSDK does not yet have any PEx projects installed with the release, but PEx can be used to create a project from scratch.&amp;nbsp; First, ensure to follow the KDS release notes to have the KSDK plugins installed.&amp;nbsp; Also, refer to the MQX documentation to ensure the latest MQX plugins are installed in KDS as well.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Now create a new project using the menu File-&amp;gt;New.&amp;nbsp; The New Project Wizard will walkthrough the project creation.&amp;nbsp; Be sure to specify a Kinetis device that is supported by the KSDK, refer to KSDK release notes to see the available list of devices.&amp;nbsp; For the "Rapid Application Development" screen, be sure to check both Kinetis SDK and Processor Expert.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="14711_14711.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119948iEDFC65E77D320B47/image-size/large?v=v2&amp;amp;px=999" role="button" title="14711_14711.jpg" alt="14711_14711.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Rapid_Development.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45768i756231C20C9D64F5/image-size/large?v=v2&amp;amp;px=999" role="button" title="Rapid_Development.jpg" alt="Rapid_Development.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Finish creating the project.&amp;nbsp; After the project is created, use the Component Library to add the components MQX_KSDK and MQX_KSDK_Task.&amp;nbsp; The project needs at least one MQX_KSDK_Task component, and more can be added for multiple tasks in the application.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="14712_14712.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119949i3FAC16D99F824035/image-size/large?v=v2&amp;amp;px=999" role="button" title="14712_14712.jpg" alt="14712_14712.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="MQX Components.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45769i5ECF1AAA73BF4879/image-size/large?v=v2&amp;amp;px=999" role="button" title="MQX Components.jpg" alt="MQX Components.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;After adding the MQX components, the Components View will show them included in the project.&amp;nbsp; The MQX_KSDK properties can be customized if needed using the Component Inspector View.&amp;nbsp; Each Task should be customized using the properties for the MQX_KSDK_Task components.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="14713_14713.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119950iF169EFE8C20A8F94/image-size/large?v=v2&amp;amp;px=999" role="button" title="14713_14713.jpg" alt="14713_14713.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Project Components.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45843iE0E10A5F7161F59D/image-size/large?v=v2&amp;amp;px=999" role="button" title="Project Components.jpg" alt="Project Components.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;MQX uses stdin/stdout typically through a UART for IO functions like printf().&amp;nbsp; This can also be easily customized for the board being used.&amp;nbsp; In this example, the project is written for the FRDM-K64F board, and uses the UART connected to the OpenSDA USB COM port.&amp;nbsp; That board uses UART0 on pins PTB16 and PTB17.&amp;nbsp; To configure in PEx, select the fsl_uart component, which is included as a sub-component under the MQX_KSDK component.&amp;nbsp; Then, in the Component Inspector, change the Properties to use the needed UART peripheral and specify the pins.&amp;nbsp; The other UART properties can also be customized if needed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="14714_14714.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119951i80213F78A6C48C08/image-size/large?v=v2&amp;amp;px=999" role="button" title="14714_14714.jpg" alt="14714_14714.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="UART Settings.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45005i20D8E6BADE7A5895/image-size/large?v=v2&amp;amp;px=999" role="button" title="UART Settings.jpg" alt="UART Settings.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Other PEx components can be added as well to configure the peripheral drivers.&amp;nbsp; Once the PEx configuration is complete, generate the code by clicking the Generate Code button in the Components View.&amp;nbsp; This will generate the KSDK and MQX kernel code and add it directly to the project.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="14715_14715.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119952iED0EE7F8B000204C/image-size/large?v=v2&amp;amp;px=999" role="button" title="14715_14715.jpg" alt="14715_14715.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Generate Code.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45006iDDA8C05080310DDC/image-size/large?v=v2&amp;amp;px=999" role="button" title="Generate Code.jpg" alt="Generate Code.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;With the current releases, PEx will generate a warning in KDS when the code is generated.&amp;nbsp; The GNU ISO C99 standard should be used when building MQX.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="14716_14716.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119953iAE0D01F67F4916AD/image-size/large?v=v2&amp;amp;px=999" role="button" title="14716_14716.jpg" alt="14716_14716.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Compiler warning.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45770iAA181232A67FAE1E/image-size/large?v=v2&amp;amp;px=999" role="button" title="Compiler warning.jpg" alt="Compiler warning.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;To change this compiler setting, right-click the project and select Properties.&amp;nbsp; Then use this screenshot to find the Language Standard in the Compiler Optimization settings, and change to GNU ISO C99.&amp;nbsp; Click OK to save the change.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="14717_14717.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119954iFDFA1EAB9B9E2FDB/image-size/large?v=v2&amp;amp;px=999" role="button" title="14717_14717.jpg" alt="14717_14717.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="Compiler settings.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45592iF9909D3DA8D1F719/image-size/large?v=v2&amp;amp;px=999" role="button" title="Compiler settings.jpg" alt="Compiler settings.jpg" /&gt;&lt;/span&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Now the MQX application can be written.&amp;nbsp; The MQX_KSDK_Task components will create function stubs for the tasks.&amp;nbsp; The task routine prototypes are located in the project header file Sources/mqx_tasks.h and stubs of task functions are in source file Sources/mqx_tasks.c.&amp;nbsp; Add the application code to these tasks.&amp;nbsp; Then use the toolchain to build the project, and download to the target hardware.&amp;nbsp; &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;The attached project is an example following these steps for KDS.&amp;nbsp; It has a single MQX task that prints "Hello World!" out the UART using printf().&amp;nbsp; It's written for the FRDM-K64F board, and setup to use the &lt;A _jive_internal="true" href="https://community.nxp.com/external-link.jspa?url=https%3A%2F%2Fsegger.com%2Fopensda.html" rel="nofollow" target="_blank"&gt;Segger JLink OpenSDA V2 debugger app&lt;/A&gt;.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-338508"&gt;MQX_KSDK_PEx.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 09 Sep 2014 18:07:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351628#M11407</guid>
      <dc:creator>dereksnell</dc:creator>
      <dc:date>2014-09-09T18:07:55Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351629#M11408</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello Derek &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I've tried to use MQX with your steps but appears this error in the console when i try degug:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;SEGGER J-Link GDB Server V4.88a Command Line Version&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;JLinkARM.dll V4.88a (DLL compiled Jul 17 2014 18:20:19)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----GDB Server start settings-----&lt;/P&gt;&lt;P&gt;GDBInit file:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; none&lt;/P&gt;&lt;P&gt;GDB Server Listening port:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2331&lt;/P&gt;&lt;P&gt;SWO raw output listening port: 2332&lt;/P&gt;&lt;P&gt;Terminal I/O port:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 2333&lt;/P&gt;&lt;P&gt;Accept remote connection:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; localhost only&lt;/P&gt;&lt;P&gt;Generate logfile:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; off&lt;/P&gt;&lt;P&gt;Verify download:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; on&lt;/P&gt;&lt;P&gt;Init regs on start:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; on&lt;/P&gt;&lt;P&gt;Silent mode:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; off&lt;/P&gt;&lt;P&gt;Single run mode:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; on&lt;/P&gt;&lt;P&gt;Target connection timeout:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 5 sec.&lt;/P&gt;&lt;P&gt;------J-Link related settings------&lt;/P&gt;&lt;P&gt;J-Link Host interface:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; USB&lt;/P&gt;&lt;P&gt;J-Link script:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; none&lt;/P&gt;&lt;P&gt;J-Link settings file:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; none&lt;/P&gt;&lt;P&gt;------Target related settings------&lt;/P&gt;&lt;P&gt;Target device:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; MK64FN1M0xxx12&lt;/P&gt;&lt;P&gt;Target interface:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; SWD&lt;/P&gt;&lt;P&gt;Target interface speed:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 1000kHz&lt;/P&gt;&lt;P&gt;Target endian:&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; little&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Connecting to J-Link...&lt;/P&gt;&lt;P&gt;J-Link is connected.&lt;/P&gt;&lt;P&gt;Firmware: J-Link OpenSDA 2 compiled Apr 24 2014 14:44:11&lt;/P&gt;&lt;P&gt;Hardware: V1.00&lt;/P&gt;&lt;P&gt;S/N: 621000000&lt;/P&gt;&lt;P&gt;Checking target voltage...&lt;/P&gt;&lt;P&gt;Target voltage: 3.30 V&lt;/P&gt;&lt;P&gt;Listening on TCP/IP port 2331&lt;/P&gt;&lt;P&gt;Connecting to target...Connected to target&lt;/P&gt;&lt;P&gt;Waiting for GDB connection...Connected to 127.0.0.1&lt;/P&gt;&lt;P&gt;Reading all registers&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0x00000000 (Data = 0xFFFFFFFF)&lt;/P&gt;&lt;P&gt;Target interface speed set to 1000 kHz&lt;/P&gt;&lt;P&gt;Resetting target&lt;/P&gt;&lt;P&gt;Halting target CPU...&lt;/P&gt;&lt;P&gt;...Target halted (PC = 0xFFFFFFFE)&lt;/P&gt;&lt;P&gt;R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000&lt;/P&gt;&lt;P&gt;R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000&lt;/P&gt;&lt;P&gt;R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000&lt;/P&gt;&lt;P&gt;R12= 00000000, R13= FFFFFFFC, MSP= FFFFFFFC, PSP= 00000000&lt;/P&gt;&lt;P&gt;R14(LR) = FFFFFFFF, R15(PC) = FFFFFFFE&lt;/P&gt;&lt;P&gt;XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000&lt;/P&gt;&lt;P&gt;CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00&lt;/P&gt;&lt;P&gt;Reading all registers&lt;/P&gt;&lt;P&gt;Select auto target interface speed (1429 kHz)&lt;/P&gt;&lt;P&gt;Flash breakpoints enabled&lt;/P&gt;&lt;P&gt;Semi-hosting enabled (VectorAddr = 0x08)&lt;/P&gt;&lt;P&gt;Semihosting I/O set to TELNET Client&lt;/P&gt;&lt;P&gt;Downloading 20 bytes @ address 0x00000410 - Verified OK&lt;/P&gt;&lt;P&gt;Writing register (PC = 0x00000410)&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0x00000410 (Data = 0x20000000)&lt;/P&gt;&lt;P&gt;Resetting target&lt;/P&gt;&lt;P&gt;Halting target CPU...&lt;/P&gt;&lt;P&gt;...Target halted (PC = 0xFFFFFFFE)&lt;/P&gt;&lt;P&gt;R0 = 00000000, R1 = 00000000, R2 = 00000000, R3 = 00000000&lt;/P&gt;&lt;P&gt;R4 = 00000000, R5 = 00000000, R6 = 00000000, R7 = 00000000&lt;/P&gt;&lt;P&gt;R8 = 00000000, R9 = 00000000, R10= 00000000, R11= 00000000&lt;/P&gt;&lt;P&gt;R12= 00000000, R13= FFFFFFFC, MSP= FFFFFFFC, PSP= 00000000&lt;/P&gt;&lt;P&gt;R14(LR) = FFFFFFFF, R15(PC) = FFFFFFFE&lt;/P&gt;&lt;P&gt;XPSR 01000000, APSR 00000000, EPSR 01000000, IPSR 00000000&lt;/P&gt;&lt;P&gt;CFBP 00000000, CONTROL 00, FAULTMASK 00, BASEPRI 00, PRIMASK 00&lt;/P&gt;&lt;P&gt;Reading all registers&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0xFFFFFFFE (Data = 0x20000000)&lt;/P&gt;&lt;P&gt;Starting target CPU...&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 15 (R15) while CPU is running&lt;/P&gt;&lt;P&gt;...Target halted (PC = 0x00000000)&lt;/P&gt;&lt;P&gt;Reading all registers&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 0 (R0) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 1 (R1) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 2 (R2) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 3 (R3) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 4 (R4) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 5 (R5) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 6 (R6) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 7 (R7) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 8 (R8) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 9 (R9) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 10 (R10) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 11 (R11) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 12 (R12) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 13 (R13) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 14 (R14) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 15 (R15) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 16 (XPSR) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 17 (MSP) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 18 (PSP) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 24 (PRIMASK) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 25 (BASEPRI) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 26 (FAULTMASK) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 27 (CONTROL) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 32 (FPSCR) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 33 (FPS0) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 34 (FPS1) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 35 (FPS2) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 36 (FPS3) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 37 (FPS4) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 38 (FPS5) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 39 (FPS6) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 40 (FPS7) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 41 (FPS8) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 42 (FPS9) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 43 (FPS10) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 44 (FPS11) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 45 (FPS12) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 46 (FPS13) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 47 (FPS14) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 48 (FPS15) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 49 (FPS16) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 50 (FPS17) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 51 (FPS18) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 52 (FPS19) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 53 (FPS20) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 54 (FPS21) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 55 (FPS22) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 56 (FPS23) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 57 (FPS24) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 58 (FPS25) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 59 (FPS26) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 60 (FPS27) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 61 (FPS28) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 62 (FPS29) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 63 (FPS30) while CPU is running&lt;/P&gt;&lt;P&gt;ERROR: Can not read register 64 (FPS31) while CPU is running&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0x00000000 (Data = 0xFFFFFFFF)&lt;/P&gt;&lt;P&gt;Read 4 bytes @ address 0x00000000 (Data = 0xFFFFFFFF)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;How can i solve this error? &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 12 Sep 2014 07:18:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351629#M11408</guid>
      <dc:creator>kevincarcel</dc:creator>
      <dc:date>2014-09-12T07:18:24Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351630#M11409</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek, thank you for posting your demo application.&amp;nbsp; I've been trying to create my own KDS project with the MQX for KDS SDK module using your walkthrough, and have been unsuccessful thus far.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I loaded your project and then switched the configuration to use the MK64FN1M0VLL12, since that's what my FRDM-K64F has.&amp;nbsp; The configuration switch went fine, but after code generation, building failed.&amp;nbsp; The error I got was:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Description&amp;nbsp;&amp;nbsp;&amp;nbsp; Resource&amp;nbsp;&amp;nbsp;&amp;nbsp; Path&amp;nbsp;&amp;nbsp;&amp;nbsp; Location&amp;nbsp;&amp;nbsp;&amp;nbsp; Type&lt;/P&gt;&lt;P&gt;fatal error: device/MK64F12/MK64F12.h: No such file or directory&amp;nbsp;&amp;nbsp;&amp;nbsp; fsl_device_registers.h&amp;nbsp;&amp;nbsp;&amp;nbsp; /MQX_KSDK_PEx/SDK/platform/CMSIS/Include/device&amp;nbsp;&amp;nbsp;&amp;nbsp; line 427&amp;nbsp;&amp;nbsp;&amp;nbsp; C/C++ Problem&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is the exact same error I get when I try to create my own project.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there something I could have missed?&amp;nbsp; I have all of the latest Eclipse updates installed.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 24 Sep 2014 17:57:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351630#M11409</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2014-09-24T17:57:35Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351631#M11410</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok, it seems that it is related to all of the packages installed on my system, or the fact that I specified the processor and not the board in the New Project wizard.&amp;nbsp; I reinstalled everything in a clean virtual machine just for testing, and it compiled.&amp;nbsp; Now the only problem is that I can't debug.&amp;nbsp; I set the -f kinetis.cfg build option, and when I try to debug I get this error:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Open On-Chip Debugger 0.8.0-dev-dirty (2014-08-20-11:07)&lt;/P&gt;&lt;P&gt;Licensed under GNU GPL v2&lt;/P&gt;&lt;P&gt;For bug reports, read&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/SPAN&gt;&lt;A class="jive-link-external-small" href="http://openocd.sourceforge.net/doc/doxygen/bugs.html"&gt;http://openocd.sourceforge.net/doc/doxygen/bugs.html&lt;/A&gt;&lt;/P&gt;&lt;P&gt;Info : only one transport option; autoselect 'cmsis-dap'&lt;/P&gt;&lt;P&gt;Error: unable to open CMSIS-DAP device&lt;/P&gt;&lt;P&gt;Error: unable to init CMSIS-DAP driver&lt;/P&gt;&lt;P&gt;Error: Error selecting 'cmsis-dap' as transport&lt;/P&gt;&lt;P&gt;Runtime Error: C:/Freescale/KDS_1.1.1/openocd/bin/..//scripts/kinetis.cfg:3: &lt;/P&gt;&lt;P&gt;in procedure 'script' &lt;/P&gt;&lt;P&gt;at file "embedded:startup.tcl", line 58&lt;/P&gt;&lt;P&gt;in procedure 'interface' called at file "C:/Freescale/KDS_1.1.1/openocd/bin/..//scripts/kinetis.cfg", line 3&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can anyone suggest a course of action?&amp;nbsp; &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 14:19:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351631#M11410</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2014-09-26T14:19:38Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351632#M11411</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think this is because you are still running the mbed code on your board. If you want to debug using the Segger J-Link you have to flash JLink_OpenSDA_V2.bin to the K20 on the board. To do that you hold down the reset while plugging in the USB cable. That should cause a BOOTLOADER USB Drive to show up on your laptop. You can then drag the JLink_OpenSDA_V2.bin to that device and it will flash the new image. Unplug and re-plug the USB and the Jlink code will expose a new virtual com port as well as a JLink debugger device. If you get the FRDM-K64-QSP.zip Quick Start Package from the Freescale web site there is a subdirectory for OpenSDAv2Applications that has a link to the Segger website with the code. Be sure you get the V2 version.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 14:44:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351632#M11411</guid>
      <dc:creator>intractablesubt</dc:creator>
      <dc:date>2014-09-26T14:44:11Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351633#M11412</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks, William, that hadn't ever occurred to me because of my debug configuration settings:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="kds_mqx_proj_debug_error.png"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/46273iCDF7E9AED7428EDA/image-size/large?v=v2&amp;amp;px=999" role="button" title="kds_mqx_proj_debug_error.png" alt="kds_mqx_proj_debug_error.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;I figured that if I selected OpenOCD, the mbed firmware would work fine.&amp;nbsp; Is this not the case?&amp;nbsp; Note that in this particular case, I followed the tutorial so I specified a debug config, as opposed to opening his project attachment.&amp;nbsp; Speaking of which, I'll try that next in the VM.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 14:48:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351633#M11412</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2014-09-26T14:48:28Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351634#M11413</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I think your choices, at least for the FRDM-K64F and the TWR-K64F120M, are to use the PE Micro OpenSDA or the Segger OpenSDA code. I'm using the Segger on my boards and it's working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 14:58:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351634#M11413</guid>
      <dc:creator>intractablesubt</dc:creator>
      <dc:date>2014-09-26T14:58:52Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351635#M11414</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Ok -- I'll load the Segger firmware onto one of my other boards so I can keep working in both environments.&amp;nbsp; Thanks for the suggestion!&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 26 Sep 2014 15:00:55 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351635#M11414</guid>
      <dc:creator>dave408</dc:creator>
      <dc:date>2014-09-26T15:00:55Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351636#M11415</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;thanks for the example.&lt;/P&gt;&lt;P&gt;Just a question:&lt;/P&gt;&lt;P&gt;every time I change something in PE and re-generate the code, it takes a huge amount of time (around 3 minutes) to recompile because it has&amp;nbsp; to recompile all the MQX files. Is there a way to speed up the compilation (in general, not only for this particular thing)?&lt;/P&gt;&lt;P&gt;In alternative is it possible to tell PE to generate the code only for the thing I changed and/or to block the generation of code for some components?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Bye Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Oct 2014 15:37:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351636#M11415</guid>
      <dc:creator>giacomopetrini</dc:creator>
      <dc:date>2014-10-28T15:37:48Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351637#M11416</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giacomo,&lt;/P&gt;&lt;P&gt;Open the Properties for your project.&lt;/P&gt;&lt;P&gt;Click on the C/C++ Build category.&lt;/P&gt;&lt;P&gt;Click on the Behavior tab.&lt;/P&gt;&lt;P&gt;Then check the “Enable parallel build” option.&lt;/P&gt;&lt;P&gt;Click Apply…the OK.&lt;/P&gt;&lt;P&gt;Re-build.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 28 Oct 2014 16:26:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351637#M11416</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2014-10-28T16:26:15Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351638#M11417</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;now it takes 1:45 to rebuild all (with 4 jobs). Better but still too long.&lt;/P&gt;&lt;P&gt;Any other ideas?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards&lt;/P&gt;&lt;P&gt;Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 14:56:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351638#M11417</guid>
      <dc:creator>giacomopetrini</dc:creator>
      <dc:date>2014-10-29T14:56:22Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351639#M11418</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Sorry no.&lt;/P&gt;&lt;P&gt;IDE's seem to be happy with fast machine and lots of RAM.&amp;nbsp; I have 8GB.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 15:10:24 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351639#M11418</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2014-10-29T15:10:24Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351640#M11419</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Here i5@2.5GHz(HT), 8GB RAM and SSD...mah&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Bye Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 29 Oct 2014 16:10:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351640#M11419</guid>
      <dc:creator>giacomopetrini</dc:creator>
      <dc:date>2014-10-29T16:10:58Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351641#M11420</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, thanks, the demo project works.&lt;BR /&gt;If I create more tasks, Their functions end up in mqx_tasks.c. How can I move the tasks funtions in others .c files?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you&lt;/P&gt;&lt;P&gt;Bye Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 30 Oct 2014 17:33:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351641#M11420</guid>
      <dc:creator>giacomopetrini</dc:creator>
      <dc:date>2014-10-30T17:33:43Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351642#M11421</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Giacomo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have you ever succeeded with Processor Expert putting MQX tasks in separate files?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Piotr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Nov 2014 16:18:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351642#M11421</guid>
      <dc:creator>piotrek</dc:creator>
      <dc:date>2014-11-04T16:18:47Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351643#M11422</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;no.&lt;/P&gt;&lt;P&gt;I tried (using MQX_KSDK_1.0.0beta) but when I add a file in the project the compilation fails (it seems that it can't find libc.a anymore). I don't know why.&lt;/P&gt;&lt;P&gt;Since I've no time to play, I decided to not use MQX for the time being and develope bare-metal (with the aid of PE).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;Giacomo&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 04 Nov 2014 19:58:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351643#M11422</guid>
      <dc:creator>giacomopetrini</dc:creator>
      <dc:date>2014-11-04T19:58:47Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351644#M11423</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello MQX team,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could we get some help here?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks,&lt;/P&gt;&lt;P&gt;Piotr&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 05 Nov 2014 01:21:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351644#M11423</guid>
      <dc:creator>piotrek</dc:creator>
      <dc:date>2014-11-05T01:21:11Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351645#M11424</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks for this demo. It works very good.&lt;/P&gt;&lt;P&gt;I'm trying to find a demo using Ethernet. Is this already in the pipe for MQX-KDS?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Nov 2014 12:58:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351645#M11424</guid>
      <dc:creator>ChrisTango</dc:creator>
      <dc:date>2014-11-23T12:58:34Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351646#M11425</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Chris&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;MQX for KSDK has Ethernet examples included in the installation. You'll find them in the directory /tcpip/RTCS/examples&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Nov 2014 15:10:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351646#M11425</guid>
      <dc:creator>dereksnell</dc:creator>
      <dc:date>2014-11-23T15:10:00Z</dc:date>
    </item>
    <item>
      <title>Re: MQX with KSDK and Processor Expert</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351647#M11426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Derek,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for this hint. In the demo attached to this thread RTCS isn't included. So, I downloaded the package for MQX; but this doesn't include KDS projects.&lt;/P&gt;&lt;P&gt;I'm now adding the RTCS files and updating the MQX files. Hopefuly this works out. After this I would be able to try the examples. :-)&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;-Chris&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sun, 23 Nov 2014 15:28:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-with-KSDK-and-Processor-Expert/m-p/351647#M11426</guid>
      <dc:creator>ChrisTango</dc:creator>
      <dc:date>2014-11-23T15:28:05Z</dc:date>
    </item>
  </channel>
</rss>