<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: USB 2.0 K70</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-2-0-K70/m-p/349327#M11263</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maurizio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only option to change the speed in a&amp;nbsp; usb device it is not by software it is by hardware, you need to add a pull-up resistor from D+ or D- depending of the speed, you want to select.&amp;nbsp; For a full speed device, the pull-up is attached to the D+ signal.&amp;nbsp; When the host detects this voltage change then it begins the enumeration process at the full speed rate.&amp;nbsp; If the voltage change is detected on the D- line, then the enumeration happens at low speed.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45167i4FAF6F7950262D20/image-size/large?v=v2&amp;amp;px=999" title="usbimage.png" alt="usbimage.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 06 Sep 2014 19:11:00 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2014-09-06T19:11:00Z</dc:date>
    <item>
      <title>USB 2.0 K70</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-2-0-K70/m-p/349326#M11262</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;hello&lt;/P&gt;&lt;P&gt;I'm using various micro-series Kinetis K70, K22 and MQX 4.0.2.&lt;/P&gt;&lt;P&gt;I'm using the USB, but I can not work with USB 2.0.&lt;/P&gt;&lt;P&gt;Communication is very slow.&lt;/P&gt;&lt;P&gt;Is there any change to the driver that allows you to work with the 2.0?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maurizio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 11 Aug 2014 08:33:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-2-0-K70/m-p/349326#M11262</guid>
      <dc:creator>Microfelix</dc:creator>
      <dc:date>2014-08-11T08:33:00Z</dc:date>
    </item>
    <item>
      <title>Re: USB 2.0 K70</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-2-0-K70/m-p/349327#M11263</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Maurizio,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The only option to change the speed in a&amp;nbsp; usb device it is not by software it is by hardware, you need to add a pull-up resistor from D+ or D- depending of the speed, you want to select.&amp;nbsp; For a full speed device, the pull-up is attached to the D+ signal.&amp;nbsp; When the host detects this voltage change then it begins the enumeration process at the full speed rate.&amp;nbsp; If the voltage change is detected on the D- line, then the enumeration happens at low speed.&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/45167i4FAF6F7950262D20/image-size/large?v=v2&amp;amp;px=999" title="usbimage.png" alt="usbimage.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 06 Sep 2014 19:11:00 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-2-0-K70/m-p/349327#M11263</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-09-06T19:11:00Z</dc:date>
    </item>
    <item>
      <title>Re: USB 2.0 K70</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/USB-2-0-K70/m-p/349328#M11264</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;dear SOL &lt;/P&gt;&lt;P&gt;I tried to put down pullup on D + and D-host. &lt;/P&gt;&lt;P&gt;With a pen-drive usb 2.0, I always loading very slow. &lt;/P&gt;&lt;P&gt;Should I do anything else?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Maurizio&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Sep 2014 07:08:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/USB-2-0-K70/m-p/349328#M11264</guid>
      <dc:creator>Microfelix</dc:creator>
      <dc:date>2014-09-08T07:08:22Z</dc:date>
    </item>
  </channel>
</rss>