<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Using MQX to generate timing pulses less than 1ms in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Using-MQX-to-generate-timing-pulses-less-than-1ms/m-p/348507#M11234</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to recommend hwtimer driver in this case.&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;P&gt;c:\Freescale\Freescale_MQX_4_1\mqx\examples\hwtimer\..&lt;/P&gt;&lt;P&gt;Source:&lt;/P&gt;&lt;P&gt;c:\Freescale\Freescale_MQX_4_1\mqx\source\io\hwtimer\..&lt;/P&gt;&lt;P&gt;Documentation:&lt;/P&gt;&lt;P&gt;c:\Freescale\Freescale_MQX_4_1\doc\mqx\MQX_IO_User_Guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Mar 2015 09:49:22 GMT</pubDate>
    <dc:creator>RadekS</dc:creator>
    <dc:date>2015-03-04T09:49:22Z</dc:date>
    <item>
      <title>Using MQX to generate timing pulses less than 1ms</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Using-MQX-to-generate-timing-pulses-less-than-1ms/m-p/348506#M11233</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I am working with a K60D100M processor and want to use the internal ADC to sample an analogue signal every 50us.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The timer functions I have used before like timer_start_periodic_at_ticks, don't seem too work when the intervals are less than 1 or 2ms.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is there an alternative timer function which will work when the period is in the region of 50us intervals...?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Ken&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 02 Mar 2015 08:55:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Using-MQX-to-generate-timing-pulses-less-than-1ms/m-p/348506#M11233</guid>
      <dc:creator>MWMinor</dc:creator>
      <dc:date>2015-03-02T08:55:31Z</dc:date>
    </item>
    <item>
      <title>Re: Using MQX to generate timing pulses less than 1ms</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Using-MQX-to-generate-timing-pulses-less-than-1ms/m-p/348507#M11234</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I would like to recommend hwtimer driver in this case.&lt;/P&gt;&lt;P&gt;Example:&lt;/P&gt;&lt;P&gt;c:\Freescale\Freescale_MQX_4_1\mqx\examples\hwtimer\..&lt;/P&gt;&lt;P&gt;Source:&lt;/P&gt;&lt;P&gt;c:\Freescale\Freescale_MQX_4_1\mqx\source\io\hwtimer\..&lt;/P&gt;&lt;P&gt;Documentation:&lt;/P&gt;&lt;P&gt;c:\Freescale\Freescale_MQX_4_1\doc\mqx\MQX_IO_User_Guide.pdf&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I hope it helps you.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Have a great day,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Mar 2015 09:49:22 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Using-MQX-to-generate-timing-pulses-less-than-1ms/m-p/348507#M11234</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2015-03-04T09:49:22Z</dc:date>
    </item>
  </channel>
</rss>