<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MQX 4.1.1 init_gpio.c potential bug in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-1-init-gpio-c-potential-bug/m-p/346594#M11178</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That conditional is an or-equal operation. The first line is setting the IRQC field in bits 16-19 and the second is setting the ISF bit 24 for PTC18. Looks like it is to be used as an external rising-edge interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The top two lines select alt function 4 for bits 8/9 on Port C which are I2S0 functions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 08 Sep 2014 16:23:38 GMT</pubDate>
    <dc:creator>razed11</dc:creator>
    <dc:date>2014-09-08T16:23:38Z</dc:date>
    <item>
      <title>MQX 4.1.1 init_gpio.c potential bug</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-1-init-gpio-c-potential-bug/m-p/346593#M11177</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;MQX 4.1.1 brings the following patch to the file mqx/source/bsp/twrk70f120m/init_gpio.c:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;SPAN style="font-family: terminal,monaco;"&gt;@@ -811,7 +811,11 @@&lt;/SPAN&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pctl-&amp;gt;PCR[18] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pctl-&amp;gt;PCR[19] = PORT_PCR_MUX(4) | PORT_PCR_ODE_MASK;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;-&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; /* Enable SDA rising edge detection */&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;+#if BSPCFG_ENABLE_LEGACY_II2C_SLAVE&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pctl-&amp;gt;PCR[18] |= PORT_PCR_IRQC(0x09);&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;+&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pctl-&amp;gt;PCR[18] |= PORT_PCR_ISF_MASK;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;+#endif&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; sim-&amp;gt;SCGC4 |= SIM_SCGC4_IIC0_MASK ;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; break;&lt;/P&gt;&lt;P style="padding-left: 30px;"&gt;&lt;/P&gt;&lt;P&gt;That visually seems to me like a potential bug, even though I have not examined it thoroughly. But as there are two lines in the conditioned block, I think it was meant to configure pins 18 and 19, not twice the same pin 18. Please correct me if I am wrong.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Sep 2014 09:52:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-1-init-gpio-c-potential-bug/m-p/346593#M11177</guid>
      <dc:creator>kubiznak_petr</dc:creator>
      <dc:date>2014-09-08T09:52:17Z</dc:date>
    </item>
    <item>
      <title>Re: MQX 4.1.1 init_gpio.c potential bug</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-1-init-gpio-c-potential-bug/m-p/346594#M11178</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;That conditional is an or-equal operation. The first line is setting the IRQC field in bits 16-19 and the second is setting the ISF bit 24 for PTC18. Looks like it is to be used as an external rising-edge interrupt.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The top two lines select alt function 4 for bits 8/9 on Port C which are I2S0 functions.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 08 Sep 2014 16:23:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-1-init-gpio-c-potential-bug/m-p/346594#M11178</guid>
      <dc:creator>razed11</dc:creator>
      <dc:date>2014-09-08T16:23:38Z</dc:date>
    </item>
  </channel>
</rss>