<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MQX Memory Direct Access ISSUE in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-Memory-Direct-Access-ISSUE/m-p/344073#M11078</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to double check. Do all the memory regions generate this problem?&lt;/P&gt;&lt;P&gt;After cheking the 0x020A_8000 address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"0x0080_0000-0x0fff_ffff 248 0x8080_0000 Reserved CM4 DDR code alias"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems to be resereve for the Cortex-A5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Mar 2015 21:10:05 GMT</pubDate>
    <dc:creator>alejandrolozan1</dc:creator>
    <dc:date>2015-03-30T21:10:05Z</dc:date>
    <item>
      <title>MQX Memory Direct Access ISSUE</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-Memory-Direct-Access-ISSUE/m-p/344072#M11077</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi, This is Sungho from South Korea.&lt;/P&gt;&lt;P&gt;I`m using 'i.mx6sx-sdb' board to build some application with PURE MQX BSP/PSP library(with no config modifications).&lt;/P&gt;&lt;P&gt;I`m wondering why Direct Memory Accessing to peripherals makes&amp;nbsp; 'MQX_AUTO_START_TASK' attributed Task stop...(may jumped to some exception handler...)&lt;/P&gt;&lt;P&gt;I didn`t set MQX_ENABLE_USER_MODE &amp;lt;= this #define when copmpiled with bsp.a/psp.a&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Is this MPU related issue? or Privileged Mode related issue? or RDC issue? or Clock Source Configure issue? :smileysad:&lt;/P&gt;&lt;P&gt;Memory Access Code is like this........reg = *(uint32_t *)0x020A8000;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regarding MPU and Privileged Mode,&lt;/P&gt;&lt;P&gt;I searched all the BSP code but could not find the MPU configuration section.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Need a Help...please&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Any replies will be appreciated.&lt;/P&gt;&lt;P&gt;Thanks.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 24 Mar 2015 09:12:49 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-Memory-Direct-Access-ISSUE/m-p/344072#M11077</guid>
      <dc:creator>sunghokim</dc:creator>
      <dc:date>2015-03-24T09:12:49Z</dc:date>
    </item>
    <item>
      <title>Re: MQX Memory Direct Access ISSUE</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-Memory-Direct-Access-ISSUE/m-p/344073#M11078</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I just want to double check. Do all the memory regions generate this problem?&lt;/P&gt;&lt;P&gt;After cheking the 0x020A_8000 address&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;"0x0080_0000-0x0fff_ffff 248 0x8080_0000 Reserved CM4 DDR code alias"&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;It seems to be resereve for the Cortex-A5.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;&lt;P&gt;Alejandro&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Mar 2015 21:10:05 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-Memory-Direct-Access-ISSUE/m-p/344073#M11078</guid>
      <dc:creator>alejandrolozan1</dc:creator>
      <dc:date>2015-03-30T21:10:05Z</dc:date>
    </item>
  </channel>
</rss>