<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Issue with TWRK70F120M</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340587#M10977</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two queries regarding K70 tower board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.       I am using K70 tower board and MQX 4.0 for developing my application. I using PE Micro Multilink Debugger to load the program to tower board. Now I have a customized prototype board when I try to load my program the program goes and gets stuck in "boot.s" file.&lt;/P&gt;&lt;P&gt;Kindly tell me if any changes are required for my code to be loaded into the prototype board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.       I'm also trying to load the demo program which is present the mentioned path "\Freescale_MQX_4_0\mqx\examples\hello\iar\hello_twrk70f120m".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I load the above demo program into SRAM of MCU of the prototype board the program is working fine, but when I load the program into DDR DRAM of the MCU, the CPU is getting reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please help me identify the issue at hand? Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Sneha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 26 Feb 2015 08:49:09 GMT</pubDate>
    <dc:creator>snehahegde</dc:creator>
    <dc:date>2015-02-26T08:49:09Z</dc:date>
    <item>
      <title>Issue with TWRK70F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340587#M10977</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I have two queries regarding K70 tower board.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;1.       I am using K70 tower board and MQX 4.0 for developing my application. I using PE Micro Multilink Debugger to load the program to tower board. Now I have a customized prototype board when I try to load my program the program goes and gets stuck in "boot.s" file.&lt;/P&gt;&lt;P&gt;Kindly tell me if any changes are required for my code to be loaded into the prototype board?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;2.       I'm also trying to load the demo program which is present the mentioned path "\Freescale_MQX_4_0\mqx\examples\hello\iar\hello_twrk70f120m".&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;When I load the above demo program into SRAM of MCU of the prototype board the program is working fine, but when I load the program into DDR DRAM of the MCU, the CPU is getting reset.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Can you please help me identify the issue at hand? Thanks in advance.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks and Regards,&lt;/P&gt;&lt;P&gt;Sneha&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 26 Feb 2015 08:49:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340587#M10977</guid>
      <dc:creator>snehahegde</dc:creator>
      <dc:date>2015-02-26T08:49:09Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with TWRK70F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340588#M10978</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sneha,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The MQX libraries (BSP and PSP) were designed for our Freescale boards, if you are using a custom board then you need to modify these libraries according your needs.&lt;/P&gt;&lt;P&gt;Did you change something, for example the clock configuration??&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol &lt;BR /&gt; &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 27 Feb 2015 18:37:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340588#M10978</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-02-27T18:37:44Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with TWRK70F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340589#M10979</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt;Hi,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt;I have not changed anything in the BSP or the PSP. Please let us&lt;BR /&gt;know what needs to be changed.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt;Thanks and Regards,&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt;Sneha &lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #1f497d; font-family: 'Calibri','sans-serif'; font-size: 11pt;"&gt; &lt;/SPAN&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 10 Mar 2015 11:09:11 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340589#M10979</guid>
      <dc:creator>snehahegde</dc:creator>
      <dc:date>2015-03-10T11:09:11Z</dc:date>
    </item>
    <item>
      <title>Re: Issue with TWRK70F120M</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340590#M10980</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello Sneha,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Could you please share the schematic file in order to check the modifications that you have?&lt;/P&gt;&lt;P&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Soledad&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 11 Mar 2015 20:58:48 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Issue-with-TWRK70F120M/m-p/340590#M10980</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-03-11T20:58:48Z</dc:date>
    </item>
  </channel>
</rss>