<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: max size for nandflash,usb,sdcard in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/max-size-for-nandflash-usb-sdcard/m-p/338767#M10914</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi T Tech,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a trick question since it is also dependant on the hardware side, for the K60 we have the following limits:&lt;/P&gt;&lt;P&gt;A) NandFlash it has been tested with 2Gbits but the limit it is on the K60 hardware.&lt;/P&gt;&lt;P&gt;B) USB. we have tested using 64GB usb stick drive.&lt;/P&gt;&lt;P&gt;C) Since the K60 it is Using SDHC the max allow with this technology is 32Gb . We have tested with 8G without issues.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 06 Aug 2014 17:51:35 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2014-08-06T17:51:35Z</dc:date>
    <item>
      <title>max size for nandflash,usb,sdcard</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/max-size-for-nandflash-usb-sdcard/m-p/338766#M10913</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hello everyone,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am using MQX4.1, CW10.6 &amp;amp; MK60FX512VLQ12 controller on our custom board.&lt;/P&gt;&lt;P&gt;I have interfaced nandflash (2Gb), USB(4GB) &amp;amp; sdcard(4GB) to controller.&lt;/P&gt;&lt;P&gt;I wanted to know the maximum size limit for all these&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt; to interface with the controller.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;Anyone knows about this?&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;1) nandflash-&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="font-size: 10pt; line-height: 1.5em;"&gt;2) usb-&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;3) sd card-&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 09:27:47 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/max-size-for-nandflash-usb-sdcard/m-p/338766#M10913</guid>
      <dc:creator>ava</dc:creator>
      <dc:date>2014-08-06T09:27:47Z</dc:date>
    </item>
    <item>
      <title>Re: max size for nandflash,usb,sdcard</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/max-size-for-nandflash-usb-sdcard/m-p/338767#M10914</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi T Tech,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is a trick question since it is also dependant on the hardware side, for the K60 we have the following limits:&lt;/P&gt;&lt;P&gt;A) NandFlash it has been tested with 2Gbits but the limit it is on the K60 hardware.&lt;/P&gt;&lt;P&gt;B) USB. we have tested using 64GB usb stick drive.&lt;/P&gt;&lt;P&gt;C) Since the K60 it is Using SDHC the max allow with this technology is 32Gb . We have tested with 8G without issues.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 06 Aug 2014 17:51:35 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/max-size-for-nandflash-usb-sdcard/m-p/338767#M10914</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-08-06T17:51:35Z</dc:date>
    </item>
    <item>
      <title>Re: max size for nandflash,usb,sdcard</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/max-size-for-nandflash-usb-sdcard/m-p/338768#M10915</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Sol,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&lt;/P&gt;&lt;P&gt;I have more doubts&lt;/P&gt;&lt;P&gt;1) the limitation for nandflash,usb &amp;amp; sdcard is at K60 hardware side&amp;nbsp; not with MQX.&lt;/P&gt;&lt;P&gt;2) on TWRK60F120M I have tested nandflash(2Gb which is already there),usb (8GB) with MQX4.1&lt;/P&gt;&lt;P&gt;And on my custom board (with MK60FX512VLQ12), circuit is same as TWRK60F120M I am able to use usb of 4GB only if I connected 8GB usb stick, its not detecting the usb stick.&lt;/P&gt;&lt;P&gt;Please let me know what may be the problem because circuit is same &amp;amp; code is also same.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for the reply.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 07 Aug 2014 05:14:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/max-size-for-nandflash-usb-sdcard/m-p/338768#M10915</guid>
      <dc:creator>ava</dc:creator>
      <dc:date>2014-08-07T05:14:54Z</dc:date>
    </item>
  </channel>
</rss>