<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCF54418 Use 8bit NAND falsh in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF54418-Use-8bit-NAND-falsh/m-p/329445#M10530</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We now use a board based on MCF54418,and its circuit is the same as development board（TWR-MCF5441x (700-26131)）bought from freescale。The NAND flash is 16bit IC MT29F2G16AADWP . But now,we want change NAND flash to 8bit MT29F2G08ABAEAWP‐IT because of its lifecycle. My question is what should be change with the Program？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 29 Jan 2015 02:04:07 GMT</pubDate>
    <dc:creator>eric_wu</dc:creator>
    <dc:date>2015-01-29T02:04:07Z</dc:date>
    <item>
      <title>MCF54418 Use 8bit NAND falsh</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF54418-Use-8bit-NAND-falsh/m-p/329445#M10530</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;We now use a board based on MCF54418,and its circuit is the same as development board（TWR-MCF5441x (700-26131)）bought from freescale。The NAND flash is 16bit IC MT29F2G16AADWP . But now,we want change NAND flash to 8bit MT29F2G08ABAEAWP‐IT because of its lifecycle. My question is what should be change with the Program？&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 02:04:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MCF54418-Use-8bit-NAND-falsh/m-p/329445#M10530</guid>
      <dc:creator>eric_wu</dc:creator>
      <dc:date>2015-01-29T02:04:07Z</dc:date>
    </item>
    <item>
      <title>Re: MCF54418 Use 8bit NAND falsh</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF54418-Use-8bit-NAND-falsh/m-p/329446#M10531</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Eric,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;We support an 8-bit wide NAND flash in TWRMPC5125 BSP with the same Freescale MQX NAND flash driver. So the driver, in general, can work with an 8-bit flash. It’s just a task of proper configuration of the MCU (pins, NFC module) according to your specific NAND flash device. I think you can follow the configuration NANDFLASH_INIT_STRUCT and NANDFLASH_INFO_STRUCT that is provided with the twrmpc5125 BSP as an example. Double check the configuration of pin functions, and reflect the difference between the NAND flash device used on TWR-MPC5125 (c:\Freescale\Freescale&lt;/P&gt;&lt;P&gt;MQX 3.x\mqx\source\io\nandflash\nand_devices\MT29F32G08.c) and your’s.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol &lt;BR /&gt; &lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 29 Jan 2015 17:06:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MCF54418-Use-8bit-NAND-falsh/m-p/329446#M10531</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2015-01-29T17:06:45Z</dc:date>
    </item>
    <item>
      <title>Re: MCF54418 Use 8bit NAND falsh</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MCF54418-Use-8bit-NAND-falsh/m-p/329447#M10532</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Dear Sol:&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt; MT29F2G16AADWP&lt;/SPAN&gt; is well used on our board.Some days ago i have tried to change it to &lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;MT29F2G08AADWP which only has a difference of bit wide(8bit &amp;amp; 16bit). About the code , i have just change "#define MT29F2G16_WIDTH&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; 16" to "8" in MT29F2G16.c as below. But it does not work.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN style="color: #3d3d3d; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif;"&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; So I am very &lt;SPAN style="color: #434343; font-family: Tahoma, Arial; font-size: 12px; background-color: #f2f2f2;"&gt;confused for a long time&lt;/SPAN&gt;. Is there anything else should be change?&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/49757iABBE0397BB404336/image-size/large?v=v2&amp;amp;px=999" title="001.PNG.png" alt="001.PNG.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 30 Jan 2015 01:13:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MCF54418-Use-8bit-NAND-falsh/m-p/329447#M10532</guid>
      <dc:creator>eric_wu</dc:creator>
      <dc:date>2015-01-30T01:13:57Z</dc:date>
    </item>
  </channel>
</rss>