<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: ftpd.h is missing in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/ftpd-h-is-missing/m-p/329316#M10520</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui Shao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MQX4.1 you need to write your code using FTPSRV. Unfortunately there is no way to use FTPD. &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;FTPD&lt;/SPAN&gt; was discontinued and FTDPSRV is recommended for new application.&lt;/P&gt;&lt;P&gt;Here is short summary of RTCS 4.1.0 enhancements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• New HTTP server implementation – HTTPSRV.&lt;/P&gt;&lt;P&gt;o It is 18 times faster than old &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;MQX&lt;/SPAN&gt; 4.0 HTTPD.&lt;/P&gt;&lt;P&gt;o Allows parallel CGI processing.&lt;/P&gt;&lt;P&gt;o More robust (pass „long run/many sessions“ kind of stress test)&lt;/P&gt;&lt;P&gt;o User code (CGI/SSI) is run in separate task.&lt;/P&gt;&lt;P&gt;o Each CGI/SSI can run in separate task.&lt;/P&gt;&lt;P&gt;o Each connection is processed independenly.&lt;/P&gt;&lt;P&gt;o Enables plugin usage – used by WebSocket implementation.&lt;/P&gt;&lt;P&gt;o Normalised API (HTTPSRV_init() and HTTPSRV_release())&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• New FTP server implementation – FTPSRV.&lt;/P&gt;&lt;P&gt;o Allows multiple connections.&lt;/P&gt;&lt;P&gt;o Allows multiple parallel file transfers.&lt;/P&gt;&lt;P&gt;o Full IPv6 support (EPSV and EPRT commands).&lt;/P&gt;&lt;P&gt;o Normalised API (FTPSRV_init() and FTPSRV_release())&lt;/P&gt;&lt;P&gt;o More robust.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• Added Multicast Listener Discovery (MLDv1) protocol for IPv6.&lt;/P&gt;&lt;P&gt;• Added socket options to join and leave IPv6 multicast groups.&lt;/P&gt;&lt;P&gt;• Added DNS Client for IPv4 and IPv6.&lt;/P&gt;&lt;P&gt;o IPv4 and IPv6 name resolving is done by the getaddrinfo() function.&lt;/P&gt;&lt;P&gt;• API for DNSv6 address list configuration.&lt;/P&gt;&lt;P&gt;• Added Recursive DNS IPv6 Server (RDNSS) option support to Router Discovery.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 18 Sep 2014 23:53:44 GMT</pubDate>
    <dc:creator>soledad</dc:creator>
    <dc:date>2014-09-18T23:53:44Z</dc:date>
    <item>
      <title>ftpd.h is missing</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/ftpd-h-is-missing/m-p/329315#M10519</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi -&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In older version of MQX, there is a ftpd.h in rtcs\source\include. MQX 4.1.1 doesn't have such a file and causes many compiler errors.&lt;/P&gt;&lt;P&gt;How to resolve the compatibility issue?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hui&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 19:08:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/ftpd-h-is-missing/m-p/329315#M10519</guid>
      <dc:creator>huishao2</dc:creator>
      <dc:date>2014-09-18T19:08:46Z</dc:date>
    </item>
    <item>
      <title>Re: ftpd.h is missing</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/ftpd-h-is-missing/m-p/329316#M10520</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Hui Shao,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;In MQX4.1 you need to write your code using FTPSRV. Unfortunately there is no way to use FTPD. &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;FTPD&lt;/SPAN&gt; was discontinued and FTDPSRV is recommended for new application.&lt;/P&gt;&lt;P&gt;Here is short summary of RTCS 4.1.0 enhancements.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• New HTTP server implementation – HTTPSRV.&lt;/P&gt;&lt;P&gt;o It is 18 times faster than old &lt;SPAN class="&amp;amp;quothighlight&amp;quot;"&gt;MQX&lt;/SPAN&gt; 4.0 HTTPD.&lt;/P&gt;&lt;P&gt;o Allows parallel CGI processing.&lt;/P&gt;&lt;P&gt;o More robust (pass „long run/many sessions“ kind of stress test)&lt;/P&gt;&lt;P&gt;o User code (CGI/SSI) is run in separate task.&lt;/P&gt;&lt;P&gt;o Each CGI/SSI can run in separate task.&lt;/P&gt;&lt;P&gt;o Each connection is processed independenly.&lt;/P&gt;&lt;P&gt;o Enables plugin usage – used by WebSocket implementation.&lt;/P&gt;&lt;P&gt;o Normalised API (HTTPSRV_init() and HTTPSRV_release())&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• New FTP server implementation – FTPSRV.&lt;/P&gt;&lt;P&gt;o Allows multiple connections.&lt;/P&gt;&lt;P&gt;o Allows multiple parallel file transfers.&lt;/P&gt;&lt;P&gt;o Full IPv6 support (EPSV and EPRT commands).&lt;/P&gt;&lt;P&gt;o Normalised API (FTPSRV_init() and FTPSRV_release())&lt;/P&gt;&lt;P&gt;o More robust.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;• Added Multicast Listener Discovery (MLDv1) protocol for IPv6.&lt;/P&gt;&lt;P&gt;• Added socket options to join and leave IPv6 multicast groups.&lt;/P&gt;&lt;P&gt;• Added DNS Client for IPv4 and IPv6.&lt;/P&gt;&lt;P&gt;o IPv4 and IPv6 name resolving is done by the getaddrinfo() function.&lt;/P&gt;&lt;P&gt;• API for DNSv6 address list configuration.&lt;/P&gt;&lt;P&gt;• Added Recursive DNS IPv6 Server (RDNSS) option support to Router Discovery.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 18 Sep 2014 23:53:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/ftpd-h-is-missing/m-p/329316#M10520</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-09-18T23:53:44Z</dc:date>
    </item>
  </channel>
</rss>