<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software Solutions中的主题 Re: K40 MQX SPI</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/K40-MQX-SPI/m-p/329007#M10512</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Carlos! I can see the clock signal. Any idea how I can change the pin mapping? Also, do you know which part of the code I should modify to get a different set of data out of the MOSI pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 05 Aug 2014 15:42:33 GMT</pubDate>
    <dc:creator>edsonsanchez</dc:creator>
    <dc:date>2014-08-05T15:42:33Z</dc:date>
    <item>
      <title>K40 MQX SPI</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/K40-MQX-SPI/m-p/329005#M10510</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am working with the K40 tower and was able to build and debug the example SPI project in the MQX directory. I realize that this example is supposed to transfer data to an external memory device. I was hoping I would be able to see at least a clock signal on one of the SPI pins, but I don't. Am I supposed to see anything or do I have to do something before I can actually see a clock signal?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I was also hoping to be able to use this example project to later change the data sent out and the device I send to. Where would I make these changes?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 31 Jul 2014 23:34:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/K40-MQX-SPI/m-p/329005#M10510</guid>
      <dc:creator>edsonsanchez</dc:creator>
      <dc:date>2014-07-31T23:34:20Z</dc:date>
    </item>
    <item>
      <title>Re: K40 MQX SPI</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/K40-MQX-SPI/m-p/329006#M10511</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Edson,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;you dont need special settings to see SPI clock. I was able to see this signal in oscilloscope, you can use the side expansion port connectors in the external side of TWR-ELEVATOR, many pins are mapped here. You can check the port number where each pinn is mapped in the TWR-K40 schematic, in this case SPI0_SCK is mapped to port B15 and SPI1_SCK to B7.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope this helps,&lt;/P&gt;&lt;P&gt;Carlos &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 04 Aug 2014 16:19:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/K40-MQX-SPI/m-p/329006#M10511</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2014-08-04T16:19:58Z</dc:date>
    </item>
    <item>
      <title>Re: K40 MQX SPI</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/K40-MQX-SPI/m-p/329007#M10512</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks Carlos! I can see the clock signal. Any idea how I can change the pin mapping? Also, do you know which part of the code I should modify to get a different set of data out of the MOSI pin?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Edson&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 05 Aug 2014 15:42:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/K40-MQX-SPI/m-p/329007#M10512</guid>
      <dc:creator>edsonsanchez</dc:creator>
      <dc:date>2014-08-05T15:42:33Z</dc:date>
    </item>
  </channel>
</rss>