<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic FFS nand flash demo fails during initialization in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/FFS-nand-flash-demo-fails-during-initialization/m-p/328597#M10466</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I have built MQX 3.8 FFS library and demo project for executing on an MPC5125 custom board. When I typed 'fsopen' shell command for initializing&amp;nbsp; the file system, It gets unresponsive. With printf debugging, I found that it stops right after this line in Media_init() function: (file: ffs\source\wearleveling\ddi_ldl\ddi_ldl_init.cpp)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;LogicalMedia * media = new nand::Media();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The new operator does not return. So is it something related to memory allocation? I have run the MQX cplus example project without any error. Is there something specific in the FFS library or demo project that I need to change for the MPC5125 platform, like linker file settings for proper C++ operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 23 Feb 2015 07:37:54 GMT</pubDate>
    <dc:creator>visakhanc</dc:creator>
    <dc:date>2015-02-23T07:37:54Z</dc:date>
    <item>
      <title>FFS nand flash demo fails during initialization</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/FFS-nand-flash-demo-fails-during-initialization/m-p/328597#M10466</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp; I have built MQX 3.8 FFS library and demo project for executing on an MPC5125 custom board. When I typed 'fsopen' shell command for initializing&amp;nbsp; the file system, It gets unresponsive. With printf debugging, I found that it stops right after this line in Media_init() function: (file: ffs\source\wearleveling\ddi_ldl\ddi_ldl_init.cpp)&lt;/P&gt;&lt;P&gt;&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P&gt;LogicalMedia * media = new nand::Media();&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The new operator does not return. So is it something related to memory allocation? I have run the MQX cplus example project without any error. Is there something specific in the FFS library or demo project that I need to change for the MPC5125 platform, like linker file settings for proper C++ operation?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks for any help&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 23 Feb 2015 07:37:54 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/FFS-nand-flash-demo-fails-during-initialization/m-p/328597#M10466</guid>
      <dc:creator>visakhanc</dc:creator>
      <dc:date>2015-02-23T07:37:54Z</dc:date>
    </item>
  </channel>
</rss>