<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: KSDK and D-Flash in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/KSDK-and-D-Flash/m-p/327588#M10428</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well Yes, I'm using a FRDM-K64 board so the example contains partly what I was looking for. Problem with these examples are to integrate into your own project, and what I wanted to do was to use FlexRAM to emulate an EEPROM, but it seems that the FRDM-K64 uC doesn't have FlexRAM.:smileysad:.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 12 Nov 2014 08:12:21 GMT</pubDate>
    <dc:creator>oaf</dc:creator>
    <dc:date>2014-11-12T08:12:21Z</dc:date>
    <item>
      <title>KSDK and D-Flash</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KSDK-and-D-Flash/m-p/327586#M10426</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;I could not find any example or documentation regarding the use of D-Flash under MQX/KSDK.&lt;/P&gt;&lt;P&gt;I suppose that the D-Flash has to be partitioned before use, so I could just not use raw&lt;/P&gt;&lt;P&gt;memory in the area 0x1400.0000 -&amp;gt; 0x1400.0fff ?&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 14:33:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KSDK-and-D-Flash/m-p/327586#M10426</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2014-11-10T14:33:18Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK and D-Flash</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KSDK-and-D-Flash/m-p/327587#M10427</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Ole,&lt;/P&gt;&lt;P&gt;What device are you using?&lt;/P&gt;&lt;P&gt;For the FRDM-K64F120M please reference the following:&lt;/P&gt;&lt;P&gt;There are two areas you can look at.&lt;/P&gt;&lt;P&gt;First is KDS/KSDK flash demo: C:\Freescale\MQX_KSDK_1.0.0\demos\flash_demo\kds\frdmk64f120m &lt;/P&gt;&lt;P&gt;Second is the flash driver document and source code:&lt;/P&gt;&lt;P&gt;C:\Freescale\MQX_KSDK_1.0.0\platform\drivers\flash\C90TFS\FSL_eNVM_FTFx_UM.pdf &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;The flash demo is actually doing a flash swap example but it also erasing and writing to flash so a good multipurpose demo.&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;David &lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 10 Nov 2014 16:18:33 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KSDK-and-D-Flash/m-p/327587#M10427</guid>
      <dc:creator>DavidS</dc:creator>
      <dc:date>2014-11-10T16:18:33Z</dc:date>
    </item>
    <item>
      <title>Re: KSDK and D-Flash</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/KSDK-and-D-Flash/m-p/327588#M10428</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Well Yes, I'm using a FRDM-K64 board so the example contains partly what I was looking for. Problem with these examples are to integrate into your own project, and what I wanted to do was to use FlexRAM to emulate an EEPROM, but it seems that the FRDM-K64 uC doesn't have FlexRAM.:smileysad:.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 12 Nov 2014 08:12:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/KSDK-and-D-Flash/m-p/327588#M10428</guid>
      <dc:creator>oaf</dc:creator>
      <dc:date>2014-11-12T08:12:21Z</dc:date>
    </item>
  </channel>
</rss>