<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Cannot debug internal RAM DS-5 Vybrid projects.  External RAM works. in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324691#M10354</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;found the issue.&lt;/P&gt;&lt;P&gt;looks like this does not work for DS-5 so I commented out the #error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#if&lt;/STRONG&gt;&lt;/SPAN&gt; __IAR_SYSTEMS_ICC__&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#pragma&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN class="s2"&gt; section = &lt;/SPAN&gt;"KERNEL_DATA"&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; BSP_DEFAULT_START_OF_KERNEL_MEMORY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((&lt;SPAN class="s1"&gt;&lt;STRONG&gt;void&lt;/STRONG&gt;&lt;/SPAN&gt; *)__sfb(&lt;SPAN class="s3"&gt;"KERNEL_DATA"&lt;/SPAN&gt;))&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#elif&lt;/STRONG&gt;&lt;/SPAN&gt; defined(__CC_ARM)&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; BSP_DEFAULT_START_OF_KERNEL_MEMORY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((&lt;SPAN class="s1"&gt;&lt;STRONG&gt;void&lt;/STRONG&gt;&lt;/SPAN&gt; *)__KERNEL_DATA_START)&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#elif&lt;/STRONG&gt;&lt;/SPAN&gt; defined(__GNUC__)&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; BSP_DEFAULT_START_OF_KERNEL_MEMORY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((&lt;SPAN class="s1"&gt;&lt;STRONG&gt;void&lt;/STRONG&gt;&lt;/SPAN&gt; *)__KERNEL_DATA_START)&lt;/P&gt;&lt;P class="p2"&gt;&lt;STRONG&gt;#else&lt;/STRONG&gt;&lt;/P&gt;&lt;P class="p5"&gt;//#error UNKNOWN COMPILER - IMPLEMENT ME!!!&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; BSP_DEFAULT_START_OF_KERNEL_MEMORY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((&lt;SPAN class="s1"&gt;&lt;STRONG&gt;void&lt;/STRONG&gt;&lt;/SPAN&gt; *)__KERNEL_DATA_START)&lt;/P&gt;&lt;P class="p4"&gt;&lt;STRONG&gt;#endif&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Thu, 24 Jul 2014 21:27:57 GMT</pubDate>
    <dc:creator>rocketdawg</dc:creator>
    <dc:date>2014-07-24T21:27:57Z</dc:date>
    <item>
      <title>Cannot debug internal RAM DS-5 Vybrid projects.  External RAM works.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324690#M10353</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;using 4.1.0.1&lt;/P&gt;&lt;P&gt;DS-5 5.19&lt;/P&gt;&lt;P&gt;using TWR-VF65GS10 dev board&lt;/P&gt;&lt;P&gt;I can build hello world or other projects and choose internal RAM or external RAM debug&lt;/P&gt;&lt;P&gt;external RAM works&lt;/P&gt;&lt;P&gt;internal RAM gives error something like this.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Stopping running target Freescale - Vybrid VF6xx on TCP:localhost on connection&lt;/P&gt;&lt;P&gt;Connected to running target Freescale - Vybrid VF6xx on TCP:localhost&lt;/P&gt;&lt;P&gt;Execution stopped at: S:0x8003984C&lt;/P&gt;&lt;P&gt;loadfile "C:\Freescale\Freescale_MQX_4_1\usb\host\examples\hid\keyboard\build\ds5\hid_kbd_twrvf65gs10_a5\Int Ram Debug\hid_kbd.axf"&lt;/P&gt;&lt;P&gt;S:0x8003984C&amp;nbsp;&amp;nbsp; MOV&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; pc,lr&lt;/P&gt;&lt;P&gt;Target Message: Memory access caused precise abort.&lt;/P&gt;&lt;P&gt;Debug Precise Abort Registers : DFSR = 0x00000805, DFAR = 0x3F000000&lt;/P&gt;&lt;P&gt;ERROR(CMD16-TAD274-NAL18): &lt;/P&gt;&lt;P&gt;! Failed to load "hid_kbd.axf"&lt;/P&gt;&lt;P&gt;! Failed to write 105,808 bytes to address S:0x3F000000 while writing block of 4,096 bytes to address S:0x3F000000&lt;/P&gt;&lt;P&gt;! Bus error on memory operation.&lt;/P&gt;&lt;P&gt;cd "C:\Users\dthedens\Documents\DS-5Workspace2"&lt;/P&gt;&lt;P&gt;Working directory "C:\Users\dthedens\Documents\DS-5Workspace2"&lt;/P&gt;&lt;P&gt;set debug-from main&lt;/P&gt;&lt;P&gt;start&lt;/P&gt;&lt;P&gt;WARNING(CMD399-COR168): &lt;/P&gt;&lt;P&gt;! Failed to start the target&lt;/P&gt;&lt;P&gt;! No function named "main" could be found&lt;/P&gt;&lt;P&gt;WARNING(CMD407): Trying the entry point instead&lt;/P&gt;&lt;P&gt;ERROR(CMD426): Cannot find symbol to start or entrypoint, the file or load commands may be used to set the entrypoint&lt;/P&gt;&lt;P&gt;wait&lt;/P&gt;&lt;P&gt;core 1&lt;/P&gt;&lt;P&gt;Current core is 1 (ID 1) - stopped in [S:0x8003984C]&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 18:32:17 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324690#M10353</guid>
      <dc:creator>rocketdawg</dc:creator>
      <dc:date>2014-07-24T18:32:17Z</dc:date>
    </item>
    <item>
      <title>Re: Cannot debug internal RAM DS-5 Vybrid projects.  External RAM works.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324691#M10354</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;found the issue.&lt;/P&gt;&lt;P&gt;looks like this does not work for DS-5 so I commented out the #error&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#if&lt;/STRONG&gt;&lt;/SPAN&gt; __IAR_SYSTEMS_ICC__&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#pragma&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;SPAN class="s2"&gt; section = &lt;/SPAN&gt;"KERNEL_DATA"&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; BSP_DEFAULT_START_OF_KERNEL_MEMORY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((&lt;SPAN class="s1"&gt;&lt;STRONG&gt;void&lt;/STRONG&gt;&lt;/SPAN&gt; *)__sfb(&lt;SPAN class="s3"&gt;"KERNEL_DATA"&lt;/SPAN&gt;))&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#elif&lt;/STRONG&gt;&lt;/SPAN&gt; defined(__CC_ARM)&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; BSP_DEFAULT_START_OF_KERNEL_MEMORY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((&lt;SPAN class="s1"&gt;&lt;STRONG&gt;void&lt;/STRONG&gt;&lt;/SPAN&gt; *)__KERNEL_DATA_START)&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#elif&lt;/STRONG&gt;&lt;/SPAN&gt; defined(__GNUC__)&lt;/P&gt;&lt;P class="p2"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; BSP_DEFAULT_START_OF_KERNEL_MEMORY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((&lt;SPAN class="s1"&gt;&lt;STRONG&gt;void&lt;/STRONG&gt;&lt;/SPAN&gt; *)__KERNEL_DATA_START)&lt;/P&gt;&lt;P class="p2"&gt;&lt;STRONG&gt;#else&lt;/STRONG&gt;&lt;/P&gt;&lt;P class="p5"&gt;//#error UNKNOWN COMPILER - IMPLEMENT ME!!!&lt;/P&gt;&lt;P class="p1"&gt;&lt;SPAN class="s1"&gt;&lt;STRONG&gt;#define&lt;/STRONG&gt;&lt;/SPAN&gt; BSP_DEFAULT_START_OF_KERNEL_MEMORY&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; ((&lt;SPAN class="s1"&gt;&lt;STRONG&gt;void&lt;/STRONG&gt;&lt;/SPAN&gt; *)__KERNEL_DATA_START)&lt;/P&gt;&lt;P class="p4"&gt;&lt;STRONG&gt;#endif&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 24 Jul 2014 21:27:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324691#M10354</guid>
      <dc:creator>rocketdawg</dc:creator>
      <dc:date>2014-07-24T21:27:57Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Cannot debug internal RAM DS-5 Vybrid projects.  External RAM works.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324692#M10355</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi David,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Please check the document attached, this may helps.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Have a great day,&lt;BR /&gt; Sol&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 15:38:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324692#M10355</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-07-25T15:38:18Z</dc:date>
    </item>
    <item>
      <title>Re: Re: Cannot debug internal RAM DS-5 Vybrid projects.  External RAM works.</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324693#M10356</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Thanks&lt;/P&gt;&lt;P&gt;I think that separate documents for different tools/dev kits is a better way to go.&lt;/P&gt;&lt;P&gt;I hope these make their way into the next release.&lt;/P&gt;&lt;P&gt;The topics are similar in the "one size fits all" "Getting Started with Freescale MQX™ RTOS Rev. 15" document in the ./docs directory.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;One thing I noticed is, section 3.1 the second screen shot is not what I see in DS-5.19&lt;/P&gt;&lt;P&gt;the "Bare Metal Debug" only has entries for A5 or M4 and the "Target Connection" is a dialog box that selects CMSIS-DAT, ULINK Pro, ULINKPro D.&amp;nbsp;&amp;nbsp; interesting, no DSTREAM.&lt;/P&gt;&lt;P&gt;you might want to update that screen shot&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;this document is missing all the content about the twrvf65gs10&amp;nbsp; jumper selections for USB and the serial port found in&lt;/P&gt;&lt;P&gt;Getting Started with Freescale MQX™ RTOS Rev. 15 section 8.1.2&lt;/P&gt;&lt;P&gt;If this information is to be elsewhere, then it would be nice to have a link or reference to point to.&lt;/P&gt;&lt;P&gt;I have not yet got the uart to work.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Fri, 25 Jul 2014 19:59:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Cannot-debug-internal-RAM-DS-5-Vybrid-projects-External-RAM/m-p/324693#M10356</guid>
      <dc:creator>rocketdawg</dc:creator>
      <dc:date>2014-07-25T19:59:31Z</dc:date>
    </item>
  </channel>
</rss>