<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MQX codesize tool not working? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-codesize-tool-not-working/m-p/324261#M10323</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use the codesize tool available in the MQX 4.1 tools folder. However the html output gives me no information, as in the following image:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43664i7BFDDA0CC51900BE/image-size/large?v=v2&amp;amp;px=999" title="codesize_report.png" alt="codesize_report.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All itens are as above, with an '-' symbol. This is the command I'm using and the stdout output:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44418i6E65071438B4514A/image-size/large?v=v2&amp;amp;px=999" title="codesize_cmd.png" alt="codesize_cmd.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea on why this could be happening? I've tried searching another threads here without success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Luiz Fernando&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 25 Jun 2014 17:58:51 GMT</pubDate>
    <dc:creator>lfschrickte</dc:creator>
    <dc:date>2014-06-25T17:58:51Z</dc:date>
    <item>
      <title>MQX codesize tool not working?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-codesize-tool-not-working/m-p/324261#M10323</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm trying to use the codesize tool available in the MQX 4.1 tools folder. However the html output gives me no information, as in the following image:&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/43664i7BFDDA0CC51900BE/image-size/large?v=v2&amp;amp;px=999" title="codesize_report.png" alt="codesize_report.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;All itens are as above, with an '-' symbol. This is the command I'm using and the stdout output:&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44418i6E65071438B4514A/image-size/large?v=v2&amp;amp;px=999" title="codesize_cmd.png" alt="codesize_cmd.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Do you have any idea on why this could be happening? I've tried searching another threads here without success.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thank you!&lt;/P&gt;&lt;P&gt;Luiz Fernando&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 25 Jun 2014 17:58:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-codesize-tool-not-working/m-p/324261#M10323</guid>
      <dc:creator>lfschrickte</dc:creator>
      <dc:date>2014-06-25T17:58:51Z</dc:date>
    </item>
    <item>
      <title>Re: MQX codesize tool not working?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-codesize-tool-not-working/m-p/324262#M10324</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;It should work.&lt;/P&gt;&lt;P&gt;However: Are you sure that you used CW compiler? GCC is currently not supported by this tool.&lt;/P&gt;&lt;P&gt;CW compiler/linker typically generate *.xMap file instead of *.map file.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Best Regards,&lt;BR /&gt;RadekS&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jun 2014 09:14:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-codesize-tool-not-working/m-p/324262#M10324</guid>
      <dc:creator>RadekS</dc:creator>
      <dc:date>2014-06-30T09:14:37Z</dc:date>
    </item>
    <item>
      <title>Re: MQX codesize tool not working?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-codesize-tool-not-working/m-p/324263#M10325</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I can't test if it will work as a change of toolchain now will be hard, but you're right: I'm using GCC and haven't realized it is not supported!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Hope I can find something similar that works with gcc soon!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Thanks very much!&lt;/P&gt;&lt;P&gt;Luiz Fernando&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Jun 2014 12:16:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-codesize-tool-not-working/m-p/324263#M10325</guid>
      <dc:creator>lfschrickte</dc:creator>
      <dc:date>2014-06-30T12:16:46Z</dc:date>
    </item>
  </channel>
</rss>