<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Adding RAM under MQX 4.1 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317226#M10107</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a custom board based on the tower TWR-K60F120M running MQX 4.1.&lt;/P&gt;&lt;P&gt;I'm running out of ram, so I'm very keen to add more RAM to the system.&lt;/P&gt;&lt;P&gt;Can anybody tell me if there is an application note on that issue? If not, how Can I implement this, and which is the type of RAM I should use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Óscar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Tue, 08 Jul 2014 07:27:16 GMT</pubDate>
    <dc:creator>oscargarciaabad</dc:creator>
    <dc:date>2014-07-08T07:27:16Z</dc:date>
    <item>
      <title>Adding RAM under MQX 4.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317226#M10107</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi all,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I'm using a custom board based on the tower TWR-K60F120M running MQX 4.1.&lt;/P&gt;&lt;P&gt;I'm running out of ram, so I'm very keen to add more RAM to the system.&lt;/P&gt;&lt;P&gt;Can anybody tell me if there is an application note on that issue? If not, how Can I implement this, and which is the type of RAM I should use?&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Óscar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jul 2014 07:27:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317226#M10107</guid>
      <dc:creator>oscargarciaabad</dc:creator>
      <dc:date>2014-07-08T07:27:16Z</dc:date>
    </item>
    <item>
      <title>Re: Adding RAM under MQX 4.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317227#M10108</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oscar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I beleive you will find this appnote interesting:&lt;/P&gt;&lt;P&gt;&lt;A href="http://cache.freescale.com/files/microcontrollers/doc/app_note/AN4393.pdf"&gt;AN4393&lt;/A&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Regards,&lt;BR /&gt;Garabo&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;-----------------------------------------------------------------------------------------------------------------------&lt;BR /&gt;Note: If this post answers your question, please click the Correct Answer button. Thank you!&lt;BR /&gt;-----------------------------------------------------------------------------------------------------------------------&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jul 2014 13:53:46 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317227#M10108</guid>
      <dc:creator>Luis_Garabo</dc:creator>
      <dc:date>2014-07-08T13:53:46Z</dc:date>
    </item>
    <item>
      <title>Re: Adding RAM under MQX 4.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317228#M10109</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Garabo,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;This is very interesting.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your help.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Óscar&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jul 2014 14:18:38 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317228#M10109</guid>
      <dc:creator>oscargarciaabad</dc:creator>
      <dc:date>2014-07-08T14:18:38Z</dc:date>
    </item>
    <item>
      <title>Re: Adding RAM under MQX 4.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317229#M10110</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Oscar,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Attached you can find a simple example in CW10.5 and MQX4.1 (will work in CW10.6 also). Please note that you must enable in user_config.h the macros mentioned in AN4393 and rebuild MQX libraries.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Regards,&lt;/P&gt;&lt;P&gt;Carlos&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 08 Jul 2014 20:00:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317229#M10110</guid>
      <dc:creator>Carlos_Musich</dc:creator>
      <dc:date>2014-07-08T20:00:37Z</dc:date>
    </item>
    <item>
      <title>Re: Adding RAM under MQX 4.1</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317230#M10111</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi Carlos,&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Many thanks for your help!&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Best regards.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Óscar.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Jul 2014 15:54:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/Adding-RAM-under-MQX-4-1/m-p/317230#M10111</guid>
      <dc:creator>oscargarciaabad</dc:creator>
      <dc:date>2014-07-10T15:54:34Z</dc:date>
    </item>
  </channel>
</rss>