<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic init_gpio and pin choice for uart using MQX 3.8 in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/init-gpio-and-pin-choice-for-uart-using-MQX-3-8/m-p/158696#M1009</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello, I'm beginner in using MQX 3.8. I want to use another pins for uart RX/TX than defined in init_gpio.c (e.g. not PTD6/PTD7, but PTB16/PTB17 for uart0 at MK60N512). What's the smartest solution. Because of 'hard wired' flags in serl_pol_kuart.c@419, the only solution is to alter the mux table after calling fopen for the uart port, isn't it?&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Mon, 30 Apr 2012 19:41:09 GMT</pubDate>
    <dc:creator>Fabi</dc:creator>
    <dc:date>2012-04-30T19:41:09Z</dc:date>
    <item>
      <title>init_gpio and pin choice for uart using MQX 3.8</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/init-gpio-and-pin-choice-for-uart-using-MQX-3-8/m-p/158696#M1009</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;Hello, I'm beginner in using MQX 3.8. I want to use another pins for uart RX/TX than defined in init_gpio.c (e.g. not PTD6/PTD7, but PTB16/PTB17 for uart0 at MK60N512). What's the smartest solution. Because of 'hard wired' flags in serl_pol_kuart.c@419, the only solution is to alter the mux table after calling fopen for the uart port, isn't it?&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Mon, 30 Apr 2012 19:41:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/init-gpio-and-pin-choice-for-uart-using-MQX-3-8/m-p/158696#M1009</guid>
      <dc:creator>Fabi</dc:creator>
      <dc:date>2012-04-30T19:41:09Z</dc:date>
    </item>
    <item>
      <title>Re: init_gpio and pin choice for uart using MQX 3.8</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/init-gpio-and-pin-choice-for-uart-using-MQX-3-8/m-p/158697#M1010</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;I have changed the port and pin code directly&amp;nbsp;into init_gpio.c: _bsp_serial_io_init().&lt;/P&gt;&lt;P&gt;I think that MQX-team has&amp;nbsp;designed&amp;nbsp;that the file init_gpio.c contains HW-dependant code,&lt;/P&gt;&lt;P&gt;which should be tailored to suitable for own HW.&lt;/P&gt;&lt;P&gt;Remove also the switch-cases for dev_num/ports&amp;nbsp;which are not included in your HW.&lt;/P&gt;&lt;P&gt;~Mark&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Tue, 01 May 2012 01:02:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/init-gpio-and-pin-choice-for-uart-using-MQX-3-8/m-p/158697#M1010</guid>
      <dc:creator>MarkP_</dc:creator>
      <dc:date>2012-05-01T01:02:03Z</dc:date>
    </item>
    <item>
      <title>Re: init_gpio and pin choice for uart using MQX 3.8</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/init-gpio-and-pin-choice-for-uart-using-MQX-3-8/m-p/158698#M1011</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi,&lt;/P&gt;&lt;P&gt;Mark, TY for reply. You are right. The BSP contains the project specific (user) files. Your suggestion solves it.&lt;/P&gt;&lt;P&gt;- Falko&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 02 May 2012 15:15:16 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/init-gpio-and-pin-choice-for-uart-using-MQX-3-8/m-p/158698#M1011</guid>
      <dc:creator>Fabi</dc:creator>
      <dc:date>2012-05-02T15:15:16Z</dc:date>
    </item>
  </channel>
</rss>