<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MQX Software SolutionsのトピックRe: MQX 4.1 FTP fails</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-FTP-fails/m-p/314264#M10063</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is example in rtcs/examples/shell. On the command line just start the FTP server "ftpsrv start". As file system it uses ramdisk file system mounted as "a:". The implementation of the ftpsrv start command is in the shell library (sh_ftpd.c).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are sure your file system on SD card is working, just configure it as the the root_dir parameter of the FTPSRV_PARAM_STRUCT.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Wed, 04 Jun 2014 13:36:20 GMT</pubDate>
    <dc:creator>Martin_</dc:creator>
    <dc:date>2014-06-04T13:36:20Z</dc:date>
    <item>
      <title>MQX 4.1 FTP fails</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-FTP-fails/m-p/314263#M10062</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Hi!!&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;I have an application that uses FTP server on a SD CARD working in MQX 4.0 and I have updated the OS to 4.1 version. The FTP server has been improved in this OS version and&amp;nbsp; I didn`t found the FTP example code (mfs_ftp in previous releases). I have built a test application based on a mfs_sd example (file system in a SD card) and HVAC demo code wich configure a FTP server.&amp;nbsp; The code of the network task is a copy from the HVAC demo (see atached code file).&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;When I try to connect via FTP I obtained this error:&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="12218_12218.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/119817iAB38DA86169711AE/image-size/large?v=v2&amp;amp;px=999" role="button" title="12218_12218.jpg" alt="12218_12218.jpg" /&gt;&lt;/span&gt;&lt;span class="lia-inline-image-display-wrapper" image-alt="FTP_error.jpg"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/44296i740BBFADCCFF1FA5/image-size/large?v=v2&amp;amp;px=999" role="button" title="FTP_error.jpg" alt="FTP_error.jpg" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Some ideas about how to solve this issue? Do someone have an example code for FTP in MQX 4.1?&amp;nbsp;&amp;nbsp;&amp;nbsp; &lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks in advance&lt;/P&gt;&lt;P style="min-height: 8pt; padding: 0px;"&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;David Cantero.&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;Original Attachment has been moved to: &lt;A _jive_internal="true" href="https://community.nxp.com/docs/DOC-339110"&gt;network_tsk.c.zip&lt;/A&gt;&lt;/STRONG&gt;&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2014 13:02:58 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-FTP-fails/m-p/314263#M10062</guid>
      <dc:creator>dcantero</dc:creator>
      <dc:date>2014-06-04T13:02:58Z</dc:date>
    </item>
    <item>
      <title>Re: MQX 4.1 FTP fails</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-FTP-fails/m-p/314264#M10063</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;There is example in rtcs/examples/shell. On the command line just start the FTP server "ftpsrv start". As file system it uses ramdisk file system mounted as "a:". The implementation of the ftpsrv start command is in the shell library (sh_ftpd.c).&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;If you are sure your file system on SD card is working, just configure it as the the root_dir parameter of the FTPSRV_PARAM_STRUCT.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Wed, 04 Jun 2014 13:36:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/MQX-4-1-FTP-fails/m-p/314264#M10063</guid>
      <dc:creator>Martin_</dc:creator>
      <dc:date>2014-06-04T13:36:20Z</dc:date>
    </item>
  </channel>
</rss>