<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic What are the differences in MFS betwen MQX4.0 and MQX 4.1? in MQX Software Solutions</title>
    <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-are-the-differences-in-MFS-betwen-MQX4-0-and-MQX-4-1/m-p/311281#M10001</link>
    <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My board has 2 K60's.&amp;nbsp; I wrote a program to have one of the K60's program the other thru the EZ_Port.&amp;nbsp; I used MQX 4.0. My program reads some configuration information from a file on a SD card and loads the K60 with data from a SREC file also stored on the SD card..&amp;nbsp; My application is based on AN44406 (KwikStik-based EzPort programmer) and uses parts of the code from the application note.&amp;nbsp; The MQX 4.0 version works fine - no problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am attempting to port the code to MQX 4.1 and my application can not find the files on the SD card!!&amp;nbsp; It is the same code.&amp;nbsp; The c files were copied from the working MQX 4.0 version.&amp;nbsp; I am not sure why this is. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a sanity check I took the section of my code that opens and reads the files on the SD card and added it to the MFS sdcard example project on a TWR-K60F120M.&amp;nbsp; This example installs the SD card with a MFS shell.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; When the project is built with MQX 4.0 my code works perfectly as do the DOS commands "dir", "type", etc.&amp;nbsp; HOWEVER, when the project is built using MQX4.1 my code does not work but the DOS shell commands do work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I stepped into the the 4.0 and 4.1 version and noted there are differences between the MQX versions.&amp;nbsp; The 4.1 files contain references to MQX_IO_OLD whatever that means.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know of any differences between versions 4.0 and 4.1 that would/could cause the problems I am seeing?&amp;nbsp; Needless to say I am disappointed that MQX 4.1 isn't working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
    <pubDate>Sat, 05 Apr 2014 00:34:37 GMT</pubDate>
    <dc:creator>pk2</dc:creator>
    <dc:date>2014-04-05T00:34:37Z</dc:date>
    <item>
      <title>What are the differences in MFS betwen MQX4.0 and MQX 4.1?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-are-the-differences-in-MFS-betwen-MQX4-0-and-MQX-4-1/m-p/311281#M10001</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;My board has 2 K60's.&amp;nbsp; I wrote a program to have one of the K60's program the other thru the EZ_Port.&amp;nbsp; I used MQX 4.0. My program reads some configuration information from a file on a SD card and loads the K60 with data from a SREC file also stored on the SD card..&amp;nbsp; My application is based on AN44406 (KwikStik-based EzPort programmer) and uses parts of the code from the application note.&amp;nbsp; The MQX 4.0 version works fine - no problems.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I am attempting to port the code to MQX 4.1 and my application can not find the files on the SD card!!&amp;nbsp; It is the same code.&amp;nbsp; The c files were copied from the working MQX 4.0 version.&amp;nbsp; I am not sure why this is. &lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;As a sanity check I took the section of my code that opens and reads the files on the SD card and added it to the MFS sdcard example project on a TWR-K60F120M.&amp;nbsp; This example installs the SD card with a MFS shell.&amp;nbsp;&amp;nbsp;&amp;nbsp;&amp;nbsp; When the project is built with MQX 4.0 my code works perfectly as do the DOS commands "dir", "type", etc.&amp;nbsp; HOWEVER, when the project is built using MQX4.1 my code does not work but the DOS shell commands do work.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;I stepped into the the 4.0 and 4.1 version and noted there are differences between the MQX versions.&amp;nbsp; The 4.1 files contain references to MQX_IO_OLD whatever that means.&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P&gt;Does anyone know of any differences between versions 4.0 and 4.1 that would/could cause the problems I am seeing?&amp;nbsp; Needless to say I am disappointed that MQX 4.1 isn't working.&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Sat, 05 Apr 2014 00:34:37 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/What-are-the-differences-in-MFS-betwen-MQX4-0-and-MQX-4-1/m-p/311281#M10001</guid>
      <dc:creator>pk2</dc:creator>
      <dc:date>2014-04-05T00:34:37Z</dc:date>
    </item>
    <item>
      <title>Re: What are the differences in MFS betwen MQX4.0 and MQX 4.1?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-are-the-differences-in-MFS-betwen-MQX4-0-and-MQX-4-1/m-p/311282#M10002</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P&gt;Problem solved.&amp;nbsp; One of the tasks had a stack overflow.&amp;nbsp; Increasing the stack size solved the problem&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Apr 2014 00:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/What-are-the-differences-in-MFS-betwen-MQX4-0-and-MQX-4-1/m-p/311282#M10002</guid>
      <dc:creator>pk2</dc:creator>
      <dc:date>2014-04-10T00:42:51Z</dc:date>
    </item>
    <item>
      <title>Re: What are the differences in MFS betwen MQX4.0 and MQX 4.1?</title>
      <link>https://community.nxp.com/t5/MQX-Software-Solutions/What-are-the-differences-in-MFS-betwen-MQX4-0-and-MQX-4-1/m-p/311283#M10003</link>
      <description>&lt;HTML&gt;&lt;HEAD&gt;&lt;/HEAD&gt;&lt;BODY&gt;&lt;P style="font-weight: normal; font-style: normal; font-size: 13px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d; text-align: left; text-indent: 0px;"&gt;Hi, &lt;/P&gt;&lt;P style="font-weight: normal; font-style: normal; font-size: 13px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d; text-align: left; text-indent: 0px;"&gt;Thank you for share your solution&lt;SPAN class="Apple-converted-space"&gt; &lt;/SPAN&gt;&lt;SPAN class="emoticon-inline emoticon_wink" style="font-weight: inherit; font-style: inherit; font-size: 13px; font-family: inherit; background-position: no-repeat no-repeat;"&gt;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: normal; font-style: normal; font-size: 13px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d; text-align: left; text-indent: 0px;"&gt;Regards&lt;/P&gt;&lt;P&gt;&lt;/P&gt;&lt;P style="font-weight: normal; font-style: normal; font-size: 13px; font-family: 'Helvetica Neue', Helvetica, Arial, 'Lucida Grande', sans-serif; color: #3d3d3d; text-align: left; text-indent: 0px;"&gt;Sol&lt;/P&gt;&lt;/BODY&gt;&lt;/HTML&gt;</description>
      <pubDate>Thu, 10 Apr 2014 16:47:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MQX-Software-Solutions/What-are-the-differences-in-MFS-betwen-MQX4-0-and-MQX-4-1/m-p/311283#M10003</guid>
      <dc:creator>soledad</dc:creator>
      <dc:date>2014-04-10T16:47:44Z</dc:date>
    </item>
  </channel>
</rss>