<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCXN947VNLT in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947VNLT/m-p/1818649#M62</link>
    <description>&lt;P&gt;&lt;FONT size="3"&gt;Hello! I have a question regarding power-up sequence for controller&amp;nbsp;&lt;SPAN&gt;MCXN947VNLT.&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;What is the exact power-up sequence must be if I'm going to use external power supply sources?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;Where I can find a detailed description of the power supply sequence?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;At the moment, all I could find was the following description:&lt;/FONT&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT size="3"&gt;If using the DCDC, the lower voltage should be selected. The DCDC is more efficient at lower voltages. The same thumb rule applies to the core LDO. The&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_CORE&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;must ramp after VDD. Designers must ensure that these conditions are met.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="3"&gt;Either source can supply&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_BAT&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;but should power up before or with&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_SYS. Designers must ensure that these conditions are met.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="3"&gt;Secondary IOs&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_P2,&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_P3, and&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_P4&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;must ramp after&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_SYS&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;unless they are shorted with the VDD.&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;FONT size="3"&gt;What is the relation in sequence of ramp up in between&amp;nbsp;VDD_CORE&amp;nbsp;&lt;FONT face="arial,helvetica,sans-serif" color="#000000"&gt;and&amp;nbsp;&lt;/FONT&gt;VDD_SYS&lt;/FONT&gt;&lt;FONT color="#000000"&gt;?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;Regards, Val&lt;/FONT&gt;&lt;/P&gt;</description>
    <pubDate>Thu, 29 Feb 2024 09:55:34 GMT</pubDate>
    <dc:creator>Valeryi</dc:creator>
    <dc:date>2024-02-29T09:55:34Z</dc:date>
    <item>
      <title>MCXN947VNLT</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947VNLT/m-p/1818649#M62</link>
      <description>&lt;P&gt;&lt;FONT size="3"&gt;Hello! I have a question regarding power-up sequence for controller&amp;nbsp;&lt;SPAN&gt;MCXN947VNLT.&amp;nbsp;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;What is the exact power-up sequence must be if I'm going to use external power supply sources?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;&lt;SPAN&gt;Where I can find a detailed description of the power supply sequence?&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="3"&gt;At the moment, all I could find was the following description:&lt;/FONT&gt;&lt;/P&gt;&lt;UL&gt;&lt;LI&gt;&lt;FONT size="3"&gt;If using the DCDC, the lower voltage should be selected. The DCDC is more efficient at lower voltages. The same thumb rule applies to the core LDO. The&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_CORE&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;must ramp after VDD. Designers must ensure that these conditions are met.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="3"&gt;Either source can supply&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_BAT&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;but should power up before or with&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_SYS. Designers must ensure that these conditions are met.&lt;/FONT&gt;&lt;/LI&gt;&lt;LI&gt;&lt;FONT size="3"&gt;Secondary IOs&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_P2,&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_P3, and&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_P4&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;must ramp after&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;VDD_SYS&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;unless they are shorted with the VDD.&lt;/FONT&gt;&lt;/LI&gt;&lt;/UL&gt;&lt;P&gt;&lt;FONT size="3"&gt;What is the relation in sequence of ramp up in between&amp;nbsp;VDD_CORE&amp;nbsp;&lt;FONT face="arial,helvetica,sans-serif" color="#000000"&gt;and&amp;nbsp;&lt;/FONT&gt;VDD_SYS&lt;/FONT&gt;&lt;FONT color="#000000"&gt;?&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT color="#000000"&gt;Regards, Val&lt;/FONT&gt;&lt;/P&gt;</description>
      <pubDate>Thu, 29 Feb 2024 09:55:34 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947VNLT/m-p/1818649#M62</guid>
      <dc:creator>Valeryi</dc:creator>
      <dc:date>2024-02-29T09:55:34Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN947VNLT</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947VNLT/m-p/1819177#M66</link>
      <description>&lt;P&gt;Hi,&lt;/P&gt;
&lt;P&gt;For the MCXN94x, there is power-up sequence requirement exactly, it is not clear in the RM.&lt;/P&gt;
&lt;P&gt;This is the power-up sequence for MCXN94x.&lt;/P&gt;
&lt;P&gt;The VDD_BAT is the first, VDD_SYS is the second, the VDD, VDD_Px, VDD_ANA are the third, the VDD_CORE is the last.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="xiangjun_rong_0-1709263156104.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/265935iA8C3429E864B81FA/image-size/medium?v=v2&amp;amp;px=400" role="button" title="xiangjun_rong_0-1709263156104.png" alt="xiangjun_rong_0-1709263156104.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Hope it can help you&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;XiangJun Rong&lt;/P&gt;</description>
      <pubDate>Fri, 01 Mar 2024 03:21:57 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN947VNLT/m-p/1819177#M66</guid>
      <dc:creator>xiangjun_rong</dc:creator>
      <dc:date>2024-03-01T03:21:57Z</dc:date>
    </item>
  </channel>
</rss>