<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MX8MP ENET voltage in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MX8MP-ENET-voltage/m-p/2421782#M6044</link>
    <description>&lt;P&gt;Thank you, Jorge. Love the avatar.&amp;nbsp; &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
    <pubDate>Fri, 16 Oct 2026 21:36:12 GMT</pubDate>
    <dc:creator>mmagargee</dc:creator>
    <dc:date>2026-10-16T21:36:12Z</dc:date>
    <item>
      <title>MX8MP ENET voltage</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MX8MP-ENET-voltage/m-p/2421705#M6041</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;&lt;P&gt;We are migrating from an MX8X controller to&amp;nbsp;MX8MP. In the older one, ENET0 and ENET1 supported voltage 1.8V, 2.5V, 3.3V (RMII all three, RGMII first two only).&lt;/P&gt;&lt;P&gt;MX8MP removes the 2.5V option, but allows 1.8V and 3.3V choices. Absolute Vmax is 3.8V. The question is, what happens in a 2.5V operation on NVCC_ENET? 2.5 will not exceed the absolute max. But how are the MAC signals configured and what kind of impact would 2.5V operation have long term?&lt;/P&gt;&lt;P&gt;I ask because it would be great to avoid updating the older PHY that is currently running both its supply and VDDIO on 2.5V.&lt;/P&gt;&lt;P&gt;Thank you,&lt;/P&gt;&lt;P&gt;Mike&lt;/P&gt;</description>
      <pubDate>Fri, 16 Oct 2026 13:15:09 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MX8MP-ENET-voltage/m-p/2421705#M6041</guid>
      <dc:creator>mmagargee</dc:creator>
      <dc:date>2026-10-16T13:15:09Z</dc:date>
    </item>
    <item>
      <title>Re: MX8MP ENET voltage</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MX8MP-ENET-voltage/m-p/2421770#M6043</link>
      <description>&lt;P&gt;Hello,&lt;/P&gt;
&lt;P&gt;As mentioned in the documentation, the interface supports only two voltage levels, 1.8 V and 3.3 V. Even if 2.5 V is within the overall operating voltage range, 2.5 V signals may not meet the specified thresholds for valid logic levels, which could result in unpredictable behavior.&lt;/P&gt;
&lt;P&gt;I recommend using either 1.8 V or 3.3 V for this interface.&lt;/P&gt;
&lt;P&gt;Best regards.&lt;/P&gt;</description>
      <pubDate>Fri, 16 Oct 2026 18:40:07 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MX8MP-ENET-voltage/m-p/2421770#M6043</guid>
      <dc:creator>JorgeCas</dc:creator>
      <dc:date>2026-10-16T18:40:07Z</dc:date>
    </item>
    <item>
      <title>Re: MX8MP ENET voltage</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MX8MP-ENET-voltage/m-p/2421782#M6044</link>
      <description>&lt;P&gt;Thank you, Jorge. Love the avatar.&amp;nbsp; &lt;LI-EMOJI id="lia_slightly-smiling-face" title=":slightly_smiling_face:"&gt;&lt;/LI-EMOJI&gt;&lt;/P&gt;</description>
      <pubDate>Fri, 16 Oct 2026 21:36:12 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MX8MP-ENET-voltage/m-p/2421782#M6044</guid>
      <dc:creator>mmagargee</dc:creator>
      <dc:date>2026-10-16T21:36:12Z</dc:date>
    </item>
  </channel>
</rss>