<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2420317#M6025</link>
    <description>&lt;P&gt;Hi Harry:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your reply. I have tried setting MCONFIG again for testing.&lt;/P&gt;&lt;P&gt;1. In the test, disableTimeout was set to true.&lt;/P&gt;&lt;P&gt;2. The image shows the current register settings, including the values ​​of MCONFIG, MSTATUS, and MERRWARN, as well as the I2C bus signal. (The difference between configuration A and configuration B is the setting of MSTENA: Configuration A: MCONFIG[MSTENA] = 3, Configuration B: MCONFIG[MSTENA] = 1).&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;The SDA/SCL IO pins should be set to openDrainEnable = kPORT_OpenDrainDisable as per the example, and pull-up resistors(4.7K) should be present.&lt;/P&gt;&lt;P&gt;Currently, it seems that the I2C bus stretching function cannot be implemented.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
    <pubDate>Mon, 12 Oct 2026 08:00:21 GMT</pubDate>
    <dc:creator>kevin_Jhuang</dc:creator>
    <dc:date>2026-10-12T08:00:21Z</dc:date>
    <item>
      <title>When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability fai</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2419236#M6008</link>
      <description>&lt;P&gt;Hello, I'm currently encountering a problem: I want to use the I3C interface of the FRDM-MCXN947 for I2C communication,but the slave device I'm connecting to experiences clock stretching during data preparation,so I have to wait for the slave device to release the SCL signal before data transfer can begin.&lt;BR /&gt;&lt;BR /&gt;I've tried using the configurable registers (such as MCONFIG[SKEW] = 0, MCONFIG[HKEEP] = 0b11, MCONFIG[MSTENA] = 0b11) from the MCXNP184M150F70RM reference file, but it doesn't seem to be working. How can I resolve this?&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;#FRDM-MCXN947 #I3C &lt;/P&gt;</description>
      <pubDate>Thu, 08 Oct 2026 02:34:26 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2419236#M6008</guid>
      <dc:creator>kevin_Jhuang</dc:creator>
      <dc:date>2026-10-08T02:34:26Z</dc:date>
    </item>
    <item>
      <title>Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2419638#M6013</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/267195"&gt;@kevin_Jhuang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The register settings are currently applied before I3C_MasterInit(), so they may be overwritten by the SDK initialization.&lt;/P&gt;
&lt;P&gt;Please enable:&lt;/P&gt;
&lt;LI-CODE lang="markup"&gt;masterConfig-&amp;gt;disableTimeout = true;&lt;/LI-CODE&gt;
&lt;P&gt;Then configure MSTENA = 3, HKEEP = 3, and SKEW = 0 after I3C_MasterInit(). Please clear the corresponding register fields before writing them instead of using |=.&lt;/P&gt;
&lt;P&gt;After initialization, please read back MCONFIG to verify that the settings are still active. Also provide the MSTATUS and MERRWARN values captured immediately after the clock-stretching failure.&lt;/P&gt;
&lt;P&gt;Please also confirm that SCL and SDA are configured for open-drain operation and that external pull-up resistors are installed.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Fri, 09 Oct 2026 02:51:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2419638#M6013</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-10-09T02:51:15Z</dc:date>
    </item>
    <item>
      <title>Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2420317#M6025</link>
      <description>&lt;P&gt;Hi Harry:&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;&lt;P&gt;Thank you very much for your reply. I have tried setting MCONFIG again for testing.&lt;/P&gt;&lt;P&gt;1. In the test, disableTimeout was set to true.&lt;/P&gt;&lt;P&gt;2. The image shows the current register settings, including the values ​​of MCONFIG, MSTATUS, and MERRWARN, as well as the I2C bus signal. (The difference between configuration A and configuration B is the setting of MSTENA: Configuration A: MCONFIG[MSTENA] = 3, Configuration B: MCONFIG[MSTENA] = 1).&lt;/P&gt;&lt;P&gt;3.&amp;nbsp;The SDA/SCL IO pins should be set to openDrainEnable = kPORT_OpenDrainDisable as per the example, and pull-up resistors(4.7K) should be present.&lt;/P&gt;&lt;P&gt;Currently, it seems that the I2C bus stretching function cannot be implemented.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2026 08:00:21 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2420317#M6025</guid>
      <dc:creator>kevin_Jhuang</dc:creator>
      <dc:date>2026-10-12T08:00:21Z</dc:date>
    </item>
    <item>
      <title>Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2420318#M6026</link>
      <description>&lt;P&gt;Following the above reply，configure B picture&lt;BR /&gt;&lt;BR /&gt;Thank you&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;</description>
      <pubDate>Mon, 12 Oct 2026 07:50:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2420318#M6026</guid>
      <dc:creator>kevin_Jhuang</dc:creator>
      <dc:date>2026-10-12T07:50:31Z</dc:date>
    </item>
    <item>
      <title>Re: When using the FRDM-MCXN947's I3C interface for I2C communication, the Clk stretching capability</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2420953#M6031</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/267195"&gt;@kevin_Jhuang&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;I can reproduce the issue and will continue investigating it. I will update you once I have any findings.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Wed, 14 Oct 2026 07:47:52 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/When-using-the-FRDM-MCXN947-s-I3C-interface-for-I2C/m-p/2420953#M6031</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-10-14T07:47:52Z</dc:date>
    </item>
  </channel>
</rss>