<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX Microcontrollers中的主题 MCXN547 SC Timer0 SDK driver Issue</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN547-SC-Timer0-SDK-driver-Issue/m-p/2416496#M5958</link>
    <description>&lt;P&gt;I am using MCXN547VKL MCU and SDK version 26.06.00.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Context: I am using SCT timer0&amp;nbsp; to generate two different PWM waveform using the COUNTER in split mode, CONFIG[UNIFY] = 0; i.e COUNT_L for one PWM generator and COUNT_H for another PWM generator.&lt;/P&gt;&lt;P&gt;The issue: When I load the COUNTER_H with the driver API "&lt;SPAN&gt;SCTIMER_SetCOUNTValue(SCT0,kSCTIMER_Counter_H,0U);" , Bus Fault occurs.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I traced the issue to SDK driver code. The driver code uses 32 bit write to write both COUNT_H and COUNT_L instead of 16 bit write to COUNT_H alone. While the COUNT_H is being written COUNT_L was running and this caused bus fault. I modified the SDK driver code to use 16 bit write and the bus fault did not occur. I have attached the driver code and marked with colours, the code line which was causing the problem and the fix. If this is really the problem, the SDK driver can be updated. - Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/*!&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* @brief Set the value of counter.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;*&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* The function is to set the value of Count register, Writing to the COUNT_L, COUNT_H, or unified register&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* is only allowed when the corresponding counter is halted (HALT bits are set to 1 in the CTRL register).&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;*&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* @&lt;/SPAN&gt;&lt;SPAN&gt;param&lt;/SPAN&gt;&lt;SPAN&gt; base SCTimer peripheral base address&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* @&lt;/SPAN&gt;&lt;SPAN&gt;param&lt;/SPAN&gt;&lt;SPAN&gt; whichCounter SCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H,&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* In 32-bit mode, we can select Counter_U.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* @&lt;/SPAN&gt;&lt;SPAN&gt;param&lt;/SPAN&gt;&lt;SPAN&gt; value the counter value update to the COUNT register.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;*/&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;static&lt;/SPAN&gt; &lt;SPAN&gt;inline&lt;/SPAN&gt; &lt;SPAN&gt;void&lt;/SPAN&gt; &lt;SPAN&gt;SCTIMER_SetCOUNTValue&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;SCT_Type&lt;/SPAN&gt;&lt;SPAN&gt; *base, &lt;/SPAN&gt;&lt;SPAN&gt;sctimer_counter_t&lt;/SPAN&gt;&lt;SPAN&gt; whichCounter, &lt;/SPAN&gt;&lt;SPAN&gt;uint32_t&lt;/SPAN&gt;&lt;SPAN&gt; value)&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;SCTIMER_StopTimer(base, (&lt;/SPAN&gt;&lt;SPAN&gt;uint32_t&lt;/SPAN&gt;&lt;SPAN&gt;)whichCounter);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;switch&lt;/SPAN&gt;&lt;SPAN&gt; (whichCounter)&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;case&lt;/SPAN&gt; &lt;SPAN&gt;kSCTIMER_Counter_L&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(value &amp;lt;= 0xFFFFU);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(0U == (base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;CONFIG&lt;/SPAN&gt;&lt;SPAN&gt; &amp;amp; SCT_CONFIG_UNIFY_MASK));&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/* Use Counter_L bits when user wants to setup the Low counter */&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;COUNT_ACCESS16BIT&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;COUNTL&lt;/SPAN&gt;&lt;SPAN&gt; = (&lt;/SPAN&gt;&lt;SPAN&gt;uint16_t&lt;/SPAN&gt;&lt;SPAN&gt;)value;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;break&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;case&lt;/SPAN&gt; &lt;SPAN&gt;kSCTIMER_Counter_H&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(value &amp;lt;= 0xFFFFU);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(0U == (base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;CONFIG&lt;/SPAN&gt;&lt;SPAN&gt; &amp;amp; SCT_CONFIG_UNIFY_MASK));&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/* Use Counter_H bits when user wants to setup the High counter */&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2" color="#FF0000"&gt;&lt;SPAN&gt;// base-&amp;gt;COUNT = (uint32_t)base-&amp;gt;COUNT_ACCESS16BIT.COUNTL | SCT_COUNT_CTR_H(value);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2" color="#00FF00"&gt;&lt;SPAN&gt;base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;COUNT_ACCESS16BIT&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;COUNTH&lt;/SPAN&gt;&lt;SPAN&gt; = (&lt;/SPAN&gt;&lt;SPAN&gt;uint16_t&lt;/SPAN&gt;&lt;SPAN&gt;)value; //the fix&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;break&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;case&lt;/SPAN&gt; &lt;SPAN&gt;kSCTIMER_Counter_U&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(1U == (base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;CONFIG&lt;/SPAN&gt;&lt;SPAN&gt; &amp;amp; SCT_CONFIG_UNIFY_MASK));&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/* Use both Counter_L/Counter_H bits when counter is operating in 32-bit mode (unify counter). */&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;COUNT&lt;/SPAN&gt;&lt;SPAN&gt; = value;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;break&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;default&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/* Fix the MISRA C-2012 issue rule 16.4. */&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;break&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;SCTIMER_StartTimer(base, (&lt;/SPAN&gt;&lt;SPAN&gt;uint32_t&lt;/SPAN&gt;&lt;SPAN&gt;)whichCounter);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
    <pubDate>Sun, 27 Sep 2026 06:22:41 GMT</pubDate>
    <dc:creator>JawaharA</dc:creator>
    <dc:date>2026-09-27T06:22:41Z</dc:date>
    <item>
      <title>MCXN547 SC Timer0 SDK driver Issue</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN547-SC-Timer0-SDK-driver-Issue/m-p/2416496#M5958</link>
      <description>&lt;P&gt;I am using MCXN547VKL MCU and SDK version 26.06.00.&amp;nbsp;&lt;/P&gt;&lt;P&gt;Context: I am using SCT timer0&amp;nbsp; to generate two different PWM waveform using the COUNTER in split mode, CONFIG[UNIFY] = 0; i.e COUNT_L for one PWM generator and COUNT_H for another PWM generator.&lt;/P&gt;&lt;P&gt;The issue: When I load the COUNTER_H with the driver API "&lt;SPAN&gt;SCTIMER_SetCOUNTValue(SCT0,kSCTIMER_Counter_H,0U);" , Bus Fault occurs.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;I traced the issue to SDK driver code. The driver code uses 32 bit write to write both COUNT_H and COUNT_L instead of 16 bit write to COUNT_H alone. While the COUNT_H is being written COUNT_L was running and this caused bus fault. I modified the SDK driver code to use 16 bit write and the bus fault did not occur. I have attached the driver code and marked with colours, the code line which was causing the problem and the fix. If this is really the problem, the SDK driver can be updated. - Thanks&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;DIV&gt;&lt;DIV&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/*!&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* @brief Set the value of counter.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;*&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* The function is to set the value of Count register, Writing to the COUNT_L, COUNT_H, or unified register&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* is only allowed when the corresponding counter is halted (HALT bits are set to 1 in the CTRL register).&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;*&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* @&lt;/SPAN&gt;&lt;SPAN&gt;param&lt;/SPAN&gt;&lt;SPAN&gt; base SCTimer peripheral base address&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* @&lt;/SPAN&gt;&lt;SPAN&gt;param&lt;/SPAN&gt;&lt;SPAN&gt; whichCounter SCTimer counter to use. In 16-bit mode, we can select Counter_L and Counter_H,&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* In 32-bit mode, we can select Counter_U.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;* @&lt;/SPAN&gt;&lt;SPAN&gt;param&lt;/SPAN&gt;&lt;SPAN&gt; value the counter value update to the COUNT register.&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;*/&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;static&lt;/SPAN&gt; &lt;SPAN&gt;inline&lt;/SPAN&gt; &lt;SPAN&gt;void&lt;/SPAN&gt; &lt;SPAN&gt;SCTIMER_SetCOUNTValue&lt;/SPAN&gt;&lt;SPAN&gt;(&lt;/SPAN&gt;&lt;SPAN&gt;SCT_Type&lt;/SPAN&gt;&lt;SPAN&gt; *base, &lt;/SPAN&gt;&lt;SPAN&gt;sctimer_counter_t&lt;/SPAN&gt;&lt;SPAN&gt; whichCounter, &lt;/SPAN&gt;&lt;SPAN&gt;uint32_t&lt;/SPAN&gt;&lt;SPAN&gt; value)&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;SCTIMER_StopTimer(base, (&lt;/SPAN&gt;&lt;SPAN&gt;uint32_t&lt;/SPAN&gt;&lt;SPAN&gt;)whichCounter);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;switch&lt;/SPAN&gt;&lt;SPAN&gt; (whichCounter)&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;{&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;case&lt;/SPAN&gt; &lt;SPAN&gt;kSCTIMER_Counter_L&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(value &amp;lt;= 0xFFFFU);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(0U == (base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;CONFIG&lt;/SPAN&gt;&lt;SPAN&gt; &amp;amp; SCT_CONFIG_UNIFY_MASK));&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/* Use Counter_L bits when user wants to setup the Low counter */&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;COUNT_ACCESS16BIT&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;COUNTL&lt;/SPAN&gt;&lt;SPAN&gt; = (&lt;/SPAN&gt;&lt;SPAN&gt;uint16_t&lt;/SPAN&gt;&lt;SPAN&gt;)value;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;break&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;case&lt;/SPAN&gt; &lt;SPAN&gt;kSCTIMER_Counter_H&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(value &amp;lt;= 0xFFFFU);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(0U == (base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;CONFIG&lt;/SPAN&gt;&lt;SPAN&gt; &amp;amp; SCT_CONFIG_UNIFY_MASK));&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/* Use Counter_H bits when user wants to setup the High counter */&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2" color="#FF0000"&gt;&lt;SPAN&gt;// base-&amp;gt;COUNT = (uint32_t)base-&amp;gt;COUNT_ACCESS16BIT.COUNTL | SCT_COUNT_CTR_H(value);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2" color="#00FF00"&gt;&lt;SPAN&gt;base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;COUNT_ACCESS16BIT&lt;/SPAN&gt;&lt;SPAN&gt;.&lt;/SPAN&gt;&lt;SPAN&gt;COUNTH&lt;/SPAN&gt;&lt;SPAN&gt; = (&lt;/SPAN&gt;&lt;SPAN&gt;uint16_t&lt;/SPAN&gt;&lt;SPAN&gt;)value; //the fix&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;break&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;case&lt;/SPAN&gt; &lt;SPAN&gt;kSCTIMER_Counter_U&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;assert(1U == (base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;CONFIG&lt;/SPAN&gt;&lt;SPAN&gt; &amp;amp; SCT_CONFIG_UNIFY_MASK));&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/* Use both Counter_L/Counter_H bits when counter is operating in 32-bit mode (unify counter). */&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;base-&amp;gt;&lt;/SPAN&gt;&lt;SPAN&gt;COUNT&lt;/SPAN&gt;&lt;SPAN&gt; = value;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;break&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;default&lt;/SPAN&gt;&lt;SPAN&gt;:&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;/* Fix the MISRA C-2012 issue rule 16.4. */&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;break&lt;/SPAN&gt;&lt;SPAN&gt;;&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;SCTIMER_StartTimer(base, (&lt;/SPAN&gt;&lt;SPAN&gt;uint32_t&lt;/SPAN&gt;&lt;SPAN&gt;)whichCounter);&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;P&gt;&lt;FONT size="2"&gt;&lt;SPAN&gt;}&lt;/SPAN&gt;&lt;/FONT&gt;&lt;/P&gt;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Sun, 27 Sep 2026 06:22:41 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN547-SC-Timer0-SDK-driver-Issue/m-p/2416496#M5958</guid>
      <dc:creator>JawaharA</dc:creator>
      <dc:date>2026-09-27T06:22:41Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN547 SC Timer0 SDK driver Issue</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN547-SC-Timer0-SDK-driver-Issue/m-p/2416726#M5963</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264875"&gt;@JawaharA&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thank you for your feedback. Your analysis of the cause of the Bus Fault is correct: updating COUNT_H uses a 32-bit write to the COUNT register, but the current function halts only the H counter. If the L counter is still running, this write access triggers an SCT bus error.&lt;/P&gt;
&lt;P&gt;However, changing the access to a 16-bit write to COUNTH is not compliant with the SCT hardware access requirements, because COUNT_H must be written as a word together with COUNT_L . The correct software solution is to halt both the L and H counters before performing the 32-bit write to COUNT , and then restore their previous running states afterward. We recommend reviewing and updating the SDK accordingly rather than using a separate 16-bit write to COUNT_H .&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Harry_Zhang_0-1790589981399.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/396951i221663A06531534B/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Harry_Zhang_0-1790589981399.png" alt="Harry_Zhang_0-1790589981399.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Harry&lt;/P&gt;</description>
      <pubDate>Mon, 28 Sep 2026 10:07:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN547-SC-Timer0-SDK-driver-Issue/m-p/2416726#M5963</guid>
      <dc:creator>Harry_Zhang</dc:creator>
      <dc:date>2026-09-28T10:07:28Z</dc:date>
    </item>
  </channel>
</rss>