<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic MCXW23x — BLE connection drops repeatedly when using FRO32K in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXW23x-BLE-connection-drops-repeatedly-when-using-FRO32K/m-p/2414364#M5925</link>
    <description>&lt;P&gt;MCXW235B BLE connection drops repeatedly, `disconnect reason=0x08` (LL supervision timeout), consistently a few seconds after connect&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hardware constraint (fixed, not changeable on this design):** the custom board does **not** populate a 32.768kHz crystal on `XI32K`/`XO32K` — both pins are left open. The board only has a 32MHz crystal on `XI32M`/`XO32M`&lt;/P&gt;</description>
    <pubDate>Thu, 17 Sep 2026 14:28:31 GMT</pubDate>
    <dc:creator>LongLeWT</dc:creator>
    <dc:date>2026-09-17T14:28:31Z</dc:date>
    <item>
      <title>MCXW23x — BLE connection drops repeatedly when using FRO32K</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXW23x-BLE-connection-drops-repeatedly-when-using-FRO32K/m-p/2414364#M5925</link>
      <description>&lt;P&gt;MCXW235B BLE connection drops repeatedly, `disconnect reason=0x08` (LL supervision timeout), consistently a few seconds after connect&amp;nbsp;&lt;/P&gt;&lt;P&gt;Hardware constraint (fixed, not changeable on this design):** the custom board does **not** populate a 32.768kHz crystal on `XI32K`/`XO32K` — both pins are left open. The board only has a 32MHz crystal on `XI32M`/`XO32M`&lt;/P&gt;</description>
      <pubDate>Thu, 17 Sep 2026 14:28:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXW23x-BLE-connection-drops-repeatedly-when-using-FRO32K/m-p/2414364#M5925</guid>
      <dc:creator>LongLeWT</dc:creator>
      <dc:date>2026-09-17T14:28:31Z</dc:date>
    </item>
    <item>
      <title>Re: MCXW23x — BLE connection drops repeatedly when using FRO32K</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXW23x-BLE-connection-drops-repeatedly-when-using-FRO32K/m-p/2414668#M5931</link>
      <description>&lt;P&gt;Hello, hope you are doing well.&lt;BR /&gt;&lt;BR /&gt;&lt;/P&gt;
&lt;P&gt;How are you selecting the clock source in your application?&amp;nbsp;&lt;/P&gt;
&lt;P&gt;FRO32K is supported as an option for the BLE sleep clock, as part of the two low-frequency sources available for MCXW23xB: external crystal oscillator XO_32K, and 32.768 kHz freely running oscillator FRO_32K.&lt;/P&gt;
&lt;P&gt;The command "HCI_CMD_OCF_LE_SELECT_SLEEP_CLOCK_SOURCE" is used to select the sleep clock source that is used for the sleep timer, where FRO32K is a sleep clock source (slp_clk_src=0x01).&amp;nbsp; In a case where the 32.768 kHz crystal (XO_32K) is absent, the free running oscillator (FRO_32K) can also act as a backup of the 32.768 kHz clocking.&lt;/P&gt;
&lt;P&gt;In MCXW23, the frequency of an on-chip or off-chip clock signal can be measured accurately with a selectable reference&amp;nbsp;clock. For example, the frequency measurement function can be used to determine the frequency of the&amp;nbsp;32.768 kHz free running oscillator (FRO32K) accurately, using the frequency measure function control register&amp;nbsp;(FREQ_ME_CTRL). To start a frequency measurement cycle and read the result, see MCXW23 Reference Manual Section 11.4.1. The FRO32K trim registers are available in RM section 45.4.11.2.13 FRO32K control (FRO32K)&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best regards,&lt;BR /&gt;Sofia.&lt;/P&gt;</description>
      <pubDate>Fri, 18 Sep 2026 23:43:20 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXW23x-BLE-connection-drops-repeatedly-when-using-FRO32K/m-p/2414668#M5931</guid>
      <dc:creator>sofiaurueta</dc:creator>
      <dc:date>2026-09-18T23:43:20Z</dc:date>
    </item>
    <item>
      <title>Re: MCXW23x — BLE connection drops repeatedly when using FRO32K</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXW23x-BLE-connection-drops-repeatedly-when-using-FRO32K/m-p/2414834#M5934</link>
      <description>&lt;P&gt;Dear&amp;nbsp;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;A href="https://community.nxp.com/t5/user/viewprofilepage/user-id/242964" rel="noopener" target="_blank"&gt;&lt;SPAN class=""&gt;sofiaurueta&lt;/SPAN&gt;&lt;/A&gt;,&amp;nbsp;&lt;/P&gt;&lt;P&gt;Thanks for your reply.&amp;nbsp;&lt;/P&gt;&lt;P&gt;We also tested ll_intf_curb_sleep_state(1) to disable sleep, which returned &lt;STRONG&gt;0&lt;/STRONG&gt;. After reviewing the code, we couldn't find any explicit sleep commands. Furthermore, ll_intf_le_select_slp_clk_src(RTC_SLPTMR) was configured with value 0x02, corresponding to the RTC clock source.&lt;/P&gt;&lt;P&gt;Additionally, we integrated FSCI into the Wireless UART sample and tested Peripheral mode, where we observed the following RX data when connecting via phone.&lt;/P&gt;&lt;P&gt;Best Regards,&lt;/P&gt;</description>
      <pubDate>Mon, 21 Sep 2026 03:44:28 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXW23x-BLE-connection-drops-repeatedly-when-using-FRO32K/m-p/2414834#M5934</guid>
      <dc:creator>LongLeWT</dc:creator>
      <dc:date>2026-09-21T03:44:28Z</dc:date>
    </item>
  </channel>
</rss>