<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: Multiple Face detection with MCXN947 - Error on image in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410807#M5898</link>
    <description>Thank you. It works now, resoldered.</description>
    <pubDate>Thu, 03 Sep 2026 05:42:51 GMT</pubDate>
    <dc:creator>Gayathriii</dc:creator>
    <dc:date>2026-09-03T05:42:51Z</dc:date>
    <item>
      <title>Multiple Face detection with MCXN947 - Error on image</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410330#M5884</link>
      <description>&lt;P&gt;Hi, I’m trying to run the “Multiple Face Detection on MCXN947” application from NXP Application Code Hub. The application is running, but the camera image is not being captured correctly. I can see some pixels and a faint outline of my face, but the image is highly distorted and not clear enough for proper recognition. Could this be caused by an issue with the camera rework/soldering or the camera signal connections? I have already followed the recommended camera rework procedure (SJ16, SJ26, and SJ27).&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2026 06:50:39 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410330#M5884</guid>
      <dc:creator>Gayathriii</dc:creator>
      <dc:date>2026-09-02T06:50:39Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Face detection with MCXN947 - Error on image</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410354#M5887</link>
      <description>&lt;P&gt;Hello,&lt;BR /&gt;&lt;BR /&gt;Yes, a distorted image with missing pixels or a faint outline can definitely still be caused by hardware soldering, connection issues, or partial contact, even if you have correctly flipped solder jumpers SJ16, SJ26, and SJ27 from side A to side B.&lt;BR /&gt;&lt;BR /&gt;&lt;BR /&gt;Best Regards&lt;/P&gt;</description>
      <pubDate>Wed, 02 Sep 2026 07:52:27 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410354#M5887</guid>
      <dc:creator>kenasa2158</dc:creator>
      <dc:date>2026-09-02T07:52:27Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Face detection with MCXN947 - Error on image</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410766#M5897</link>
      <description>&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/261601"&gt;@Gayathriii&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for your post.&amp;nbsp;You may find some helpful tips in&amp;nbsp;&lt;A style="background-color: #ffffff; outline: 0px;" href="https://community.nxp.com/t5/MCX-Microcontrollers-Knowledge/Vision-ML-with-the-FRDM-MCXN947/ta-p/2313227" target="_blank"&gt;Vision ML with the FRDM-MCXN947&lt;/A&gt;&lt;SPAN&gt;, which could be useful for addressing this issue.&amp;nbsp;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;1. After POR there may be some glitching on the camera due to the fact the camera is expecting 2.8V but the board is at 3.3V and the initial HSYNC signal was missed. Press the reset button (SW1) and it should fix any camera issue.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;2.&amp;nbsp;Please confirm the OV7670 camera is plugged into J11 (not J9) and the LCD-PAR-S035 is connected to J12&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1788406926113.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395808iBFFFBC5EDBDBFE21/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1788406926113.png" alt="Celeste_Liu_0-1788406926113.png" /&gt;&lt;span class="lia-inline-image-caption" onclick="event.preventDefault();"&gt;Celeste_Liu_0-1788406926113.png&lt;/span&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;3.&amp;nbsp;Confirm correct solder jumper orientation for SJ16, SJ26, and SJ27&lt;/P&gt;
&lt;P&gt;Hope it helps. Please let me know if you still have problem on this.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Thu, 03 Sep 2026 03:45:18 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410766#M5897</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-09-03T03:45:18Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Face detection with MCXN947 - Error on image</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410807#M5898</link>
      <description>Thank you. It works now, resoldered.</description>
      <pubDate>Thu, 03 Sep 2026 05:42:51 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410807#M5898</guid>
      <dc:creator>Gayathriii</dc:creator>
      <dc:date>2026-09-03T05:42:51Z</dc:date>
    </item>
    <item>
      <title>Re: Multiple Face detection with MCXN947 - Error on image</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410808#M5899</link>
      <description>Thank you, I re soldered and It works now.</description>
      <pubDate>Thu, 03 Sep 2026 05:43:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Multiple-Face-detection-with-MCXN947-Error-on-image/m-p/2410808#M5899</guid>
      <dc:creator>Gayathriii</dc:creator>
      <dc:date>2026-09-03T05:43:15Z</dc:date>
    </item>
  </channel>
</rss>