<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックRe: Implementing Wi-Fi on MCXW72 using IW612/RW612 for EdgeLock 2GO Provisioning</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2408095#M5833</link>
    <description>Thanks for the reply and the Mongoose pointer! Quick follow-up though — before considering RW612, I was actually trying to get MCXW72 working with IW612 specifically (not RW612), since MCXW72 is our required security/application core (TF-M, EdgeLock Secure Enclave) for this project.&lt;BR /&gt;&lt;BR /&gt;From the IW612 datasheet, Wi-Fi is hardwired to SDIO only (Table 1, and the CONFIG_HOST_BOOT[1:0] pin table where every option except SDIO/UART/SPI for Wi-Fi/BT/802.15.4 respectively is marked "Reserved"). MCXW72's datasheet doesn't list any SDIO peripheral — only I2C, SPI, UART, CAN, FlexIO.&lt;BR /&gt;&lt;BR /&gt;So my question is: is it correct that MCXW72 physically cannot drive IW612's Wi-Fi at all, since it has no SDIO host controller? Or is there some way around this that I'm missing — e.g., an SDIO-over-SPI/UART workaround, or some other supported bridging method NXP provides for pairing these two specific chips?&lt;BR /&gt;&lt;BR /&gt;If MCXW72 + IW612 genuinely isn't feasible, that's useful to know — but I wanted to confirm this is a hard hardware limitation before ruling it out.</description>
    <pubDate>Tue, 25 Aug 2026 08:32:45 GMT</pubDate>
    <dc:creator>harshal_mehta5</dc:creator>
    <dc:date>2026-08-25T08:32:45Z</dc:date>
    <item>
      <title>Implementing Wi-Fi on MCXW72 using IW612/RW612 for EdgeLock 2GO Provisioning</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2407820#M5827</link>
      <description>&lt;DIV class=""&gt;Hi NXP Support,&lt;BR /&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;Hello NXP team,&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;BR /&gt;How can I practically implement Wi-Fi on the &lt;STRONG&gt;MCXW72&lt;/STRONG&gt; using either the &lt;STRONG&gt;IW612&lt;/STRONG&gt; or &lt;STRONG&gt;RW612&lt;/STRONG&gt; specifically to execute &lt;STRONG&gt;EdgeLock 2GO provisioning&lt;/STRONG&gt;?&lt;BR /&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;Please provide the exact hardware connection requirements, drivers, and software stacks needed to make this specific setup work. Note that our application &lt;STRONG&gt;cannot use Thread or Matter protocols&lt;/STRONG&gt;.&lt;BR /&gt;&lt;BR /&gt;&lt;/DIV&gt;&lt;DIV class=""&gt;Thanks,&lt;BR /&gt;Harshal&lt;/DIV&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;DIV class=""&gt;&lt;DIV class=""&gt;&amp;nbsp;&lt;/DIV&gt;&lt;/DIV&gt;</description>
      <pubDate>Mon, 24 Aug 2026 13:34:01 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2407820#M5827</guid>
      <dc:creator>harshal_mehta5</dc:creator>
      <dc:date>2026-08-24T13:34:01Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing Wi-Fi on MCXW72 using IW612/RW612 for EdgeLock 2GO Provisioning</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2407886#M5828</link>
      <description>&lt;P&gt;Hello Harshal,&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Hope you are doing well. Could you please clarify what are your requirements?&lt;/P&gt;
&lt;P&gt;Could you please confirm if you are following any of these Application Notes?&lt;/P&gt;
&lt;UL type="disc"&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN15038&amp;amp;isHTMLorPDF=HTML" target="_blank"&gt;EdgeLock&amp;nbsp;2GO&amp;nbsp;Provisioning MCUs via Product Type using Secure Provisioning (SEC) Tool&lt;/A&gt;[AN15038]&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://docs.nxp.com/bundle/AN14670/page/topics/introduction.html" target="_blank"&gt;EdgeLock&amp;nbsp;2GO&amp;nbsp;Provisioning via SPSDK for MCUs&lt;/A&gt;[AN14670]&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN14624&amp;amp;isHTMLorPDF=HTML" target="_blank"&gt;EdgeLock&amp;nbsp;2GO&amp;nbsp;Provisioning via Secure Provisioning Tool (SEC) for MCUs&lt;/A&gt;[AN14624]&lt;/LI&gt;
&lt;LI&gt;&lt;A href="https://www.nxp.com/webapp/Download?colCode=AN14544&amp;amp;isHTMLorPDF=HTML" target="_blank"&gt;EdgeLock&amp;nbsp;2GO&amp;nbsp;Services for MPU and MCU&lt;/A&gt;[AN14544]&lt;/LI&gt;
&lt;/UL&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The MCXW72 doesn't offer the hardware interfaces the IW612 needs to operate as a hosted Wi-Fi module. The IW612 requires SDIO 3.0 for Wi-Fi, UART for Bluetooth, and SPI for 802.15.4&lt;/P&gt;
&lt;P&gt;If you are looking for a device that supports all these protocols, then I would recommend the RW612 as an all-in-one product.&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Best Regards,&lt;/P&gt;
&lt;P&gt;Ricardo&lt;/P&gt;</description>
      <pubDate>Mon, 24 Aug 2026 21:23:43 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2407886#M5828</guid>
      <dc:creator>Ricardo_Zamora</dc:creator>
      <dc:date>2026-08-24T21:23:43Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing Wi-Fi on MCXW72 using IW612/RW612 for EdgeLock 2GO Provisioning</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2408088#M5832</link>
      <description>&lt;P&gt;Hi Harshal,&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Quick question: why do you need the MCXW72 for this setup? The RW612 is already a wireless MCU. You could just run your application directly on the RW612 and drop the extra microcontroller entirely.&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;If you go with the RW612, you can use the Mongoose networking library to handle your Wi-Fi and networking stacks. From there, you can focus directly on your application. There is a ready to use RW612 example &lt;A href="https://mongoose.ws/wizard/#/output?board=rw612-w&amp;amp;ide=MCUXpresso&amp;amp;rtos=FreeRTOS&amp;amp;file=README.md" target="_self"&gt;here&lt;/A&gt; that can give you a good starting point.&lt;/P&gt;&lt;P&gt;&lt;SPAN&gt;To download it to your local workspace, open the link, select the 'Settings' panel and choose a destination directory. Then download the project to your computer by clicking the blue 'Generate C/C++' button. You can then open it with MCUXpresso IDE, build it, and flash it.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;&lt;BR /&gt;Heads up: I am part of the Mongoose development team, I hope this helps you in your project&lt;/P&gt;</description>
      <pubDate>Tue, 25 Aug 2026 08:24:44 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2408088#M5832</guid>
      <dc:creator>MStackDev_376</dc:creator>
      <dc:date>2026-08-25T08:24:44Z</dc:date>
    </item>
    <item>
      <title>Re: Implementing Wi-Fi on MCXW72 using IW612/RW612 for EdgeLock 2GO Provisioning</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2408095#M5833</link>
      <description>Thanks for the reply and the Mongoose pointer! Quick follow-up though — before considering RW612, I was actually trying to get MCXW72 working with IW612 specifically (not RW612), since MCXW72 is our required security/application core (TF-M, EdgeLock Secure Enclave) for this project.&lt;BR /&gt;&lt;BR /&gt;From the IW612 datasheet, Wi-Fi is hardwired to SDIO only (Table 1, and the CONFIG_HOST_BOOT[1:0] pin table where every option except SDIO/UART/SPI for Wi-Fi/BT/802.15.4 respectively is marked "Reserved"). MCXW72's datasheet doesn't list any SDIO peripheral — only I2C, SPI, UART, CAN, FlexIO.&lt;BR /&gt;&lt;BR /&gt;So my question is: is it correct that MCXW72 physically cannot drive IW612's Wi-Fi at all, since it has no SDIO host controller? Or is there some way around this that I'm missing — e.g., an SDIO-over-SPI/UART workaround, or some other supported bridging method NXP provides for pairing these two specific chips?&lt;BR /&gt;&lt;BR /&gt;If MCXW72 + IW612 genuinely isn't feasible, that's useful to know — but I wanted to confirm this is a hard hardware limitation before ruling it out.</description>
      <pubDate>Tue, 25 Aug 2026 08:32:45 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/Implementing-Wi-Fi-on-MCXW72-using-IW612-RW612-for-EdgeLock-2GO/m-p/2408095#M5833</guid>
      <dc:creator>harshal_mehta5</dc:creator>
      <dc:date>2026-08-25T08:32:45Z</dc:date>
    </item>
  </channel>
</rss>