<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>MCX MicrocontrollersのトピックIMX8QXP RAM ECC</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/IMX8QXP-RAM-ECC/m-p/2406398#M5813</link>
    <description>&lt;P&gt;&lt;SPAN class=""&gt;My i.MX 8QXP board is configured to use sideband ECC mode. Is there a Linux driver available that supports this and can detect ECC errors? I haven't found any ECC-related registers in the Applications Processor Reference Manual (PRM).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;THANKS.&lt;/P&gt;</description>
    <pubDate>Wed, 19 Aug 2026 04:00:06 GMT</pubDate>
    <dc:creator>qwerty1123</dc:creator>
    <dc:date>2026-08-19T04:00:06Z</dc:date>
    <item>
      <title>IMX8QXP RAM ECC</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/IMX8QXP-RAM-ECC/m-p/2406398#M5813</link>
      <description>&lt;P&gt;&lt;SPAN class=""&gt;My i.MX 8QXP board is configured to use sideband ECC mode. Is there a Linux driver available that supports this and can detect ECC errors? I haven't found any ECC-related registers in the Applications Processor Reference Manual (PRM).&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;THANKS.&lt;/P&gt;</description>
      <pubDate>Wed, 19 Aug 2026 04:00:06 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/IMX8QXP-RAM-ECC/m-p/2406398#M5813</guid>
      <dc:creator>qwerty1123</dc:creator>
      <dc:date>2026-08-19T04:00:06Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP RAM ECC</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/IMX8QXP-RAM-ECC/m-p/2406441#M5814</link>
      <description>&lt;P&gt;&lt;SPAN&gt;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252549"&gt;@qwerty1123&lt;/a&gt;&amp;nbsp;&lt;BR /&gt;ECC can be enabled and errors can be detected by the DDRC hardware, but you should not expect an existing Linux EDAC driver for i.MX 8QXP sideband ECC unless you have a BSP/private patch outside the retrieved sources. A board-specific driver would need to map the DDRC ECC registers from &lt;STRONG&gt;AN13566&lt;/STRONG&gt;, handle&amp;nbsp;&lt;/SPAN&gt;&lt;CODE class=""&gt;ECC_CORRECT_INT&lt;/CODE&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;/&amp;nbsp;&lt;/SPAN&gt;&lt;CODE class=""&gt;ECC_NCORRECT_INT&lt;/CODE&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;, read&amp;nbsp;&lt;/SPAN&gt;&lt;CODE class=""&gt;ECCSTAT&lt;/CODE&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;/&amp;nbsp;&lt;/SPAN&gt;&lt;CODE class=""&gt;ECCERRCNT&lt;/CODE&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;, clear through&amp;nbsp;&lt;/SPAN&gt;&lt;CODE class=""&gt;ECCCTL&lt;/CODE&gt;&lt;SPAN&gt;&amp;nbsp;&lt;/SPAN&gt;&lt;SPAN&gt;, and optionally register with the Linux EDAC framework.&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;DIV&gt;The app note describes correctable, uncorrectable, and AP error interrupt enables and status handling through DDRC registers. So, you most probably have to write a custom driver for it.&lt;/DIV&gt;
&lt;P&gt;&lt;SPAN&gt;&lt;BR /&gt;&lt;BR /&gt;&lt;/SPAN&gt;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Aug 2026 06:26:31 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/IMX8QXP-RAM-ECC/m-p/2406441#M5814</guid>
      <dc:creator>gaurav_sharma</dc:creator>
      <dc:date>2026-08-19T06:26:31Z</dc:date>
    </item>
    <item>
      <title>Re: IMX8QXP RAM ECC</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/IMX8QXP-RAM-ECC/m-p/2406453#M5816</link>
      <description>&lt;P&gt;Hi&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/252549"&gt;@qwerty1123&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;We have not yet released a verification module for ECC. You will need to write your own verification program. Please refer to the documentation below.&lt;/P&gt;
&lt;P&gt;&lt;A href="https://www.nxp.com/docs/en/application-note/AN13566.pdf" target="_blank"&gt;https://www.nxp.com/docs/en/application-note/AN13566.pdf&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;You can refer IMX8DXL RM about ECC register. imx8qxp and imx8dxl use the same DDRC IP.&amp;nbsp;&lt;/P&gt;
&lt;P&gt;B.R&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Wed, 19 Aug 2026 07:03:40 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/IMX8QXP-RAM-ECC/m-p/2406453#M5816</guid>
      <dc:creator>pengyong_zhang</dc:creator>
      <dc:date>2026-08-19T07:03:40Z</dc:date>
    </item>
  </channel>
</rss>