<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic Re: MCXN236 not supported in Config Tools..!? in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2405688#M5804</link>
    <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83226"&gt;@dav1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you for your question on the NXP Community!&lt;/P&gt;
&lt;P&gt;MCXN236 is supported in MCUXpresso Config Tools. Support for the MCXN2xx series (including FRDM-MCXN236) was introduced in Config Tools v15 (bundled with MCUXpresso IDE v11.9.0) and continues to be available in the current v26.06.&lt;/P&gt;
&lt;P&gt;The error you are seeing is most likely related to how the project was set up. Config Tools needs to be launched from within a proper SDK-based project in order to correctly identify the device and generate initialization code, simply downloading processor data via the Data Manager is not sufficient to enable full tool functionality.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1786953700422.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394734i4140B7342743B45C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1786953700422.png" alt="Celeste_Liu_0-1786953700422.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;When creating a new configuration in the standalone Config Tools, we recommend selecting a project type that is associated with an SDK or a specific toolchain, rather than a processor-only configuration, to ensure the device is correctly recognized.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_1-1786953835716.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394735i0562199E29883880/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_1-1786953835716.png" alt="Celeste_Liu_1-1786953835716.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Additionally, please note that the standalone Config Tools is not intended for use with MCUXpresso IDE, if your development environment is MCUXpresso IDE, please use the Config Tools that are integrated within MCUXpresso IDE directly. For other supported IDEs such as IAR Embedded Workbench or Keil MDK, the standalone Config Tools is the appropriate choice. If you are using MCUXpresso for VS Code, Config Tools is also built in and does not require the standalone version.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_2-1786954108390.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394739i585613370FF297F8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_2-1786954108390.png" alt="Celeste_Liu_2-1786954108390.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;We hope this helps! Please feel free to follow up if you have further questions.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
    <pubDate>Mon, 17 Aug 2026 08:13:15 GMT</pubDate>
    <dc:creator>Celeste_Liu</dc:creator>
    <dc:date>2026-08-17T08:13:15Z</dc:date>
    <item>
      <title>MCXN236 not supported in Config Tools..!?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2405575#M5799</link>
      <description>&lt;P&gt;I just downloaded what I believe is the latest &lt;STRONG&gt;MCUXpresso Config Tools 26.06&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;Using the "Data Manager", downloaded the FRDM-MCXN236 Design Files + the N236 processor files as well&lt;/P&gt;&lt;P&gt;issue: tool says,&amp;nbsp;&lt;STRONG&gt;Device Configuration tool does not support the selected processor. Select a different tool&lt;/STRONG&gt;&lt;/P&gt;&lt;P&gt;see below screenshot.&amp;nbsp;&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dav1_0-1786910536184.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394708iEACA26458A8FE0E9/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dav1_0-1786910536184.png" alt="dav1_0-1786910536184.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;is there a plan to add N23-series?&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Sun, 16 Aug 2026 20:04:25 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2405575#M5799</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2026-08-16T20:04:25Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN236 not supported in Config Tools..!?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2405688#M5804</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83226"&gt;@dav1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thank you for your question on the NXP Community!&lt;/P&gt;
&lt;P&gt;MCXN236 is supported in MCUXpresso Config Tools. Support for the MCXN2xx series (including FRDM-MCXN236) was introduced in Config Tools v15 (bundled with MCUXpresso IDE v11.9.0) and continues to be available in the current v26.06.&lt;/P&gt;
&lt;P&gt;The error you are seeing is most likely related to how the project was set up. Config Tools needs to be launched from within a proper SDK-based project in order to correctly identify the device and generate initialization code, simply downloading processor data via the Data Manager is not sufficient to enable full tool functionality.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1786953700422.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394734i4140B7342743B45C/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1786953700422.png" alt="Celeste_Liu_0-1786953700422.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;When creating a new configuration in the standalone Config Tools, we recommend selecting a project type that is associated with an SDK or a specific toolchain, rather than a processor-only configuration, to ensure the device is correctly recognized.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_1-1786953835716.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394735i0562199E29883880/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_1-1786953835716.png" alt="Celeste_Liu_1-1786953835716.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;Additionally, please note that the standalone Config Tools is not intended for use with MCUXpresso IDE, if your development environment is MCUXpresso IDE, please use the Config Tools that are integrated within MCUXpresso IDE directly. For other supported IDEs such as IAR Embedded Workbench or Keil MDK, the standalone Config Tools is the appropriate choice. If you are using MCUXpresso for VS Code, Config Tools is also built in and does not require the standalone version.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_2-1786954108390.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/394739i585613370FF297F8/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_2-1786954108390.png" alt="Celeste_Liu_2-1786954108390.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;We hope this helps! Please feel free to follow up if you have further questions.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Mon, 17 Aug 2026 08:13:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2405688#M5804</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-08-17T08:13:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN236 not supported in Config Tools..!?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2407738#M5824</link>
      <description>&lt;P&gt;hi, thanks for answer.&amp;nbsp;&lt;/P&gt;&lt;P&gt;first, we use Zephyr, so no need to install MCUXpresso IDE.&lt;BR /&gt;seems there are several variants of the pins tools, can you please guide me to which one is the correct installer/app for MCX series.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;about the error message, I used this option as I'm using the FRDM kit and wanted its config/schematic wiring&lt;BR /&gt;when working on my own board, i will try again the order you mentioned, but I'm pretty sure that error message still shows&lt;/P&gt;&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="dav1_0-1787560877796.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395176iDC3B9C8424837A04/image-size/medium?v=v2&amp;amp;px=400" role="button" title="dav1_0-1787560877796.png" alt="dav1_0-1787560877796.png" /&gt;&lt;/span&gt;&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;</description>
      <pubDate>Mon, 24 Aug 2026 08:42:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2407738#M5824</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2026-08-24T08:42:15Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN236 not supported in Config Tools..!?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2409229#M5846</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83226"&gt;@dav1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Sorry for the late reply. And thanks for you telling me that you are using config tools for Zephyr. Thus you should choose “Create a new configuration for Zephyr RTOS":&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_0-1787911049792.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395497i01F53A2D65EF62B1/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_0-1787911049792.png" alt="Celeste_Liu_0-1787911049792.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;For the detailed steps, you can refer to&amp;nbsp;&lt;A href="https://docs.mcuxpresso.nxp.com/config/26.06/user_interface.html#creating-a-new-configuration-for-zephyr-rtos" target="_blank"&gt;User interface — MCUXpresso Configuration Tools 26.06 documentation&lt;/A&gt;&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_1-1787911611797.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395498i6D2CA5BC93B3DF49/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_1-1787911611797.png" alt="Celeste_Liu_1-1787911611797.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;The error message you saw was expected. Because config tools &lt;STRONG&gt;only support pin&lt;/STRONG&gt; configuration for zephyr.&lt;/P&gt;
&lt;P&gt;&lt;span class="lia-inline-image-display-wrapper lia-image-align-inline" image-alt="Celeste_Liu_2-1787911669445.png" style="width: 400px;"&gt;&lt;img src="https://community.nxp.com/t5/image/serverpage/image-id/395499i0519FCAC87B91113/image-size/medium?v=v2&amp;amp;px=400" role="button" title="Celeste_Liu_2-1787911669445.png" alt="Celeste_Liu_2-1787911669445.png" /&gt;&lt;/span&gt;&lt;/P&gt;
&lt;P&gt;For your convenience, I have also recorded a video demonstrating the steps. Please feel free to use it as a reference. I hope it helps.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Fri, 28 Aug 2026 10:32:14 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2409229#M5846</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-08-28T10:32:14Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN236 not supported in Config Tools..!?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2409261#M5847</link>
      <description>&lt;P&gt;hi, thanks for great support. but i'm not sure what you mean with&lt;/P&gt;&lt;P&gt;&lt;STRONG&gt;&amp;gt; only support pin&lt;/STRONG&gt;&lt;SPAN&gt; configuration for zephyr.&lt;/SPAN&gt;&lt;/P&gt;&lt;P&gt;what features are omitted?&amp;nbsp;&lt;/P&gt;&lt;P&gt;i want to ensure clock-config is valid, should I expect these views to be broken?&lt;/P&gt;</description>
      <pubDate>Fri, 28 Aug 2026 13:57:29 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2409261#M5847</guid>
      <dc:creator>dav1</dc:creator>
      <dc:date>2026-08-28T13:57:29Z</dc:date>
    </item>
    <item>
      <title>Re: MCXN236 not supported in Config Tools..!?</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2409480#M5848</link>
      <description>&lt;P&gt;Hello&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/83226"&gt;@dav1&lt;/a&gt;&amp;nbsp;,&lt;/P&gt;
&lt;P&gt;Thanks for the follow-up, happy to clarify.&lt;/P&gt;
&lt;P&gt;When you open MCUXpresso Config Tools on a Zephyr project, the tool acts only as a generator for pin control(the Device Tree pinctrl entries). It does not operate on the project the same way it does for an MCUXpresso SDK project, it doesn't import or manage the rest of your project configuration.&lt;/P&gt;
&lt;P&gt;Because of this, when you create a Zephyr configuration, only the Pins tool is enabled. The other views are intentionally greyed out (disabled) in this mode.&lt;/P&gt;
&lt;P&gt;So Clocks/Peripherals aren't broken, they are simply not offered in the Zephyr workflow, as noted in the Config Tools documentation I shared earlier (screenshot above) for your reference.&lt;/P&gt;
&lt;P&gt;BR&lt;/P&gt;
&lt;P&gt;Celeste&lt;/P&gt;</description>
      <pubDate>Mon, 31 Aug 2026 04:14:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/MCXN236-not-supported-in-Config-Tools/m-p/2409480#M5848</guid>
      <dc:creator>Celeste_Liu</dc:creator>
      <dc:date>2026-08-31T04:14:03Z</dc:date>
    </item>
  </channel>
</rss>