<?xml version="1.0" encoding="UTF-8"?>
<rss xmlns:content="http://purl.org/rss/1.0/modules/content/" xmlns:dc="http://purl.org/dc/elements/1.1/" xmlns:rdf="http://www.w3.org/1999/02/22-rdf-syntax-ns#" xmlns:taxo="http://purl.org/rss/1.0/modules/taxonomy/" version="2.0">
  <channel>
    <title>topic kw45 in MCX Microcontrollers</title>
    <link>https://community.nxp.com/t5/MCX-Microcontrollers/kw45/m-p/2395198#M5642</link>
    <description>&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;WE were designing a product using KW45 and we saw it&amp;nbsp; supports LPSPI, but we wanted to interact with the QSPI flash&amp;nbsp;W25Q128JWFIQ TR.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does it supports?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if it does, what and all possible hardware and software configurations need to be done&lt;/P&gt;</description>
    <pubDate>Wed, 15 Jul 2026 06:15:15 GMT</pubDate>
    <dc:creator>TejasN2255</dc:creator>
    <dc:date>2026-07-15T06:15:15Z</dc:date>
    <item>
      <title>kw45</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/kw45/m-p/2395198#M5642</link>
      <description>&lt;P&gt;Hello team,&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;WE were designing a product using KW45 and we saw it&amp;nbsp; supports LPSPI, but we wanted to interact with the QSPI flash&amp;nbsp;W25Q128JWFIQ TR.&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;Does it supports?&lt;/P&gt;&lt;P&gt;&amp;nbsp;&lt;/P&gt;&lt;P&gt;if it does, what and all possible hardware and software configurations need to be done&lt;/P&gt;</description>
      <pubDate>Wed, 15 Jul 2026 06:15:15 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/kw45/m-p/2395198#M5642</guid>
      <dc:creator>TejasN2255</dc:creator>
      <dc:date>2026-07-15T06:15:15Z</dc:date>
    </item>
    <item>
      <title>Re: kw45</title>
      <link>https://community.nxp.com/t5/MCX-Microcontrollers/kw45/m-p/2395845#M5644</link>
      <description>&lt;P&gt;Hi,&amp;nbsp;&lt;a href="https://community.nxp.com/t5/user/viewprofilepage/user-id/264722"&gt;@TejasN2255&lt;/a&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;Thanks for creating case to us.&lt;/P&gt;
&lt;P&gt;Yes, it supports.&lt;/P&gt;
&lt;P&gt;You can use KW45 to&amp;nbsp;&lt;SPAN&gt;interact with the QSPI flash&amp;nbsp;W25Q128JWFIQ TR.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;But because KW45 doesn't have &lt;STRONG&gt;FlexSPI&amp;nbsp;and no execute-in-place (XIP) path&lt;/STRONG&gt;, so you could&amp;nbsp;only talk to the W25Q128JWFIQ over its &lt;STRONG&gt;LPSPI&lt;/STRONG&gt; peripheral.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;To use it, you need to be careful for the&lt;STRONG&gt;&amp;nbsp;Supply voltage.&lt;/STRONG&gt; The W25Q128JWFIQ is 1.8 V nominal (1.7–1.95 V). The KW45's I/O rail feeding LPSPI1 (VDD_MEM on the EVK) must be set to 1.8 V; do not tie it to a 3.3 V rail.&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&lt;SPAN&gt;You can refer to our &lt;A href="https://www.nxp.com/webapp/Download?colCode=KW45B41Z-EVK_SCH" target="_self"&gt;KW45B41Z-EVK_SCH&lt;/A&gt; schematics page 5, we have a similar connection with&amp;nbsp;AT25XE161D-MAHN-T, but the difference is the&amp;nbsp;&lt;STRONG&gt;Supply voltage.&lt;/STRONG&gt;&lt;/SPAN&gt;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;&lt;/P&gt;
&lt;P&gt;&amp;nbsp;Best regards,&lt;/P&gt;
&lt;P&gt;Christine.&lt;/P&gt;</description>
      <pubDate>Thu, 16 Jul 2026 09:27:03 GMT</pubDate>
      <guid>https://community.nxp.com/t5/MCX-Microcontrollers/kw45/m-p/2395845#M5644</guid>
      <dc:creator>Christine_Li</dc:creator>
      <dc:date>2026-07-16T09:27:03Z</dc:date>
    </item>
  </channel>
</rss>